End Devices#

EmberZNet API relating to end device children.

See child.h for source code.

Power Management#

enum
@5 {
SL_ZIGBEE_OUTGOING_MESSAGES = 0x0001
SL_ZIGBEE_INCOMING_MESSAGES = 0x0002
SL_ZIGBEE_RADIO_IS_ON = 0x0004
SL_ZIGBEE_TRANSPORT_ACTIVE = 0x0008
SL_ZIGBEE_APS_LAYER_ACTIVE = 0x0010
SL_ZIGBEE_ASSOCIATING = 0x0020
SL_ZIGBEE_ZLL_TOUCH_LINKING = 0x0040
SL_ZIGBEE_NETWORK_TIMEOUT_REQUEST = 0x0200
SL_ZIGBEE_SEND_ORPHAN_NOTIFICATION = 0x0400
SL_802154_DATA_POLL_SUPER_RETRY = 0x0800
}

Define tasks that are taken into account when dealing with sleep related behavior.

uint16_t

Return a bitmask indicating the stack's current tasks.

bool

Indicate whether the stack is currently in a state where there are no high-priority tasks, allowing the device to sleep.

bool

Indicate whether the parent token has been set by association.

bool

Indicate whether the stack currently has any tasks pending.

bool

Indicate whether the stack is currently in a state that does not require the application to periodically poll.

void

Immediately turn the radio power completely off.

void

Initialize the radio. Typically called coming out of deep sleep.

sl_status_t

Send a link power delta request to the parent.

int8_t

Accessor function for recent average RSSI value between this device and the parent (SoC only).

sl_802154_short_addr_t

Accessor function for the parent's node ID if applicable (SoC only).

sl_status_t

: Bit mask that decides which timeout values are acceptable for a child. It defaults to 0xFFFF which covers all the following 15 options:

#define
SL_ZIGBEE_HIGH_PRIORITY_TASKS (SL_ZIGBEE_OUTGOING_MESSAGES | SL_ZIGBEE_INCOMING_MESSAGES | SL_ZIGBEE_RADIO_IS_ON)

A mask of the tasks that prevent a device from sleeping.

Functions#

sl_802154_short_addr_t
sl_zigbee_child_id(uint8_t childIndex)

Convert a child index to a node ID.

int8_t
sl_zigbee_child_power(uint8_t childIndex)

Return radio power value of the child from the given childIndex.

void
sl_zigbee_set_child_power(uint8_t childIndex, int8_t newPower)

Set the radio power value for a given child index.

uint8_t
sl_zigbee_child_index(sl_802154_short_addr_t childId)

Convert a node ID to a child index.

sl_status_t
sl_zigbee_get_child_data(uint8_t index, sl_zigbee_child_data_t *childData)

Get the EUI64 and node type of the child at the provided index. If there is no child at 'index', it returns ::SL_STATUS_NOT_JOINED. Possible child indexes run from zero to sl_zigbee_max_child_count() - 1.

sl_status_t
sl_zigbee_set_child_data(uint8_t index, const sl_zigbee_child_data_t *childData)

Sets the EUI64, node ID, and node type of the child at the provided index in nonvolatile memory. No other data from the childData argument is used or copied. The user is responsible for rebooting the device after calling this API in order to initialize RAM-based child data. Possible child indexes run from zero to sl_zigbee_max_child_count() - 1.

void
sl_zigbee_child_join_handler(uint8_t index, bool joining, sl_802154_short_addr_t childId, sl_802154_long_addr_t childEui64, sl_zigbee_node_type_t childType)

Called by the stack when a child joins or leaves. 'Joining' is true if the child is joining and false if leaving.

sl_status_t
sl_zigbee_set_keep_alive_mode(sl_zigbee_keep_alive_mode_t mode)
sl_status_t

Request any pending data from the parent node. This function allows an end device to query its parent for any pending data.

void
sl_zigbee_set_mac_poll_failure_wait_time(uint32_t waitBeforeRetryIntervalMs)
void
sl_status_t
sl_zigbee_set_message_flag(sl_802154_short_addr_t childId)

Set a flag to indicate that a message is pending for a child. The next time that the child polls, it will be informed that it has a pending message. The message is sent from sl_zigbee_poll_handler, which is called when the child requests data.

sl_status_t
sl_zigbee_clear_message_flag(sl_802154_short_addr_t childId)

Clear a flag to indicate that there are no more messages for a child. The next time the child polls, it will be informed that it does not have any pending messages.

void
sl_zigbee_poll_handler(sl_802154_short_addr_t childId, bool transmitExpected)

Called to allow the application to send a message in response to a poll from a child.

sl_status_t
sl_zigbee_add_child(sl_802154_short_addr_t shortId, sl_802154_long_addr_t longId, sl_zigbee_node_type_t nodeType)

Add a child to the child/neighbor table only on SoC, allowing direct manipulation of these tables by the application. This can affect the network functionality, and needs to be used wisely. If used appropriately, the application can maintain more than the maximum of children provided by the stack.

sl_status_t
sl_zigbee_remove_child(sl_802154_long_addr_t childEui64)

Remove a node from child/neighbor table only on SoC, allowing direct manipulation of these tables by the application. This can affect the network functionality, and needs to be used wisely.

void
sl_zigbee_remove_neighbor(sl_802154_short_addr_t shortId, sl_802154_long_addr_t longId)

Remove a neighbor from neighbor table only on SoC, allowing direct manipulation of neighbor table by the application. This can affect the network functionality, and needs to be used wisely.

uint8_t

Return the number of children the node currently has.

uint8_t

Return the number of router children that the node currently has.

uint8_t

Return the maximum number of children for this node. The return value is undefined for nodes that are not joined to a network.

uint8_t

Return the maximum number of router children for this node. The return value is undefined for nodes that are not joined to a network.

sl_802154_short_addr_t

Return the parent's node ID. The return value is undefined for nodes without parents (coordinators and nodes that are not joined to a network).

sl_802154_long_addr_t

Return the parent's EUI64. The return value is undefined for nodes without parents (coordinators and nodes that are not joined to a network).

Power Management Documentation#

@5#

@5

Define tasks that are taken into account when dealing with sleep related behavior.

As opposed to its subset of SL_ZIGBEE_HIGH_PRIORITY_TASKS, these tasks do not necessarily prevent the device from going to sleep. However, they are taken into account when calculating how long we can sleep until the next event.

Enumerator
SL_ZIGBEE_OUTGOING_MESSAGES

Messages are waiting for transmission.

SL_ZIGBEE_INCOMING_MESSAGES

One or more incoming messages are being processed.

SL_ZIGBEE_RADIO_IS_ON

The radio is currently powered on. On sleepy devices, the radio is turned off when not in use. On non-sleepy devices (SL_ZIGBEE_COORDINATOR, SL_ZIGBEE_ROUTER, or SL_ZIGBEE_END_DEVICE), the radio is always on.

SL_ZIGBEE_TRANSPORT_ACTIVE

The transport layer has messages awaiting an ACK.

SL_ZIGBEE_APS_LAYER_ACTIVE

The ZigBee APS layer has messages awaiting an ACK.

SL_ZIGBEE_ASSOCIATING

The node is currently trying to associate with a ZigBee PRO network.

SL_ZIGBEE_ZLL_TOUCH_LINKING

The node is currently touch linking.

SL_ZIGBEE_NETWORK_TIMEOUT_REQUEST

Network Timeout Request Event.

SL_ZIGBEE_SEND_ORPHAN_NOTIFICATION

Sending Orphan Notification Event.

SL_802154_DATA_POLL_SUPER_RETRY

MAC Data Poll Super Retry Event .


Definition at line 372 of file stack/include/child.h

sl_zigbee_current_stack_tasks#

uint16_t sl_zigbee_current_stack_tasks (void )

Return a bitmask indicating the stack's current tasks.

Parameters
N/A

The mask SL_ZIGBEE_HIGH_PRIORITY_TASKS defines which tasks are high priority. Devices should not sleep if any high priority tasks are active. Active tasks that are not high priority are waiting for messages to arrive from other devices. If there are active tasks, but no high priority ones, the device may sleep but should periodically wake up and call sl_zigbee_poll_for_data() in order to receive messages. Parents will hold messages for SL_ZIGBEE_INDIRECT_TRANSMISSION_TIMEOUT milliseconds before discarding them.

Returns

  • A bitmask of the stack's active tasks.


Definition at line 416 of file stack/include/child.h

sl_zigbee_ok_to_nap#

bool sl_zigbee_ok_to_nap (void )

Indicate whether the stack is currently in a state where there are no high-priority tasks, allowing the device to sleep.

Parameters
N/A

There may be tasks expecting incoming messages, in which case the device should periodically wake up and call sl_zigbee_poll_for_data() in order to receive messages. This function can only be called when the node type is SL_ZIGBEE_SLEEPY_END_DEVICE

Returns

  • True if the application may sleep but the stack may be expecting incoming messages.


Definition at line 430 of file stack/include/child.h

sl_zigbee_parent_token_set#

bool sl_zigbee_parent_token_set (void )

Indicate whether the parent token has been set by association.

Parameters
N/A

Returns

  • True if the parent token has been set.


Definition at line 440 of file stack/include/child.h

sl_zigbee_ok_to_hibernate#

bool sl_zigbee_ok_to_hibernate (void )

Indicate whether the stack currently has any tasks pending.

Parameters
N/A

If no tasks are pending, sl_zigbee_tick() does not need to be called until the next time a stack API function is called. This function can only be called when the node type is SL_ZIGBEE_SLEEPY_END_DEVICE or

Returns

  • True if the application may sleep for as long as it wishes.


Definition at line 451 of file stack/include/child.h

sl_zigbee_ok_to_long_poll#

bool sl_zigbee_ok_to_long_poll (void )

Indicate whether the stack is currently in a state that does not require the application to periodically poll.

Parameters
N/A

Returns

  • True if the application may stop polling periodically.


Definition at line 462 of file stack/include/child.h

sl_zigbee_stack_power_down#

void sl_zigbee_stack_power_down (void )

Immediately turn the radio power completely off.

Parameters
N/A

Calling this function will render all other stack functions except sl_zigbee_stack_power_up() non-functional until the radio is powered back on.


Definition at line 472 of file stack/include/child.h

sl_zigbee_stack_power_up#

void sl_zigbee_stack_power_up (void )

Initialize the radio. Typically called coming out of deep sleep.

Parameters
N/A

For non-sleepy devices, also turns the radio on and leaves it in RX mode.


Definition at line 478 of file stack/include/child.h

sl_zigbee_send_link_power_delta_request#

sl_status_t sl_zigbee_send_link_power_delta_request (void )

Send a link power delta request to the parent.

Parameters
N/A

Definition at line 486 of file stack/include/child.h

sl_zigbee_get_avg_parent_rssi#

int8_t sl_zigbee_get_avg_parent_rssi (void )

Accessor function for recent average RSSI value between this device and the parent (SoC only).

Parameters
N/A

Definition at line 490 of file stack/include/child.h

sl_zigbee_get_parent_id#

sl_802154_short_addr_t sl_zigbee_get_parent_id (void )

Accessor function for the parent's node ID if applicable (SoC only).

Parameters
N/A

Definition at line 494 of file stack/include/child.h

sl_zigbee_set_child_timeout_option_mask#

sl_status_t sl_zigbee_set_child_timeout_option_mask (uint16_t mask)

: Bit mask that decides which timeout values are acceptable for a child. It defaults to 0xFFFF which covers all the following 15 options:

Parameters
N/Amask

#define SECONDS_10 0 #define MINUTES_2 1 #define MINUTES_4 2 #define MINUTES_8 3 #define MINUTES_16 4 #define MINUTES_32 5 #define MINUTES_64 6 #define MINUTES_128 7 #define MINUTES_256 8 #define MINUTES_512 9 #define MINUTES_1024 10 #define MINUTES_2048 11 #define MINUTES_4096 12 #define MINUTES_8192 13 #define MINUTES_16384 14 // ~11 days


Definition at line 516 of file stack/include/child.h

SL_ZIGBEE_HIGH_PRIORITY_TASKS#

#define SL_ZIGBEE_HIGH_PRIORITY_TASKS
Value:
  (SL_ZIGBEE_OUTGOING_MESSAGES | SL_ZIGBEE_INCOMING_MESSAGES | SL_ZIGBEE_RADIO_IS_ON)

A mask of the tasks that prevent a device from sleeping.


Definition at line 400 of file stack/include/child.h

Function Documentation#

sl_zigbee_child_id#

sl_802154_short_addr_t sl_zigbee_child_id (uint8_t childIndex)

Convert a child index to a node ID.

Parameters
N/AchildIndex

The index.

Returns


Definition at line 38 of file stack/include/child.h

sl_zigbee_child_power#

int8_t sl_zigbee_child_power (uint8_t childIndex)

Return radio power value of the child from the given childIndex.

Parameters
N/AchildIndex

The index.

Returns

  • The power of the child or maximum radio power, which is the power value provided by the user while forming/joining a network if there isn't a child at the childIndex specified.


Definition at line 48 of file stack/include/child.h

sl_zigbee_set_child_power#

void sl_zigbee_set_child_power (uint8_t childIndex, int8_t newPower)

Set the radio power value for a given child index.

Parameters
N/AchildIndex

The index.

N/AnewPower

The new power value.


Definition at line 55 of file stack/include/child.h

sl_zigbee_child_index#

uint8_t sl_zigbee_child_index (sl_802154_short_addr_t childId)

Convert a node ID to a child index.

Parameters
N/AchildId

The node ID of the child.

Returns

  • The child index or 0xFF if the node ID does not belong to a child.


Definition at line 63 of file stack/include/child.h

sl_zigbee_get_child_data#

sl_status_t sl_zigbee_get_child_data (uint8_t index, sl_zigbee_child_data_t * childData)

Get the EUI64 and node type of the child at the provided index. If there is no child at 'index', it returns ::SL_STATUS_NOT_JOINED. Possible child indexes run from zero to sl_zigbee_max_child_count() - 1.

Parameters
N/Aindex

The index of the child of interest.

N/AchildData

The child's data is copied here.

Returns

  • Returns ::SL_STATUS_OK if a child is found at that index, ::SL_STATUS_NOT_JOINED if not.


Definition at line 78 of file stack/include/child.h

sl_zigbee_set_child_data#

sl_status_t sl_zigbee_set_child_data (uint8_t index, const sl_zigbee_child_data_t * childData)

Sets the EUI64, node ID, and node type of the child at the provided index in nonvolatile memory. No other data from the childData argument is used or copied. The user is responsible for rebooting the device after calling this API in order to initialize RAM-based child data. Possible child indexes run from zero to sl_zigbee_max_child_count() - 1.

Parameters
N/Aindex

The index of the child.

N/AchildData

The child's data.

Returns

  • Returns ::SL_STATUS_OK if successfully setting child at that index, ::SL_STATUS_INVALID_INDEX if provided index is out of range.

Note

  • This API only sets the child data to nonvolatile memory. A reboot is required after calling this API to read the nonvolatile child data and set it to RAM structures. This API does not set other child RAM data, such as power and timeout values.


Definition at line 99 of file stack/include/child.h

sl_zigbee_child_join_handler#

void sl_zigbee_child_join_handler (uint8_t index, bool joining, sl_802154_short_addr_t childId, sl_802154_long_addr_t childEui64, sl_zigbee_node_type_t childType)

Called by the stack when a child joins or leaves. 'Joining' is true if the child is joining and false if leaving.

Parameters
N/Aindex

The index of the child of interest.

N/Ajoining

True if the child is joining, false if the child is leaving.

N/AchildId

Node ID of the child.

N/AchildEui64

The EUI64 of the child.

N/AchildType

Node type of the child.

The index is the same as the value that should be passed to sl_zigbee_get_child_data() to get this child's data. Note that if the child is leaving, sl_zigbee_get_child_data() will return ::SL_STATUS_NOT_JOINED if called with this index. If the application includes sl_zigbee_child_join_handler(), it must define SL_ZIGBEE_APPLICATION_HAS_CHILD_JOIN_HANDLER in its CONFIGURATION_HEADER


Definition at line 123 of file stack/include/child.h

sl_zigbee_set_keep_alive_mode#

sl_status_t sl_zigbee_set_keep_alive_mode (sl_zigbee_keep_alive_mode_t mode)
Parameters
N/Amode

One of the four configurations in the sl_zigbee_keep_alive_mode_t.

@ brief Set the keep alive mode.


Definition at line 135 of file stack/include/child.h

sl_zigbee_get_keep_alive_mode#

sl_zigbee_keep_alive_mode_t sl_zigbee_get_keep_alive_mode (void )
Parameters
N/A

@ brief Get the keep alive mode.

Returns

  • mode One of the four configurations in the sl_zigbee_keep_alive_mode_t.


Definition at line 143 of file stack/include/child.h

sl_zigbee_poll_for_data#

sl_status_t sl_zigbee_poll_for_data (void )

Request any pending data from the parent node. This function allows an end device to query its parent for any pending data.

Parameters
N/A

End devices must call this function periodically to maintain contact with their parent. The parent will remove a child if it has not received a poll from it within the configured timeout.

If the end device has lost contact with its parent, sl_zigbee_poll_for_data() calls ::emberRejoinNetwork(true) and returns ::SL_STATUS_FAIL.

The default values for the timeouts are set in config/sl_zigbee_configuration_defaults.h and can be overridden in the application's configuration header.

Returns

  • An sl_status_t value:

    • ::SL_STATUS_OK - The poll message has been submitted for transmission.

    • ::SL_STATUS_INVALID_STATE - The node is not an end device.

    • ::SL_STATUS_NOT_JOINED - The node is not part of a network.

    • ::SL_STATUS_MAC_TRANSMIT_QUEUE_FULL - The MAC layer transmit queue is full.

    • ::SL_STATUS_ALLOCATION_FAILED - No buffers available to create the data poll message.

    • ::SL_STATUS_FAIL - Too much time has elapsed since the last successful poll. A rejoin attempt has been initiated. This error is not "fatal". The command can be retried until successful.


Definition at line 170 of file stack/include/child.h

sl_zigbee_set_mac_poll_failure_wait_time#

void sl_zigbee_set_mac_poll_failure_wait_time (uint32_t waitBeforeRetryIntervalMs)
Parameters
N/AwaitBeforeRetryIntervalMs

Time in milliseconds the device waits before retrying a data poll when a MAC level data poll fails for any reason. The retry feature can be disabled by setting this value to zero.

@ brief Set the retry interval (in milliseconds) for mac data poll. This function is useful for sleepy end devices. The retry interval is the time in milliseconds the device waits before retrying a data poll when a MAC level data poll fails for any reason. The retry feature can be disabled by setting the retry interval to zero.


Definition at line 186 of file stack/include/child.h

sl_zigbee_poll_complete_handler#

void sl_zigbee_poll_complete_handler (sl_status_t status)
Parameters
N/Astatus

An sl_status_t value:

  • ::SL_STATUS_OK - Data was received in response to the poll.

  • ::SL_STATUS_MAC_NO_DATA - No data was pending.

  • ::SL_STATUS_CCA_FAILURE - The poll message could not be sent over the air.

  • ::SL_STATUS_MAC_NO_ACK_RECEIVED - The poll message was sent but not acknowledged by the parent.

@ brief Called by the stack when a data poll to the parent is complete.

If the application includes sl_zigbee_poll_complete_handler(), it must define SL_ZIGBEE_APPLICATION_HAS_POLL_COMPLETE_HANDLER within its CONFIGURATION_HEADER


Definition at line 203 of file stack/include/child.h

sl_zigbee_set_message_flag#

sl_status_t sl_zigbee_set_message_flag (sl_802154_short_addr_t childId)

Set a flag to indicate that a message is pending for a child. The next time that the child polls, it will be informed that it has a pending message. The message is sent from sl_zigbee_poll_handler, which is called when the child requests data.

Parameters
N/AchildId

The ID of the child that just polled for data.

Returns

  • An ::sl_status_t value.

    • ::SL_STATUS_OK - The next time that the child polls, it will be informed that it has pending data.

    • ::SL_STATUS_NOT_JOINED - The child identified by childId is not our child.


Definition at line 217 of file stack/include/child.h

sl_zigbee_clear_message_flag#

sl_status_t sl_zigbee_clear_message_flag (sl_802154_short_addr_t childId)

Clear a flag to indicate that there are no more messages for a child. The next time the child polls, it will be informed that it does not have any pending messages.

Parameters
N/AchildId

The ID of the child that no longer has pending messages.

Returns

  • An ::sl_status_t value.

    • ::SL_STATUS_OK - The next time that the child polls, it will be informed that it does not have any pending messages.

    • ::SL_STATUS_NOT_JOINED - The child identified by childId is not our child.


Definition at line 230 of file stack/include/child.h

sl_zigbee_poll_handler#

void sl_zigbee_poll_handler (sl_802154_short_addr_t childId, bool transmitExpected)

Called to allow the application to send a message in response to a poll from a child.

Parameters
N/AchildId

The ID of the child that is requesting data.

N/AtransmitExpected

True if the child is expecting an application- supplied data message. False otherwise.

This function is called when a child polls, provided that the pending message flag is set for that child (see sl_zigbee_set_message_flag(). The message should be sent to the child using sl_zigbee_send_unicast() with the SL_ZIGBEE_APS_OPTION_POLL_RESPONSE option.

If the application includes ::emberPollHanlder(), it must define SL_ZIGBEE_APPLICATION_HAS_POLL_HANDLER in its CONFIGURATION_HEADER.


Definition at line 249 of file stack/include/child.h

sl_zigbee_add_child#

sl_status_t sl_zigbee_add_child (sl_802154_short_addr_t shortId, sl_802154_long_addr_t longId, sl_zigbee_node_type_t nodeType)

Add a child to the child/neighbor table only on SoC, allowing direct manipulation of these tables by the application. This can affect the network functionality, and needs to be used wisely. If used appropriately, the application can maintain more than the maximum of children provided by the stack.

Parameters
N/AshortId

The preferred short ID of the node.

N/AlongId

The long ID of the node.

N/AnodeType

The nodetype e.g., SL_ZIGBEE_ROUTER defining, if this would be added to the child table or neighbor table.

Returns

  • An ::sl_status_t value.

    • ::SL_STATUS_OK - This node has been successfully added.

    • ::SL_STATUS_FAIL - The child was not added to the child/neighbor table.


Definition at line 268 of file stack/include/child.h

sl_zigbee_remove_child#

sl_status_t sl_zigbee_remove_child (sl_802154_long_addr_t childEui64)

Remove a node from child/neighbor table only on SoC, allowing direct manipulation of these tables by the application. This can affect the network functionality, and needs to be used wisely.

Parameters
N/AchildEui64

The long ID of the node.

Returns

  • An ::sl_status_t value.

    • ::SL_STATUS_OK - This node has been successfully removed.

    • ::SL_STATUS_FAIL - The node was not found in either of the child or neighbor tables.


Definition at line 282 of file stack/include/child.h

sl_zigbee_remove_neighbor#

void sl_zigbee_remove_neighbor (sl_802154_short_addr_t shortId, sl_802154_long_addr_t longId)

Remove a neighbor from neighbor table only on SoC, allowing direct manipulation of neighbor table by the application. This can affect the network functionality, and needs to be used wisely.

Parameters
N/AshortId

The short ID of the neighbor.

N/AlongId

The long ID of the neighbor.


Definition at line 293 of file stack/include/child.h

sl_zigbee_child_count#

uint8_t sl_zigbee_child_count (void )

Return the number of children the node currently has.

Parameters
N/A

Returns

  • The number of children.


Definition at line 301 of file stack/include/child.h

sl_zigbee_router_child_count#

uint8_t sl_zigbee_router_child_count (void )

Return the number of router children that the node currently has.

Parameters
N/A

Returns

  • The number of router children.


Definition at line 308 of file stack/include/child.h

sl_zigbee_max_child_count#

uint8_t sl_zigbee_max_child_count (void )

Return the maximum number of children for this node. The return value is undefined for nodes that are not joined to a network.

Parameters
N/A

Returns

  • The maximum number of children.


Definition at line 315 of file stack/include/child.h

sl_zigbee_max_router_child_count#

uint8_t sl_zigbee_max_router_child_count (void )

Return the maximum number of router children for this node. The return value is undefined for nodes that are not joined to a network.

Parameters
N/A

Returns

  • The maximum number of router children.


Definition at line 322 of file stack/include/child.h

sl_zigbee_get_parent_node_id#

sl_802154_short_addr_t sl_zigbee_get_parent_node_id (void )

Return the parent's node ID. The return value is undefined for nodes without parents (coordinators and nodes that are not joined to a network).

Parameters
N/A

Returns

  • The parent's node ID.


Definition at line 330 of file stack/include/child.h

sl_zigbee_get_parent_eui64#

sl_802154_long_addr_t sl_zigbee_get_parent_eui64 (void )

Return the parent's EUI64. The return value is undefined for nodes without parents (coordinators and nodes that are not joined to a network).

Parameters
N/A

Returns

  • The parent's EUI64.


Definition at line 338 of file stack/include/child.h