This structure contains information about child nodes.

Public Attributes#

sl_802154_long_addr_t
sl_802154_short_addr_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

eui64#

sl_802154_long_addr_t sl_zigbee_child_data_t::eui64

Definition at line 1340 of file stack/include/sl_zigbee_types.h

type#

sl_zigbee_node_type_t sl_zigbee_child_data_t::type

Definition at line 1341 of file stack/include/sl_zigbee_types.h

id#

sl_802154_short_addr_t sl_zigbee_child_data_t::id

Definition at line 1342 of file stack/include/sl_zigbee_types.h

phy#

uint8_t sl_zigbee_child_data_t::phy

Definition at line 1343 of file stack/include/sl_zigbee_types.h

power#

uint8_t sl_zigbee_child_data_t::power

Definition at line 1344 of file stack/include/sl_zigbee_types.h

timeout#

uint8_t sl_zigbee_child_data_t::timeout

Definition at line 1345 of file stack/include/sl_zigbee_types.h

remainingTimeout#

uint32_t sl_zigbee_child_data_t::remainingTimeout

Definition at line 1346 of file stack/include/sl_zigbee_types.h