Public Attributes#

uint32_t
uint16_t

Public Attribute Documentation#

bitmask#

uint32_t sl_zigbee_tok_type_stack_zll_data_t::bitmask

Definition at line 276 of file stack/include/zll-types.h

freeNodeIdMin#

uint16_t sl_zigbee_tok_type_stack_zll_data_t::freeNodeIdMin

Definition at line 277 of file stack/include/zll-types.h

freeNodeIdMax#

uint16_t sl_zigbee_tok_type_stack_zll_data_t::freeNodeIdMax

Definition at line 278 of file stack/include/zll-types.h

myGroupIdMin#

uint16_t sl_zigbee_tok_type_stack_zll_data_t::myGroupIdMin

Definition at line 279 of file stack/include/zll-types.h

freeGroupIdMin#

uint16_t sl_zigbee_tok_type_stack_zll_data_t::freeGroupIdMin

Definition at line 280 of file stack/include/zll-types.h

freeGroupIdMax#

uint16_t sl_zigbee_tok_type_stack_zll_data_t::freeGroupIdMax

Definition at line 281 of file stack/include/zll-types.h

rssiCorrection#

uint8_t sl_zigbee_tok_type_stack_zll_data_t::rssiCorrection

Definition at line 282 of file stack/include/zll-types.h