Command Class Firmware Update - Firmware targets#
Command Class Firmware Update - Firmware targets.
Macros#
#define
Number of firmware targets <0..10:1>
Macro Definition Documentation#
ZAF_CONFIG_FIRMWARE_TARGET_COUNT#
#define ZAF_CONFIG_FIRMWARE_TARGET_COUNTValue:
1
Number of firmware targets <0..10:1>
Defines the number of supported firmware targets. Setting this number to more than 1 requires the application to implement CC_Version_GetFirmwareVersion_handler(). The default value is 1 because firmware target 0 is the Z-Wave application firmware (including Z-Wave stack).
Definition at line
61
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/configuration/config/zaf_config.h