ColorSwitch#
Modules#
Enumerations#
enum
ECOLORCOMPONENT_WARM_WHITE
ECOLORCOMPONENT_COLD_WHITE
ECOLORCOMPONENT_RED
ECOLORCOMPONENT_GREEN
ECOLORCOMPONENT_BLUE
ECOLORCOMPONENT_AMBER
ECOLORCOMPONENT_CYAN
ECOLORCOMPONENT_PURPLE
ECOLORCOMPONENT_COLOR_UNDEFINED
}
Defined Color Components ID.
Typedefs#
typedef enum EColorComponents_
Defined Color Components ID.
typedef struct colorComponent_
Structure that holds Color Switch CC related data.
Functions#
void
Can be used as single cb function for all colors.
void
cc_color_switch_cb(s_colorComponent *colorComponent)
uint8_t
uint8_t
bool
cc_color_switch_write(uint8_t color_component_id, s_colorComponent *color_component)
bool
cc_color_switch_read(uint8_t color_component_id, s_colorComponent *color_component)
Enumeration Documentation#
EColorComponents_#
EColorComponents_
Defined Color Components ID.
Enumerator | |
---|---|
ECOLORCOMPONENT_WARM_WHITE | ECOLORCOMPONENT_WARM_WHITE. |
ECOLORCOMPONENT_COLD_WHITE | ECOLORCOMPONENT_COLD_WHITE. |
ECOLORCOMPONENT_RED | ECOLORCOMPONENT_RED. |
ECOLORCOMPONENT_GREEN | ECOLORCOMPONENT_GREEN. |
ECOLORCOMPONENT_BLUE | ECOLORCOMPONENT_BLUE. |
ECOLORCOMPONENT_AMBER | ECOLORCOMPONENT_AMBER. |
ECOLORCOMPONENT_CYAN | ECOLORCOMPONENT_CYAN (For 6ch color mixing) |
ECOLORCOMPONENT_PURPLE | ECOLORCOMPONENT_PURPLE (For 6ch color mixing) |
ECOLORCOMPONENT_COLOR_UNDEFINED |
Definition at line
23
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/inc/CC_ColorSwitch.h
Typedef Documentation#
EColorComponents#
typedef enum EColorComponents_ EColorComponents
Defined Color Components ID.
Definition at line
34
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/inc/CC_ColorSwitch.h
s_colorComponent#
typedef struct colorComponent_ s_colorComponent
Structure that holds Color Switch CC related data.
Definition at line
48
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/inc/CC_ColorSwitch.h
Function Documentation#
cc_color_switch_refresh_cb#
void cc_color_switch_refresh_cb (void )
Can be used as single cb function for all colors.
Parameters
N/A |
Defined in the app. Called when change takes place in driver and app needs to update LED status
Definition at line
55
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/inc/CC_ColorSwitch.h
cc_color_switch_cb#
void cc_color_switch_cb (s_colorComponent * colorComponent)
Parameters
N/A | colorComponent |
Definition at line
19
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/src/cc_color_switch_config_api.h
cc_color_switch_get_colorComponents#
s_colorComponent * cc_color_switch_get_colorComponents (void )
Parameters
N/A |
Definition at line
20
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/src/cc_color_switch_config_api.h
cc_color_switch_get_length_colorComponents#
uint8_t cc_color_switch_get_length_colorComponents (void )
Parameters
N/A |
Definition at line
21
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/src/cc_color_switch_config_api.h
cc_color_switch_get_default_duration#
uint8_t cc_color_switch_get_default_duration (void )
Parameters
N/A |
Definition at line
22
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/src/cc_color_switch_config_api.h
cc_color_switch_write#
bool cc_color_switch_write (uint8_t color_component_id, s_colorComponent * color_component)
Parameters
N/A | color_component_id | |
N/A | color_component |
Definition at line
19
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/src/cc_color_switch_io.h
cc_color_switch_read#
bool cc_color_switch_read (uint8_t color_component_id, s_colorComponent * color_component)
Parameters
N/A | color_component_id | |
N/A | color_component |
Definition at line
20
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/src/cc_color_switch_io.h