Zpal-uart#
Defines a platform abstraction layer for the Z-Wave UART.
How to use the UART API
The ZPAL UART API is used by only SerialAPI application, all functions are required.
The following outlines an example of use:
To initialize UART interface, invoke zpal_uart_init().
Enable UART by invoking zpal_uart_enable().
Invoke zpal_uart_transmit() to send data.
Use zpal_uart_transmit_in_progress() to check if transmission is in progress.
To get number of bytes available for reading, invoke zpal_uart_get_available().
Read received data with zpal_uart_receive().
Requirements:
This interface must implement a non-blocking behavior.
Transmit and receive buffers are provided by application.
Transmit and receive buffers should be at least 200 bytes large.
Modules#
Enumerations#
IDs for each of the parity mode.
IDs for each of the stop bits configuration.
Typedefs#
UART handle type.
Defines a type for the UART receive callback that is invoked whenever data is ready.
Defines a type for the UART transmit done callback that is invoked when data has been transmitted.
Functions#
Initializes a UART based on the given configuration.
Enables a given UART.
Disables a given UART.
Transmits data using a given UART.
Returns whether transmission is in progress.
Get the number of bytes ready for reading.
Receive available data into buffer using a given UART.
Macros#
Set this flag in the configuration if the UART must be configured as a blocking UART.
Enumeration Documentation#
zpal_uart_id_t#
zpal_uart_id_t
IDs for each of the UARTs.
Enumerator | |
---|---|
ZPAL_UART0 | |
ZPAL_UART1 |
63
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
zpal_uart_parity_bit_t#
zpal_uart_parity_bit_t
IDs for each of the parity mode.
Enumerator | |
---|---|
ZPAL_UART_NO_PARITY | No parity. |
ZPAL_UART_EVEN_PARITY | Even parity. |
ZPAL_UART_ODD_PARITY | Odd parity. |
72
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
zpal_uart_stop_bits_t#
zpal_uart_stop_bits_t
IDs for each of the stop bits configuration.
Enumerator | |
---|---|
ZPAL_UART_STOP_BITS_0P5 | 0.5 stop bits. |
ZPAL_UART_STOP_BITS_1 | 1 stop bits. |
ZPAL_UART_STOP_BITS_1P5 | 1.5 stop bits. |
ZPAL_UART_STOP_BITS_2 | 2 stop bits. |
82
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
Typedef Documentation#
zpal_uart_handle_t#
typedef void* zpal_uart_handle_t
UART handle type.
93
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
zpal_uart_receive_callback_t#
typedef void(* zpal_uart_receive_callback_t) (zpal_uart_handle_t handle, size_t length) )(zpal_uart_handle_t handle, size_t length)
Defines a type for the UART receive callback that is invoked whenever data is ready.
[in] | handle | UART handle. |
[in] | length | Length of available data in bytes. |
101
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
zpal_uart_transmit_done_t#
typedef void(* zpal_uart_transmit_done_t) (zpal_uart_handle_t handle) )(zpal_uart_handle_t handle)
Defines a type for the UART transmit done callback that is invoked when data has been transmitted.
[in] | handle | UART handle. |
108
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
Function Documentation#
zpal_uart_init#
zpal_status_t zpal_uart_init (const zpal_uart_config_t * config, zpal_uart_handle_t * handle)
Initializes a UART based on the given configuration.
[in] | config | Pointer to UART configuration. |
[out] | handle | Outputs a handle to a UART. |
Returns
ZPAL_STATUS_OK on success and ZPAL_STATUS_FAIL otherwise.
135
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
zpal_uart_enable#
zpal_status_t zpal_uart_enable (zpal_uart_handle_t handle)
Enables a given UART.
[in] | handle | UART handle. |
Returns
ZPAL_STATUS_OK on success and ZPAL_STATUS_FAIL otherwise.
143
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
zpal_uart_disable#
zpal_status_t zpal_uart_disable (zpal_uart_handle_t handle)
Disables a given UART.
[in] | handle | UART handle. |
Returns
ZPAL_STATUS_OK on success and ZPAL_STATUS_FAIL otherwise.
151
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
zpal_uart_transmit#
zpal_status_t zpal_uart_transmit (zpal_uart_handle_t handle, const uint8_t * data, size_t length, zpal_uart_transmit_done_t tx_cb)
Transmits data using a given UART.
[in] | handle | UART handle. |
[in] | data | Pointer to data. |
[in] | length | Length of data. |
[in] | tx_cb | Transmission done callback. |
Returns
ZPAL_STATUS_OK if transmission has started, ZPAL_STATUS_FAIL otherwise.
Note
Expect
tx_cb
callback to be invoked in interrupt context.This function will block if length of data exceeds internal transmit buffer.
166
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
zpal_uart_transmit_in_progress#
bool zpal_uart_transmit_in_progress (zpal_uart_handle_t handle)
Returns whether transmission is in progress.
[in] | handle | UART handle. |
Returns
True if transmission is in progress, false otherwise.
175
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
zpal_uart_get_available#
size_t zpal_uart_get_available (zpal_uart_handle_t handle)
Get the number of bytes ready for reading.
[in] | handle | UART handle. |
Returns
Number of bytes in the receive buffer available for reading with zpal_uart_receive
184
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
zpal_uart_receive#
size_t zpal_uart_receive (zpal_uart_handle_t handle, uint8_t * data, size_t length)
Receive available data into buffer using a given UART.
[in] | handle | UART handle. |
[out] | data | The data buffer to receive into |
[in] | length | the maximum number of bytes we'd like to read |
Returns
Number of bytes received into buffer
194
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h
Macro Definition Documentation#
ZPAL_UART_CONFIG_FLAG_BLOCKING#
#define ZPAL_UART_CONFIG_FLAG_BLOCKINGValue:
(1 << 1)
Set this flag in the configuration if the UART must be configured as a blocking UART.
Example of use:
zpal_uart_config_t config = {
.flags = ZPAL_UART_CONFIG_FLAG_BLOCKING
}
58
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_uart.h