Struct used to pass operational data to TSE module.
Public Attributes#
rxOptions
uint8_t
uint8_t *
index of notification in notifications array
uint8_t
Pointer to event parameters.
Public Attribute Documentation#
rxOptions#
RECEIVE_OPTIONS_TYPE_EX s_CC_notification_data_t_::rxOptions
rxOptions
Definition at line
67
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/CC_Notification.h
index#
uint8_t s_CC_notification_data_t_::index
Definition at line
68
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/CC_Notification.h
pEventParameters#
uint8_t* s_CC_notification_data_t_::pEventParameters
index of notification in notifications array
Definition at line
69
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/CC_Notification.h
eventParamLength#
uint8_t s_CC_notification_data_t_::eventParamLength
Pointer to event parameters.
Definition at line
70
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/CC_Notification.h