Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

S2_groupID#

uint8_t _TRANSMIT_OPTIONS_TYPE_EX_::S2_groupID

Definition at line 75 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZW_TransportEndpoint.h

txOptions#

uint8_t _TRANSMIT_OPTIONS_TYPE_EX_::txOptions

Definition at line 76 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZW_TransportEndpoint.h

sourceEndpoint#

uint8_t _TRANSMIT_OPTIONS_TYPE_EX_::sourceEndpoint

Definition at line 77 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZW_TransportEndpoint.h

pList#

MULTICHAN_NODE_ID* _TRANSMIT_OPTIONS_TYPE_EX_::pList

Definition at line 78 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZW_TransportEndpoint.h

list_length#

uint8_t _TRANSMIT_OPTIONS_TYPE_EX_::list_length

Definition at line 79 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZW_TransportEndpoint.h