Can be used for pairing a command class with a specific command in the command class.

Public Attributes#

uint8_t

Command class.

uint8_t

Command.

Public Attribute Documentation#

cmdClass#

uint8_t ccc_pair_t::cmdClass

Command class.


Definition at line 117 of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

cmd#

uint8_t ccc_pair_t::cmd

Command.


Definition at line 118 of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h