Structure with radio parameters for a received frame.
Public Attributes#
Speed for the frame received.
Channel id on which the frame was received.
Z-Wave Header format used in channel frame was received on.
int8_t
Rssi value.
Public Attribute Documentation#
speed#
zpal_radio_speed_t zpal_radio_rx_parameters_t::speed
Speed for the frame received.
Definition at line
410
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
channel_id#
zpal_radio_zwave_channel_t zpal_radio_rx_parameters_t::channel_id
Channel id on which the frame was received.
Definition at line
411
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
channel_header_format#
zpal_radio_header_type_t zpal_radio_rx_parameters_t::channel_header_format
Z-Wave Header format used in channel frame was received on.
Definition at line
412
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
rssi#
int8_t zpal_radio_rx_parameters_t::rssi
Rssi value.
Definition at line
413
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h