BGX Framework

The Silicon Labs BGX device provides a bridge between Bluetooth Low Energy (BLE) and Serial communication. More...

Classes

protocol <BGXpressDelegate >
Delegate class for the BGXpressManager object. More...
class BGXpressManager
This class is used to interact with a BGX device. More...

Enumerations

enum ConnectionState {
DISCONNECTED , SCANNING , CONNECTING , INTERROGATING ,
CONNECTED , DISCONNECTING , CONNECTIONTIMEDOUT
}
Possible values for the connection state of the BGXpressManager . More...
enum BusMode {
UNKNOWN_MODE , STREAM_MODE , LOCAL_COMMAND_MODE , REMOTE_COMMAND_MODE ,
UNSUPPORTED_MODE
}
Values of the bus mode. More...

Variables

NSErrorDomain NSBGXErrorDomain
The NSBGXErrorDomain is used as an error domain for NSError objects passed by BGXpress.framework. More...

Detailed Description

The Silicon Labs BGX device provides a bridge between Bluetooth Low Energy (BLE) and Serial communication.

BGXpress.framework makes it easier to write an iOS app that interacts with BGX. It supports discovery of BGX devices, connecting and disconnecting, setting and detecting the bus mode of the BGX, sending and receiving data, and OTA (Over The Air) Firmware Updates of the BGX accessed through the Silicon Labs DMS (Device Management Service).

Remarks
BGXpress.framework is designed for use with iOS.
BGXpress.framework is currently designed for connecting to one BGX at a time.

Class Documentation

◆ BGXpressDelegate

protocol BGXpressDelegate

Delegate class for the BGXpressManager object.

Your application should supply an object conforming to the BGXpressDelegate protocol which has a lifecycle similar to the instance of BGXpressManager you create. The BGXCommander example app uses the AppDelegate for this purpose. The various methods in this protocol are called in order to indicate changes to the Bluetooth state, ConnectionState, BusMode, when devices are discovered, when data is read or data is written.

Inherits <NSObject>.

Instance Methods

(void) - connectionStateChanged:
Detect connection state changes. More...
(void) - busModeChanged:
Detect bus mode changes. More...
(void) - dataRead:
Delegate method is called when data is received. More...
(void) - dataWritten
Delegate method used to advise that the data has been written. More...
(void) - deviceDiscovered
Delegate method called when a device is discovered. More...
(void) - bluetoothStateChanged:
Notify application about bluetooth state changes. More...

Method Documentation

◆ connectionStateChanged:()

- (void BGXpressDelegate) connectionStateChanged: ( ConnectionState ) newConnectionState
required

Detect connection state changes.

Delegate method advising when the connection state has changed and the new connection state

Parameters
newConnectionState ConnectionState of the current connection

◆ busModeChanged:()

- (void BGXpressDelegate) busModeChanged: ( BusMode ) newBusMode
required

Detect bus mode changes.

Delegate method called when the bus mode changes or is read. If you call the BGXpressManager method -(BOOL)readBusMode, this delegate will be called with the bus mode that was read whether or not it was different than the previous bus mode.

Parameters
newBusMode the new bus mode for the connection

◆ dataRead:()

- (void BGXpressDelegate) dataRead: (NSData *) newData
required

Delegate method is called when data is received.

Parameters
newData updated values

◆ dataWritten()

- (void BGXpressDelegate) dataWritten
required

Delegate method used to advise that the data has been written.

◆ deviceDiscovered()

- (void BGXpressDelegate) deviceDiscovered
required

Delegate method called when a device is discovered.

Check the devicesDiscovered property of BGXpressManager for the list of device that have been discovered.

◆ bluetoothStateChanged:()

- (void BGXpressDelegate) bluetoothStateChanged: (CBManagerState) state
optional

Notify application about bluetooth state changes.

Passes the notifications from the CBManager through so that the calling app will know when to start/stop scanning (you get an error when you start scanning before you we get the bluetooth state change notification saying that bluetooth is on which seems like a flaw in the design of this API).

Parameters
state The state of the CBManager which in theory the calling application shouldn't have to know about.

◆ BGXpressManager

class BGXpressManager

This class is used to interact with a BGX device.

Create one of these objects in your application and store it in a place where it will be retained while your application is running. The BGXCommander example app uses the AppDelegate class to store an instance of the BGXpressManager class. Your app should do this or something that is equivalent. We recommend against storing it as a property of a UIViewController instance because view controllers may be created and destroyed during the lifecycle of your app.

Remarks
Most of the methods of this class are asynchronous. To determine that an operation has occurred, rely on the BGXpressDelegate.
Operations may fail because of an incompatible state of this object (e.g. connectToDevice:), or the state of the Bluetooth hardware (e.g. startScan).

Inherits NSObject, <CBCentralManagerDelegate>, and <CBPeripheralDelegate>.

Instance Methods

(BOOL) - startScan
Call this method to start scanning for devices. More...
(BOOL) - stopScan
Call this method to stop scanning for devices. More...
(BOOL) - connectToDevice:
Method to connect to a device. More...
(BOOL) - disconnect
Method used to disconnect from a device. More...
(BOOL) - readBusMode
Method used to read the BusMode for a device eg Stream, Local or Remote commands. More...
(BOOL) - writeBusMode:
Method used to write new bus mode for device. More...
(BOOL) - canWrite
Method to see if you can write to the device. More...
(BOOL) - writeData:
Method used to write data to a device. More...
(BOOL) - writeString:
Method used to write a string to device. More...
(BOOL) - sendCommand:args:
Method used to send commands to the device. More...
(NSString *) - device_unique_id
Returns the device unique id. More...

Class Methods

(NSString *) + uniqueIDForPeripheral:
Get the unique ID for the specified peripheral. More...

Properties

id< BGXpressDelegate > delegate
NSString * modelNumber
NSMutableArray * devicesDiscovered
ConnectionState connectionState
BusMode busMode

Method Documentation

◆ startScan()

- (BOOL) startScan

Call this method to start scanning for devices.

Returns
Boolean value to indicate if scanning will start.
Remarks
Calling this method will clear the contents of the devicesDiscovered mutable array property.

◆ stopScan()

- (BOOL) stopScan

Call this method to stop scanning for devices.

Returns
Boolean value to indicate if scanning will stop.

◆ connectToDevice:()

- (BOOL) connectToDevice: (NSString *) deviceName

Method to connect to a device.

Parameters
deviceName The name of the device you wish to connect to
Returns
Boolean value to indicate if there has been a successful connection to the device

◆ disconnect()

- (BOOL) disconnect

Method used to disconnect from a device.

◆ readBusMode()

- (BOOL) readBusMode

Method used to read the BusMode for a device eg Stream, Local or Remote commands.

Returns
Boolean value, FALSE if not connected else TRUE.

◆ writeBusMode:()

- (BOOL) writeBusMode: ( BusMode ) newBusMode

Method used to write new bus mode for device.

Parameters
newBusMode The new BusMode for the device
Returns
Boolean value, FALSE if not connected or BusMode not changed. TRUE if BusMode written.

◆ canWrite()

- (BOOL) canWrite

Method to see if you can write to the device.

Returns
Boolean value, TRUE if device is connected and no data waiting to be written to the device, else FALSE.

◆ writeData:()

- (BOOL) writeData: (NSData *) data

Method used to write data to a device.

Parameters
data Data to be writted to device.
Returns
Boolean value advising if the data has been written to the device or not.

◆ writeString:()

- (BOOL) writeString: (NSString *) string

Method used to write a string to device.

Parameters
string String value to be writted to device.
Returns
Boolean value advising if the string has been written to the device or not.

◆ sendCommand:args:()

- (BOOL) sendCommand: (NSString *) command
args: (NSString *) args

Method used to send commands to the device.

Parameters
command Command
args Arguments
Returns
Boolean value advising if the command has been written to the device or not.

◆ device_unique_id()

- (NSString *) device_unique_id

Returns the device unique id.

Returns
NSString with the unique id of the device. Nil on error.

◆ uniqueIDForPeripheral:()

+ (NSString *) uniqueIDForPeripheral: (CBPeripheral *) peripheral

Get the unique ID for the specified peripheral.

Parameters
peripheral the peripheral to be read.

This call assumes that the services and characteristics have been discovered and that the device id characteristic has already been read once.

Returns
NSString with the unique id of the device. Nil on error.

Property Documentation

◆ delegate

- (id<BGXpressDelegate>) delegate
read write nonatomic weak

◆ modelNumber

- (NSString*) modelNumber
read write nonatomic strong

◆ devicesDiscovered

- (NSMutableArray*) devicesDiscovered
read write nonatomic strong

◆ connectionState

- ( ConnectionState ) connectionState
read write nonatomic assign

◆ busMode

- ( BusMode ) busMode
read write nonatomic assign

Enumeration Type Documentation

◆ ConnectionState

Possible values for the connection state of the BGXpressManager .

Enumerator
DISCONNECTED

The BGXpressManager is not connected to any BGX device and is not scanning.

SCANNING

The BGXpressManager is scanning for BGX devices.

CONNECTING

The BGXpressManager is connecting to a BGX device.

INTERROGATING

The BGXpressManager has connected to a BGX device and is discovering bluetooth services and characteristics.

CONNECTED

The BGXpressManager is connected to a BGX device.

DISCONNECTING

The BGXpressManager is in the process of disconnecting from a BGX device.

CONNECTIONTIMEDOUT

A connection that was in progress has timed out.

◆ BusMode

Values of the bus mode.

Enumerator
UNKNOWN_MODE

an invalid mode used to indicate that the mode has not been determined

STREAM_MODE

send and receive serial data to the device to which the BGX is connected

LOCAL_COMMAND_MODE

data received over the serial lines is processed as a command by the BGX and results returned over the serial lines

REMOTE_COMMAND_MODE

data received over bluetooth is processed as a command by the BGX and results returned over bluetooth

UNSUPPORTED_MODE

an invalid mode state

Variable Documentation

◆ NSBGXErrorDomain

NSErrorDomain NSBGXErrorDomain

The NSBGXErrorDomain is used as an error domain for NSError objects passed by BGXpress.framework.