Modules
Here is a list of all modules:
| BGX Framework | The Silicon Labs BGX device provides a bridge between Bluetooth Low Energy (BLE) and Serial communication |
| BGX DMS | The BGX DMS module is used for interacting with the Silicon Labs Device Management Service (DMS) in order to get a list of firmware versions that are available for your BGX device and to download firmware images |
| BGX OTA Update | Bgx_ota_update contains a class ( BGX_OTA_Updater ) and other datatypes that are used to perform an OTA update operation (i.e |
| Safe Type |
SafeType is a convienient way to verify that an
NSObject
passed using id is the expected type when assigning the value to a pointer of a specific Objective-C type
|