BGXpress Framework Usage
Using BGXpress.framework
Adding BGXpress to your Xcode project
Add bgxpress.xcodeproj to your app's workspace file. Next, select your app in the Project Navigator in Xcode. Switch to Build Phases and add BGXpress to the list of target dependencies. Then add a new copy files build phase, choose Frameworks as the destination, and add BGXpress.framework to the build phase. This will allow BGXpress.framework to be built as needed and copied into your app bundle.
Including the bgxpress header file
In order to use the BGXpress.framework, you should include the following line:
#import <bgxpress/bgxpress.h>
Using the BGXpressManager class
The
BGXpressManager
class is used to interact with a BGX device. Create one of these objects in your application and store it in a place where it will be retained while your application is running. The BGXCommander app uses the
AppDelegate
class to store an instance of the
BGXpressManager
class. Your app should do this or something that is equivalent. We recommend against using it in a
UIViewController
instance because those objects may be created and destroyed during the lifecycle of your app.
self.bgxManager = [[BSXpressManager alloc] init];
Creating a BGXpressDelegate
Your application should supply an object conforming to the
BGXpressDelegate
protocol which has a lifecycle similar to the instance of
BGXpressManager
you create. The BGXCommander app uses the
AppDelegate
for this purpose. The file BGXpress.h declares this protocol. The various methods in this protocol are called in order to indicate changes to the Bluetooth state,
ConnectionState
,
BusMode
. It is called when devices are discovered, data is read or data is written.
@interface MyDelegate :
NSObject
<BGXpressDelegate>
self.myDelegate = [[MyDelegate alloc] init];
self.bgxManager.delegate = self.myDelegate;
Device Discovery
To discover devices you must wait until the Bluetooth state is
CBManagerStatePoweredOn
. You can detect this by implementing the method
-(void)bluetoothStateChanged:(CBManagerState)state
in your
BGXpressDelegate
class. After you have received this notification, call:
[self.bgxManager startScan];
As BGX devices are discovered, the
-(void)deviceDiscovered
method is called. When this happens, you can access the list of devices using the
devicesDiscovered
property of your
BGXpressManager
instance.
When you wish to stop scanning call:
[self.bgxManager stopScan];
Note that if BGX devices are turned off or move out of range they are not automatically removed from the
discoveredDevices
array. When you call startScan, the
discoveredDevices
array is emptied of devices. One way to ensure that your list of devices is not stale is to periodically stop scanning and the scan again.
Connecting to a BGX
To connect to a specific BGX device, call the
BGXpressManager
method
- (BOOL)connectToDevice:(NSString *)deviceName
using the device name. The call will return
YES
if the device is in the list and the connectionState of the
BGXpressManager
is
SCANNING
or
DISCONNECTED
; otherwise it will return
NO
meaning that no connection attempt will occur. This call is asynchronous. To detect when the connection occurs, the
BGXpressDelegate
for your
BGXpressManager
will be called using the method
- (void)connectionStateChanged:(ConnectionState)newConnectionState;
When this is called with the value of
CONNECTED
, the connection has finished.
Note that BGX devices only support one connection at a time when they are acting as a peripheral.
Detecting device changes
The
BGXpressDelegate
for your
BGXpressManager
will be called when certain events occur related to the connected device. For example, the method
- (void)dataRead:(NSData *)newData
is called when data is received by the BGX.
Read/Write Serial data
To write serial data to a connected BGX device, the
BGXpressManager
method
Bus Mode
To read the
BusMode
, call the
BGXpressManager
method
- (BOOL)readBusMode;
. This method will return YES if the
BusMode
can be read. When it is read, the
BGXpressDelegate
method
- (void)busModeChanged:(BusMode)newBusMode
will be called.
To change the
BusMode
, call the
BGXpressManager
method
- (BOOL)writeBusMode:(BusMode)newBusMode;
The call will return
YES
if the
BusMode
can be written. When the write has completed, the
BGXpressDelegate
delegate method
- (void)busModeChanged:(BusMode)newBusMode
will be called.
Disconnecting from a BGX
To disconnect from the currently connected BGX device, call the
BGXpressManager
method
- (BOOL)disconnect;
. This method returns
YES
if the disconnect operation can be performed (i.e. a device is connected or connecting). The call is asynchronous. When the disconnect is complete, your
BGXpressDelegate
method
- (void)connectionStateChanged:(ConnectionState)newConnectionState;
will be called.
Firmware Update
Updating the firmware on a BGX device involves the following steps:
- Select the BGX you wish to update.
- Get a list of available firmware for the device.
- Retrieve the image of the firmware to be installed.
- Install it on the BGX.
Get available firmware using DMS
To get a list of available firmware, first use the unique device id for the BGX to create an instance of
bgx_dms
:
self.bgx_dms = [[
bgx_dms
alloc] initWithBGXUniqueDeviceID: self.bgxpressManager.device_unique_id];
Then call the method
`- (void)retrieveAvailableVersions:(void (^)(NSError *, NSArray *))completionBlock;`
to get the available firmware for the BGX.
The completion block will be called with an array of
NSDictionary
objects representing firmware versions. Each
NSDictionary
will contain a
version
(NSString), a
tag
(NSString), and a
size
(NSNumber).
Note that this operation requires the DMS server to be reachable by your iOS device. When the DMS server becomes rechable or unreachable, the notification
DMSServerReachabilityChangedNotificationName
will be sent with an object of an
NSNumber
containing a boolean.
YES
indicates reachable;
NO
indicates not reachable. You can register to receive this notification using the default NSNotificationCenter. You may receive this notication anytime after you create an instance of
bgx_dms
. Therefore, you should register for the notification before creating a
bgx_dms
instance.
Get firmware image using DMS
To retrieve a specific firmware image, use the
`- (void)loadFirmwareVersion:(NSString *)version completion:(void (^)(NSError *, NSString * firmware_path))completionBlock;`
method. The completion routine will be called with the absolute path to the file containing the firmware image.
You can use the same image to update the firmware on more than one BGX provided they are have the same part id. To determine the part id, use the
bgx_dms
method
+ (NSString *)bgxPartInfoForDeviceID:(NSString *)device_uuid;
Updating a BGX using a firmware image
To update a BGX using a firmware image:
-
Create an instance of
BGX_OTA_Updater. -
Use KVO to observe changes to the properties you are interested in. This will usually be the
operationInProgressproperty, theota_stepproperty, and theupload_progressproperty. -
Call
- (void)updateFirmwareWithImageAtPath:(NSString *)path2FWImage withVersion:(NSString *)version.
The simplest way to detect that the firmware update has finished is that the
operationsInProgress
property has the value
ota_firmware_update_complete
. The value of
ota_step
will be
ota_step_end
when the update has completed without error.