Host Boot

hboot.filename

Abbreviation

hb f

Access

get/set

Description

Set the default value of the host boot filename.

See hboot command.

Arguments

<filename>

where filename is name of the firmware file from which to boot.

Default

host_firmware.bin

Properties

Get example

> get hb f
R000019
host_firmware.bin

Set example

> set hb f EFM8/UB1/SpaceInvaders.efm8
R000008
Set OK

hboot.gpio

Abbreviation

hb g

Access

get/set

Description

Set the host boot GPIO.

See hboot command.

Arguments

<GPIO#>

where GPIO# is the number of an available GPIO.

Set to -1 to disable the host boot GPIO.

Default

-1

Properties

Get example

> get hb g
R000004
-1

Set example

> set hb g 3
R000008
Set OK