IO Connection
ioconn.control_gpio
Abbreviation
io c
Access
get/set
Description
The GPIO used for control of the GPIO controlled network connection (stream). See the GPIO-Controlled Network Connection application note.
Arguments
<GPIO#>
Default
-1
Properties
Platforms
- AMW007
Get example
> get io c
R000004
-1
Set example
> set io c 6
R000008
Set OK
ioconn.enabled
Abbreviation
io e
Access
get/set
Description
Enable/disable the GPIO controlled network connection feature.
Arguments
<0/off/false/1/on/true>
Default
0
Properties
Platforms
- AMW007
Get example
> get io e
R000003
0
Set example
> set io e true
R000008
Set OK
ioconn.local_port
Abbreviation
io l
Access
get/set
Description
The local port associated with the GPIO controlled network connection, If 0, a random port is assigned.
Arguments
<port>
Default
0
Properties
Platforms
- AMW007
Get example
> get io l
R000003
0
Set example
> set io l 30001
R000008
Set OK
ioconn.protocol
Abbreviation
io p
Access
get/set
Description
The network protocol associated with the GPIO controlled network connection.
Arguments
<udp/tcp/tls>
Default
tcp
Properties
Platforms
- AMW007
Get example
> get io p
R000005
tcp
Set example
> set io p udp
R000008
Set OK
ioconn.remote_host
Abbreviation
io h
Access
get/set
Description
The remote host associated with the GPIO controlled network connection. An IP address or hostname may be specified.
Arguments
<IP address/hostname>
Default
-
Properties
Platforms
- AMW007
Get example
> get > get io h
R000013
10.11.176.12
Set example
> set io h example.com
R000008
Set OK
ioconn.remote_port
Abbreviation
io r
Access
get/set
Description
The remote port associated with the GPIO controlled network connection.
Arguments
<port>
Default
0
Properties
Platforms
- AMW007
Get example
> get io r
R000003
0
Set example
> set io r 55000
R000008
Set OK
ioconn.status_gpio
Abbreviation
io s
Access
get/set
Description
The GPIO used to indicate connection status when the GPIO controlled network connection feature is enabled.
See also system.oob.gpio.
Arguments
<GPIO#>
Default
-1
Properties
Platforms
- AMW007
Get example
> get io s
R000004
-1
Set example
> set io s 13
R000008
Set OK