Setup #
setup.auto.cmd #
Abbreviation
se a c
Access
get/set
Description
The Gecko OS command specified by
setup.auto.cmd
is run after boot up if:
- setup.gpio.control_gpio is NOT asserted AND
- wlan.ssid is NOT configured.
This corresponds to the 'out-of-the-box' default state of a module. You can set
setup.auto.cmd
to
setup cmd
to run a setup script file. See
Setup Configuration Script
.
Arguments
<command>
Default
None
Platforms
- WGM160P
Properties
Gecko OS Plugin
Get example
> get se a c
R000005
wps
Set example
> set se a c "setup web"
R000008
Set OK
setup.gpio.cmd #
Abbreviation
se g c
Access
get/set
Description
The specified command is executed in response to a reboot, or a specified GPIO being asserted, depending on the setting of the setup.gpio.control_gpio and the setup.gpio.mode .
Arguments
<command>
Default
setup_web
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get se g c
R000011
setup_web
Set example
> set se g c setup_web
R000008
Set OK
setup.gpio.control_gpio #
Abbreviation
se g g
Access
get/set
Description
Asserting the GPIO specified by
setup.gpio.control_gpio
for
3
seconds during and immediately after reset causes the Gecko OS command specified by
setup.gpio.cmd
to run. A value of
-1
disables this feature.
Arguments
<GPIO#>
Default
The default GPIO is platform dependent
The default GPIO is typically mapped to button 2 on evaluation boards (the wake button).
Platforms
- WGM160P
Properties
Gecko OS Plugin
Get example
> get se g g
R000003
3
Set example
> set se g g 12
R000008
Set OK
setup.gpio.level #
Abbreviation
se g l
Access
get/set
Description
The active logic level used when setup.gpio.control_gpio is asserted.
Arguments
<GPIO#>
Default
1
Platforms
- WGM160P
Properties
Gecko OS Plugin
Get example
> get se g l
R000003
1
Set example
> set se g l 0
R000008
Set OK
setup.gpio.mode #
Abbreviation
se g m
Access
get/set
Description
The mode setting determines what events result in running the command string specified by setup.gpio.cmd .
If the setup.gpio.cmd is set, the command is run as follows:
Mode | Event Causing Command to Run | Note |
---|---|---|
boot
|
The command is run on PoR (Power on Reset, or reboot) | The operation ignores the control GPIO. |
gpio
|
If setup.gpio.control_gpio is set, the command runs when the GPIO is asserted for 3 seconds through a PoR. |
This corresponds to the legacy behavior of running
setup_web
using Button 2 on evaluation boards.
Control GPIO is not registered so may be used as another function. |
any
|
If setup.gpio.control_gpio is set, the command runs any time the GPIO is asserted. | Control GPIO is registered so cannot be used as another function. |
Otherwise the command does not run.
Arguments
boot/gpio/any
Default
None
Platforms
- WGM160P
Properties
Gecko OS Plugin
Get example
> get se g m
gpio
Set example
> set se g m boot
R000008
Set OK
setup.web.captive_portal_enabled #
Abbreviation
se w a
Access
get/set
Description
Enable or disable captive portal during web setup. See softap.captive_portal_enabled .
Arguments
1|True|On/0|False|Off
Default
1
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get setup.web.captive_portal_enabled
1
Set example
> set setup.web.captive_portal_enabled 0
Set OK
setup.web.client_list #
Abbreviation
se w c
Access
get
Description
List MAC address, IP address and OS of connected websetup clients.
Note : 'Invalid' means the client has not yet connected to the webpage (but is connected to the softap).
The additional info comes from the browser's 'User-Agent' field in its HTTP request header.
The following is a list of supported OSs:
- Windows
- Windows Mobile
- Linux
- Mac
- Android
- iPhone
- iPod
- iPad
- Blackberry
- Chrome
- Symbian
- Unknown
Arguments
None
Default
None
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get setup.web.client_list
R000143
! Connected: 2
! # MAC IP Address OS
# 1 90:18:7C:34:CB:97 10.10.10.2 Android
# 2 F8:16:54:35:0F:8E 0.0.0.0 Windows
setup.web.idle_timeout #
Abbreviation
se w i
Access
get/set
Description
If no client connects to the web setup webpage after
setup.web.idle_timeout
seconds, web setup times out and is terminated. Upon timeout, if a
wlan.ssid
has previously been set, Gecko OS attempts to re-join the WLAN network.
setup.web.idle_timeout
is disabled when a client requests the root index of the webapp.
Arguments
<seconds>
Note
: Setting this variable to
0
disables web setup idle timeout.
Default
300
(5 minutes)
Platforms
- WGM160P
Properties
- restart setup to apply change
Gecko OS Plugin
Get example
> get setup.web.idle_timeout
R000005
300
Set example
> set se w i 0
R000008
Set OK
setup.web.passkey #
Abbreviation
se w p
Access
get/set
Description
The softAP WPA2-AES passphrase used for web setup.
Arguments
<passphrase>
where
<passphrase>
is one of the following:
<passphrase> / <WEP key>
|
Description |
---|---|
WPA Passphrase | length: 8 - 63 characters |
WPA PSK | length: 64 characters |
""
|
Sets a NULL passphrase |
For allowable values and set syntax see: Networking and Security, Passkeys .
Default
password
Platforms
- WGM160P
Properties
- restart setup to apply change
Gecko OS Plugin
Get example
> get we p
R000010
password
Set example
> set we p my-new-password
R000008
Set OK
setup.web.root_filename #
Abbreviation
se w r
Access
get/set
Description
The root filename of the web setup. In response to a request for
http://gecko-os.com
, the web server returns
http://Gecko OS.com/<root_filename>
.
Note : The file must be a supported type for it to appear correctly in the browser. The type is determined by the file extension. The following types are supported:
Extension | MIME |
---|---|
.css | text/css |
.js | application/javascript |
.html/.htm | text/html |
.png | image/png |
.ico | image/x-icon |
.gif | image/gif |
.jpg/.jpeg | image/jpeg |
.txt | text/plain |
Arguments
<root_filename>
Default
/setup/index.html
Platforms
- WGM160P
Properties
- restart setup to apply change
Gecko OS Plugin
Get example
> get se w r
/setup/index.html
Set example
> set se w r home.htm
R000008
Set OK
setup.web.ssid #
Abbreviation
se w s
Access
get/set
Description
The softAP SSID used for web setup. If the SSID ends in a # character, the last three hex characters of the WLAN MAC address replace the
#
.
For example, if the device MAC address is
4C:55:CC:10:26:05
, and
setup.web.ssid
is set to
Gecko OS Web Setup #
, then SSID becomes:
Gecko OS Web Setup 605
.
Arguments
<ssid>
Default
Gecko_OS-#
Platforms
- WGM160P
Properties
- restart setup to apply change
Gecko OS Plugin
Get example
> get we s
R000021
Gecko_OS-#
Set example
> set we s "This is my softAP!"
R000012
Set OK
setup.web.url #
Abbreviation
se w u
Access
get/set
Description
A comma separated list of host names the webserver responds to in web setup mode.
Arguments
<url list>
Default
gecko-os.com,www.gecko-os.com,setup.com,www.setup.com
Platforms
- WGM160P
Properties
- restart setup to apply change
Gecko OS Plugin
Get example
> get we u
R000057
gecko-os.com,www.gecko-os.com,setup.com,www.setup.com
Set example
> set we u setup,start,lets.go,hello
R000008
Set OK