TCP Client #

tcp.client.auto_interface #

Abbreviation

tc c i

Access

get/set

Description

Interface to auto-start TCP client connection.

See TCP Client .

Arguments

default

Default

default/wlan/softap

Platforms

Properties

Gecko OS Plugin

Get example

> get tcp.client.auto_interface
default

Set example

> set tc c i wlan
Set OK

tcp.client.auto_retries #

Abbreviation

tc c e

Access

get/set

Description

Determines number of attempts to reconnect after remote server disconnects client.

Note : This counter is reset when the interface is brought down.

To control how the client connects to the server, use tcp.client.retries , tcp.client.connect_timeout and tcp.client.retry_period .

See TCP Client .

Arguments

0-255

Default

0

Platforms

Properties

Gecko OS Plugin

Get example

> get tcp.client.auto_retries
0

Set example

set tc c e 20
Set OK

tcp.client.auto_start #

Abbreviation

tc c a

Access

get/set

Description

Enable/disable TCP client auto-start feature. If enabled, TCP client automatically connects to remote server when interface is brought up.

To enable TLS, see tcp.client.tls_enabled .

See TCP Client .

Arguments

1|true|on/0|false|off

where

Default

0

Platforms

Properties

Gecko OS Plugin

Get example

> get tcp.client.auto_start
0

Set example

> set tc c a 1
Set OK

tcp.client.connect_timeout #

Abbreviation

tc c t

Access

get/set

Description

TCP client connect timeout in milliseconds.

This variable controls timeout for the following commands:

See TCP Client .

Arguments

<milliseconds>

Default

5000

Platforms

Properties

Gecko OS Plugin

Get example

> get tc c t
R000006
5000

Set example

> set tc c t 6500
R000008
Set OK

tcp.client.local_port #

Abbreviation

tc c p

Access

get/set

Description

TCP client local port. 0 = automatic.

If you set this value, the first connection is made using the specified local port.

Subsequent additional TCP client connections determine the port by incrementing the last port used. If the specified port is X , the first subsequent connection uses port X+1 . The next TCP client connection uses port X+2 , and so on.

To reset the local port back to X , reboot the client.

See TCP Client .

Arguments

<port>

Default

0

Platforms

Properties

Gecko OS Plugin

Get example

> get tc c p
R000003
0

Set example

> set tc c p 30009
R000008
Set OK

tcp.client.remote_host #

Abbreviation

tc c h

Access

get/set

Description

Domain or IP address of remote tcp server to auto connect.

See TCP Client .

Arguments

<domain/ip address>

Default

None

Platforms

Properties

Gecko OS Plugin

Get example

> get tcp.client.remote_host
mydomain.com

Set example

> set tc c h mydomain.com
Set OK

tcp.client.remote_port #

Abbreviation

tc c o

Access

get/set

Description

Port of remote tcp server to auto connect.

See TCP Client .

Arguments

<port>

Default

3000

Platforms

Properties

Gecko OS Plugin

Get example

> get tcp.client.remote_port

Set example

> set tc c o 5000
Set OK

tcp.client.retries #

Abbreviation

tc c r

Access

get/set

Description

Maximum TCP client connection retry attempts.

See TCP Client .

Arguments

<max #retries>

Range: 1 - 255

Default

3

Platforms

Properties

Gecko OS Plugin

Get example

> get tc c r
R000003
3

Set example

> set tc c r 5
R000008
Set OK

tcp.client.retry_period #

Abbreviation

tc c w

Access

get/set

Description

TCP client wait time between connection retry attempts.

See TCP Client .

Arguments

<milliseconds>

Range: 0 - 65535

Default

1000

Platforms

Properties

Gecko OS Plugin

Get example

> get tc c w
R000006
1000

Set example

> set tc c w 2000
R000008
Set OK

tcp.client.tls_enabled #

Abbreviation

tc c s

Access

get/set

Description

Enables TLS for the [ tcp.client.auto_start feature.

The TLS certs are configured with the following variables:

See TLS Client .

Arguments

1|true|on/0|false|off

where

Default

0

Platforms

Properties

Gecko OS Plugin

Get example

> get tc c s
0

Set example

> set tc c s 1
Set OK