TCP Keepalive #
tcp.keepalive.enabled #
Abbreviation
tc k e
Access
get/set
Description
Enable/disable TCP keepalive feature of network stack.
Note : These settings apply to ALL TCP connections (TCP client, TLS, TCP server)
Keepalive is a system for determining whether a connected peer is still connected. If the peer reboots or otherwise drops out without notice, keepalive detects the problem. It works by sending an empty message at a specified interval and receiving an ACK in reply from the peer. If the ACK is not received with an initial expiration period, the keepalive exchange is periodically retried at a specified retry period until the retry count is exceeded.
To determine the initial expiration period, see tcp.keepalive.initial_timeout .
To determine the retry period, see tcp.keepalive.retry_timeout .
To determine the maximum retry count, see tcp.keepalive.retry_count .
Arguments
1|true|on/0|false|off
where
-
0
orfalse
oroff
: disabled -
1
ortrue
oron
: enabled
Default
False
Platforms
- WGM160P
Properties
- takes effect immediately
- preserved by NVM Backup
Gecko OS Plugin
Get example
> get tc k e
0
Set example
> set tc k e 1
Set OK
tcp.keepalive.initial_timeout #
Abbreviation
tc k i
Access
get/set
Description
Number of seconds for initial keepalive expiration.
See tcp.keepalive.enabled .
Arguments
<seconds>
Range:
1 - 65535
Default
60
Platforms
- WGM160P
Properties
- takes effect immediately
- preserved by NVM Backup
Gecko OS Plugin
Get example
> get tc k i
60
Set example
> set tc k i 20
Set OK
tcp.keepalive.retry_count #
Abbreviation
tc k c
Access
get/set
Description
Maximum number of times to retry keepalive. Once all retries are expired, close connection.
See tcp.keepalive.enabled .
Arguments
<retries>
Range:
1 - 255
Default
5
Platforms
- WGM160P
Properties
- takes effect immediately
- preserved by NVM Backup
Gecko OS Plugin
Get example
> get tc k c
5
Set example
> set tc k c 10
Set OK
tcp.keepalive.retry_timeout #
Abbreviation
tc k r
Access
get/set
Description
After initial expiration, period of retries in seconds.
See tcp.keepalive.enabled .
Arguments
<seconds>
Range:
1 - 255
Default
5
Platforms
- WGM160P
Properties
- takes effect immediately
- preserved by NVM Backup
Gecko OS Plugin
Get example
> get tc k r
5
Set example
> set tc k r 10
Set OK