LESENSE_PerCtrlDesc_TypeDef Struct Reference
LESENSE peripheral control descriptor structure.
#include <em_lesense.h>
Data Fields | |
LESENSE_ControlDACData_TypeDef | dacCh0Data |
Configure DAC channel 0 data control. | |
LESENSE_ControlDACConv_TypeDef | dacCh0ConvMode |
Configure how LESENSE controls conversion on DAC channel 0. | |
LESENSE_ControlDACOut_TypeDef | dacCh0OutMode |
Configure how LESENSE controls output on DAC channel 0. | |
LESENSE_ControlDACData_TypeDef | dacCh1Data |
Configure DAC channel 1 data control. | |
LESENSE_ControlDACConv_TypeDef | dacCh1ConvMode |
Configure how LESENSE controls conversion on DAC channel 1. | |
LESENSE_ControlDACOut_TypeDef | dacCh1OutMode |
Configure how LESENSE controls output on DAC channel 1. | |
uint8_t | dacPresc |
Configure the prescaling factor for the LESENSE - DAC interface. | |
LESENSE_DACRef_TypeDef | dacRef |
Configure the DAC reference to be used. | |
LESENSE_ControlACMP_TypeDef | acmp0Mode |
Configure how LESENSE controls ACMP 0. | |
LESENSE_ControlACMP_TypeDef | acmp1Mode |
Configure how LESENSE controls ACMP 1. | |
LESENSE_WarmupMode_TypeDef | warmupMode |
Configure how LESENSE controls ACMPs and DAC in idle mode. | |
LESENSE peripheral control descriptor structure.
Field Documentation
◆ dacCh0Data
LESENSE_ControlDACData_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0Data |
Configure DAC channel 0 data control.
◆ dacCh0ConvMode
LESENSE_ControlDACConv_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0ConvMode |
Configure how LESENSE controls conversion on DAC channel 0.
◆ dacCh0OutMode
LESENSE_ControlDACOut_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0OutMode |
Configure how LESENSE controls output on DAC channel 0.
◆ dacCh1Data
LESENSE_ControlDACData_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1Data |
Configure DAC channel 1 data control.
◆ dacCh1ConvMode
LESENSE_ControlDACConv_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1ConvMode |
Configure how LESENSE controls conversion on DAC channel 1.
◆ dacCh1OutMode
LESENSE_ControlDACOut_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1OutMode |
Configure how LESENSE controls output on DAC channel 1.
◆ dacPresc
uint8_t LESENSE_PerCtrlDesc_TypeDef::dacPresc |
Configure the prescaling factor for the LESENSE - DAC interface.
Valid range: 0-31 (5-bit).
◆ dacRef
LESENSE_DACRef_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacRef |
Configure the DAC reference to be used.
Set to lesenseDACRefVdd to use VDD and set to lesenseDACRefBandGap to use band gap as reference.
◆ acmp0Mode
LESENSE_ControlACMP_TypeDef LESENSE_PerCtrlDesc_TypeDef::acmp0Mode |
Configure how LESENSE controls ACMP 0.
◆ acmp1Mode
LESENSE_ControlACMP_TypeDef LESENSE_PerCtrlDesc_TypeDef::acmp1Mode |
Configure how LESENSE controls ACMP 1.
◆ warmupMode
LESENSE_WarmupMode_TypeDef LESENSE_PerCtrlDesc_TypeDef::warmupMode |
Configure how LESENSE controls ACMPs and DAC in idle mode.