PRS - Peripheral Reflex System
Description
Peripheral Reflex System (PRS) Peripheral API.
This module contains functions to control the PRS peripheral of Silicon Labs 32-bit MCUs and SoCs. The PRS allows configurable, fast, and autonomous communication between peripherals on the MCU or SoC.
Functions |
|
| void | PRS_SourceSignalSet (unsigned int ch, uint32_t source, uint32_t signal, PRS_Edge_TypeDef edge) |
|
Set a source and signal for a channel.
|
|
| void | PRS_SourceAsyncSignalSet (unsigned int ch, uint32_t source, uint32_t signal) |
|
Set the source and asynchronous signal for a channel.
|
|
| void | PRS_GpioOutputLocation (unsigned int ch, unsigned int location) |
|
Send the output of a PRS channel to a GPIO pin.
|
|
| int | PRS_GetFreeChannel ( PRS_ChType_t type) |
|
Search for the first free PRS channel.
|
|
| void | PRS_Reset (void) |
|
Reset all PRS channels.
|
|
| void | PRS_ConnectSignal (unsigned int ch, PRS_ChType_t type, PRS_Signal_t signal) |
|
Connect a PRS signal to a channel.
|
|
| void | PRS_LevelSet (uint32_t level, uint32_t mask) |
|
Set level control bit for one or more channels.
|
|
| uint32_t | PRS_LevelGet (void) |
|
Get level control bit for all channels.
|
|
| uint32_t | PRS_Values ( PRS_ChType_t type) |
|
Get the PRS channel values for all channels.
|
|
| bool | PRS_ChannelValue (unsigned int ch, PRS_ChType_t type) |
|
Get the PRS channel value for a single channel.
|
|
| void | PRS_PulseTrigger (uint32_t channels) |
|
Trigger a high pulse (one HFPERCLK) for one or more channels.
|
|
| void | PRS_ChannelLevelSet (unsigned int ch, bool level) |
|
Set the PRS channel level for one asynchronous PRS channel.
|
|
| void | PRS_ChannelPulse (unsigned int ch) |
|
Trigger a pulse on one PRS channel.
|
|
Macros |
|
| #define | PRS_SYNC_CHAN_COUNT PRS_CHAN_COUNT |
|
PRS Synchronous channel count.
|
|
| #define | PRS_ASYNC_CHAN_COUNT PRS_CHAN_COUNT |
|
PRS Asynchronous channel count.
|
|
| #define | PRS_ASYNC_SUPPORTED 1 |
|
PRS asynchronous support.
|
|
Enumerations |
|
| enum |
PRS_ChType_t
{
prsTypeAsync , prsTypeSync } |
|
PRS Channel type.
|
|
| enum |
PRS_Edge_TypeDef
{
prsEdgeOff , prsEdgePos , prsEdgeNeg , prsEdgeBoth } |
|
Edge detection type.
|
|
| enum |
PRS_Signal_t
{
prsSignalNone = PRS_CH_CTRL_SOURCESEL_NONE | (0x0 << _PRS_CH_CTRL_SIGSEL_SHIFT), prsSignalSW = PRS_CH_CTRL_SOURCESEL_NONE | (0x1 << _PRS_CH_CTRL_SIGSEL_SHIFT), prsSignalPRS_CH0 = PRS_PRS_CH0, prsSignalPRS_CH1 = PRS_PRS_CH1, prsSignalPRS_CH2 = PRS_PRS_CH2, prsSignalPRS_CH3 = PRS_PRS_CH3, prsSignalPRS_CH4 = PRS_PRS_CH4, prsSignalPRS_CH5 = PRS_PRS_CH5, prsSignalPRS_CH6 = PRS_PRS_CH6, prsSignalPRS_CH7 = PRS_PRS_CH7, prsSignalPRS_CH8 = PRS_PRS_CH8, prsSignalPRS_CH9 = PRS_PRS_CH9, prsSignalPRS_CH10 = PRS_PRS_CH10, prsSignalPRS_CH11 = PRS_PRS_CH11, prsSignalPRS_CH12 = PRS_PRS_CH12, prsSignalPRS_CH13 = PRS_PRS_CH13, prsSignalPRS_CH14 = PRS_PRS_CH14, prsSignalPRS_CH15 = PRS_PRS_CH15, prsSignalPRS_CH16 = PRS_PRS_CH16, prsSignalPRS_CH17 = PRS_PRS_CH17, prsSignalPRS_CH18 = PRS_PRS_CH18, prsSignalPRS_CH19 = PRS_PRS_CH19, prsSignalPRS_CH20 = PRS_PRS_CH20, prsSignalPRS_CH21 = PRS_PRS_CH21, prsSignalPRS_CH22 = PRS_PRS_CH22, prsSignalPRS_CH23 = PRS_PRS_CH23, prsSignalADC0_SINGLE = PRS_ADC0_SINGLE, prsSignalADC0_SCAN = PRS_ADC0_SCAN, prsSignalADC1_SINGLE = PRS_ADC1_SINGLE, prsSignalADC1_SCAN = PRS_ADC1_SCAN, prsSignalTIMER0_UF = PRS_TIMER0_UF, prsSignalTIMER0_OF = PRS_TIMER0_OF, prsSignalTIMER0_CC0 = PRS_TIMER0_CC0, prsSignalTIMER0_CC1 = PRS_TIMER0_CC1, prsSignalTIMER0_CC2 = PRS_TIMER0_CC2, prsSignalTIMER1_UF = PRS_TIMER1_UF, prsSignalTIMER1_OF = PRS_TIMER1_OF, prsSignalTIMER1_CC0 = PRS_TIMER1_CC0, prsSignalTIMER1_CC1 = PRS_TIMER1_CC1, prsSignalTIMER1_CC2 = PRS_TIMER1_CC2, prsSignalTIMER2_UF = PRS_TIMER2_UF, prsSignalTIMER2_OF = PRS_TIMER2_OF, prsSignalTIMER2_CC0 = PRS_TIMER2_CC0, prsSignalTIMER2_CC1 = PRS_TIMER2_CC1, prsSignalTIMER2_CC2 = PRS_TIMER2_CC2, prsSignalTIMER3_UF = PRS_TIMER3_UF, prsSignalTIMER3_OF = PRS_TIMER3_OF, prsSignalTIMER3_CC0 = PRS_TIMER3_CC0, prsSignalTIMER3_CC1 = PRS_TIMER3_CC1, prsSignalTIMER3_CC2 = PRS_TIMER3_CC2, prsSignalTIMER1_CC3 = PRS_TIMER1_CC3, prsSignalTIMER4_UF = PRS_TIMER4_UF, prsSignalTIMER4_OF = PRS_TIMER4_OF, prsSignalTIMER4_CC0 = PRS_TIMER4_CC0, prsSignalTIMER4_CC1 = PRS_TIMER4_CC1, prsSignalTIMER4_CC2 = PRS_TIMER4_CC2, prsSignalTIMER5_UF = PRS_TIMER5_UF, prsSignalTIMER5_OF = PRS_TIMER5_OF, prsSignalTIMER5_CC0 = PRS_TIMER5_CC0, prsSignalTIMER5_CC1 = PRS_TIMER5_CC1, prsSignalTIMER5_CC2 = PRS_TIMER5_CC2, prsSignalTIMER6_UF = PRS_TIMER6_UF, prsSignalTIMER6_OF = PRS_TIMER6_OF, prsSignalTIMER6_CC0 = PRS_TIMER6_CC0, prsSignalTIMER6_CC1 = PRS_TIMER6_CC1, prsSignalTIMER6_CC2 = PRS_TIMER6_CC2, prsSignalLETIMER0_CH0 = PRS_LETIMER0_CH0, prsSignalLETIMER0_CH1 = PRS_LETIMER0_CH1, prsSignalLETIMER1_CH0 = PRS_LETIMER1_CH0, prsSignalLETIMER1_CH1 = PRS_LETIMER1_CH1, prsSignalPCNT0_TCC = PRS_PCNT0_TCC, prsSignalPCNT0_UFOF = PRS_PCNT0_UFOF, prsSignalPCNT0_DIR = PRS_PCNT0_DIR, prsSignalPCNT1_TCC = PRS_PCNT1_TCC, prsSignalPCNT1_UFOF = PRS_PCNT1_UFOF, prsSignalPCNT1_DIR = PRS_PCNT1_DIR, prsSignalPCNT2_TCC = PRS_PCNT2_TCC, prsSignalPCNT2_UFOF = PRS_PCNT2_UFOF, prsSignalPCNT2_DIR = PRS_PCNT2_DIR, prsSignalCRYOTIMER_PERIOD = PRS_CRYOTIMER_PERIOD, prsSignalRTC_OF = PRS_RTC_OF, prsSignalRTC_COMP0 = PRS_RTC_COMP0, prsSignalRTC_COMP1 = PRS_RTC_COMP1, prsSignalRTC_COMP2 = PRS_RTC_COMP2, prsSignalRTC_COMP3 = PRS_RTC_COMP3, prsSignalRTC_COMP4 = PRS_RTC_COMP4, prsSignalRTC_COMP5 = PRS_RTC_COMP5, prsSignalRTCC_CCV0 = PRS_RTCC_CCV0, prsSignalRTCC_CCV1 = PRS_RTCC_CCV1, prsSignalRTCC_CCV2 = PRS_RTCC_CCV2, prsSignalACMP0_OUT = PRS_ACMP0_OUT, prsSignalACMP1_OUT = PRS_ACMP1_OUT, prsSignalACMP2_OUT = PRS_ACMP2_OUT, prsSignalACMP3_OUT = PRS_ACMP3_OUT, prsSignalVDAC0_CH0 = PRS_VDAC0_CH0, prsSignalVDAC0_CH1 = PRS_VDAC0_CH1, prsSignalVDAC0_OPA0 = PRS_VDAC0_OPA0, prsSignalVDAC0_OPA1 = PRS_VDAC0_OPA1, prsSignalVDAC0_OPA2 = PRS_VDAC0_OPA2, prsSignalVDAC0_OPA3 = PRS_VDAC0_OPA3, prsSignalLESENSE_SCANRES0 = PRS_LESENSE_SCANRES0, prsSignalLESENSE_SCANRES1 = PRS_LESENSE_SCANRES1, prsSignalLESENSE_SCANRES2 = PRS_LESENSE_SCANRES2, prsSignalLESENSE_SCANRES3 = PRS_LESENSE_SCANRES3, prsSignalLESENSE_SCANRES4 = PRS_LESENSE_SCANRES4, prsSignalLESENSE_SCANRES5 = PRS_LESENSE_SCANRES5, prsSignalLESENSE_SCANRES6 = PRS_LESENSE_SCANRES6, prsSignalLESENSE_SCANRES7 = PRS_LESENSE_SCANRES7, prsSignalLESENSE_SCANRES8 = PRS_LESENSE_SCANRES8, prsSignalLESENSE_SCANRES9 = PRS_LESENSE_SCANRES9, prsSignalLESENSE_SCANRES10 = PRS_LESENSE_SCANRES10, prsSignalLESENSE_SCANRES11 = PRS_LESENSE_SCANRES11, prsSignalLESENSE_SCANRES12 = PRS_LESENSE_SCANRES12, prsSignalLESENSE_SCANRES13 = PRS_LESENSE_SCANRES13, prsSignalLESENSE_SCANRES14 = PRS_LESENSE_SCANRES14, prsSignalLESENSE_SCANRES15 = PRS_LESENSE_SCANRES15, prsSignalLESENSE_DEC0 = PRS_LESENSE_DEC0, prsSignalLESENSE_DEC1 = PRS_LESENSE_DEC1, prsSignalLESENSE_DEC2 = PRS_LESENSE_DEC2, prsSignalLESENSE_DECCMP = PRS_LESENSE_DECCMP, prsSignalLESENSE_MEASACT = PRS_LESENSE_MEASACT, prsSignalUSART0_TXC = PRS_USART0_TXC, prsSignalUSART0_RXDATAV = PRS_USART0_RXDATAV, prsSignalUSART0_IRTX = PRS_USART0_IRTX, prsSignalUSART0_RTS = PRS_USART0_RTS, prsSignalUSART0_TX = PRS_USART0_TX, prsSignalUSART0_CS = PRS_USART0_CS, prsSignalUSART1_TXC = PRS_USART1_TXC, prsSignalUSART1_RXDATAV = PRS_USART1_RXDATAV, prsSignalUSART1_RTS = PRS_USART1_RTS, prsSignalUSART1_TX = PRS_USART1_TX, prsSignalUSART1_CS = PRS_USART1_CS, prsSignalUSART2_TXC = PRS_USART2_TXC, prsSignalUSART2_RXDATAV = PRS_USART2_RXDATAV, prsSignalUSART2_IRTX = PRS_USART2_IRTX, prsSignalUSART2_RTS = PRS_USART2_RTS, prsSignalUSART2_TX = PRS_USART2_TX, prsSignalUSART2_CS = PRS_USART2_CS, prsSignalUSART3_TXC = PRS_USART3_TXC, prsSignalUSART3_RXDATAV = PRS_USART3_RXDATAV, prsSignalUSART3_RTS = PRS_USART3_RTS, prsSignalUSART3_TX = PRS_USART3_TX, prsSignalUSART3_CS = PRS_USART3_CS, prsSignalUSART4_TXC = PRS_USART4_TXC, prsSignalUSART4_RXDATAV = PRS_USART4_RXDATAV, prsSignalUSART4_RTS = PRS_USART4_RTS, prsSignalUSART4_TX = PRS_USART4_TX, prsSignalUSART4_CS = PRS_USART4_CS, prsSignalUSART5_TXC = PRS_USART5_TXC, prsSignalUSART5_RXDATAV = PRS_USART5_RXDATAV, prsSignalUSART5_RTS = PRS_USART5_RTS, prsSignalUSART5_TX = PRS_USART5_TX, prsSignalUSART5_CS = PRS_USART5_CS, prsSignalUART0_TXC = PRS_UART0_TXC, prsSignalUART0_RXDATAV = PRS_UART0_RXDATAV, prsSignalUART0_RTS = PRS_UART0_RTS, prsSignalUART0_TX = PRS_UART0_TX, prsSignalUART0_CS = PRS_UART0_CS, prsSignalUART1_TXC = PRS_UART1_TXC, prsSignalUART1_RXDATAV = PRS_UART1_RXDATAV, prsSignalUART1_RTS = PRS_UART1_RTS, prsSignalUART1_TX = PRS_UART1_TX, prsSignalUART1_CS = PRS_UART1_CS, prsSignalUSB_SOF = PRS_USB_SOF, prsSignalUSB_SOFSR = PRS_USB_SOFSR, prsSignalCM4_TXEV = PRS_CM4_TXEV, prsSignalCM4_ICACHEPCHITSOF = PRS_CM4_ICACHEPCHITSOF, prsSignalCM4_ICACHEPCMISSESOF = PRS_CM4_ICACHEPCMISSESOF, prsSignalWTIMER0_UF = PRS_WTIMER0_UF, prsSignalWTIMER0_OF = PRS_WTIMER0_OF, prsSignalWTIMER0_CC0 = PRS_WTIMER0_CC0, prsSignalWTIMER0_CC1 = PRS_WTIMER0_CC1, prsSignalWTIMER0_CC2 = PRS_WTIMER0_CC2, prsSignalWTIMER1_UF = PRS_WTIMER1_UF, prsSignalWTIMER1_OF = PRS_WTIMER1_OF, prsSignalWTIMER1_CC0 = PRS_WTIMER1_CC0, prsSignalWTIMER1_CC1 = PRS_WTIMER1_CC1, prsSignalWTIMER1_CC2 = PRS_WTIMER1_CC2, prsSignalWTIMER1_CC3 = PRS_WTIMER1_CC3, prsSignalWTIMER2_UF = PRS_WTIMER2_UF, prsSignalWTIMER2_OF = PRS_WTIMER2_OF, prsSignalWTIMER2_CC0 = PRS_WTIMER2_CC0, prsSignalWTIMER2_CC1 = PRS_WTIMER2_CC1, prsSignalWTIMER2_CC2 = PRS_WTIMER2_CC2, prsSignalWTIMER3_UF = PRS_WTIMER3_UF, prsSignalWTIMER3_OF = PRS_WTIMER3_OF, prsSignalWTIMER3_CC0 = PRS_WTIMER3_CC0, prsSignalWTIMER3_CC1 = PRS_WTIMER3_CC1, prsSignalWTIMER3_CC2 = PRS_WTIMER3_CC2, prsSignalGPIO_PIN0 = PRS_GPIO_PIN0, prsSignalGPIO_PIN1 = PRS_GPIO_PIN1, prsSignalGPIO_PIN2 = PRS_GPIO_PIN2, prsSignalGPIO_PIN3 = PRS_GPIO_PIN3, prsSignalGPIO_PIN4 = PRS_GPIO_PIN4, prsSignalGPIO_PIN5 = PRS_GPIO_PIN5, prsSignalGPIO_PIN6 = PRS_GPIO_PIN6, prsSignalGPIO_PIN7 = PRS_GPIO_PIN7, prsSignalGPIO_PIN8 = PRS_GPIO_PIN8, prsSignalGPIO_PIN9 = PRS_GPIO_PIN9, prsSignalGPIO_PIN10 = PRS_GPIO_PIN10, prsSignalGPIO_PIN11 = PRS_GPIO_PIN11, prsSignalGPIO_PIN12 = PRS_GPIO_PIN12, prsSignalGPIO_PIN13 = PRS_GPIO_PIN13, prsSignalGPIO_PIN14 = PRS_GPIO_PIN14, prsSignalGPIO_PIN15 = PRS_GPIO_PIN15 } |
|
PRS Signal.
|
|
Function Documentation
â—† PRS_SourceSignalSet()
| void PRS_SourceSignalSet | ( | unsigned int |
ch,
|
| uint32_t |
source,
|
||
| uint32_t |
signal,
|
||
| PRS_Edge_TypeDef |
edge
|
||
| ) |
Set a source and signal for a channel.
- Parameters
-
[in] chA channel to define the signal and source for. [in] sourceA source to select for the channel. Use one of PRS_CH_CTRL_SOURCESEL_x defines. [in] signalA signal (for selected source) to use. Use one of PRS_CH_CTRL_SIGSEL_x defines.[in] edgeAn edge (for selected source/signal) to generate the pulse for.
â—† PRS_SourceAsyncSignalSet()
| void PRS_SourceAsyncSignalSet | ( | unsigned int |
ch,
|
| uint32_t |
source,
|
||
| uint32_t |
signal
|
||
| ) |
Set the source and asynchronous signal for a channel.
Asynchronous reflexes are not clocked on HFPERCLK and can be used even in EM2/EM3. There is a limitation to reflexes operating in asynchronous mode in that they can only be used by a subset of the reflex consumers. See the PRS chapter in the reference manual for the complete list of supported asynchronous signals and consumers.
- Note
- This function is not supported on EFM32GxxxFyyy parts. In asynchronous mode, the edge detector only works in EM0 and should not be used. The EDSEL parameter in PRS_CHx_CTRL register is set to 0 (OFF) by default.
- Parameters
-
[in] chA channel to define the source and asynchronous signal for. [in] sourceA source to select for the channel. Use one of PRS_CH_CTRL_SOURCESEL_x defines. [in] signalAn asynchronous signal (for selected source) to use. Use one of the PRS_CH_CTRL_SIGSEL_x defines that support asynchronous operation.
â—† PRS_GpioOutputLocation()
| void PRS_GpioOutputLocation | ( | unsigned int |
ch,
|
| unsigned int |
location
|
||
| ) |
Send the output of a PRS channel to a GPIO pin.
This function is used to send the output of a PRS channel to a GPIO pin. Note that there are certain restrictions to where a PRS channel can be routed. Consult the datasheet of the device to see if a channel can be routed to the requested GPIO pin.
- Parameters
-
[in] chPRS channel number. [in] locationPRS routing location.
â—† PRS_GetFreeChannel()
| int PRS_GetFreeChannel | ( | PRS_ChType_t |
type
|
) |
Search for the first free PRS channel.
- Parameters
-
[in] typePRS channel type. This can be either prsTypeAsync or prsTypeSync .
- Returns
- Channel number >= 0 if an unused PRS channel was found. If no free PRS channel was found then -1 is returned.
â—† PRS_Reset()
| void PRS_Reset | ( | void |
|
) |
Reset all PRS channels.
This function will reset all the PRS channel configuration.
â—† PRS_ConnectSignal()
| void PRS_ConnectSignal | ( | unsigned int |
ch,
|
| PRS_ChType_t |
type,
|
||
| PRS_Signal_t |
signal
|
||
| ) |
Connect a PRS signal to a channel.
This function will make the PRS signal available on the specific channel. Only a single PRS signal can be connected to any given channel.
- Parameters
-
[in] chPRS channel number. [in] typePRS channel type. This can be either prsTypeAsync or prsTypeSync . [in] signalThis is the PRS signal that should be placed on the channel.
â—† PRS_LevelSet()
|
inline |
Set level control bit for one or more channels.
The level value for a channel is XORed with both the pulse possibly issued by PRS_PulseTrigger() and the PRS input signal selected for the channel(s).
- Parameters
-
[in] levelLevel to use for channels indicated by mask. Use logical OR combination of PRS_SWLEVEL_CHnLEVEL defines for channels to set high level, otherwise 0.[in] maskMask indicating which channels to set level for. Use logical OR combination of PRS_SWLEVEL_CHnLEVEL defines.
â—† PRS_LevelGet()
|
inline |
Get level control bit for all channels.
- Returns
- The current software level configuration.
â—† PRS_Values()
|
inline |
Get the PRS channel values for all channels.
- Parameters
-
[in] typePRS channel type. This can be either prsTypeAsync or prsTypeSync .
- Returns
- The current PRS channel output values for all channels as a bitset.
â—† PRS_ChannelValue()
|
inline |
Get the PRS channel value for a single channel.
- Parameters
-
[in] chPRS channel number. [in] typePRS channel type. This can be either prsTypeAsync or prsTypeSync .
- Returns
- The current PRS channel output value. This is either 0 or 1.
â—† PRS_PulseTrigger()
|
inline |
Trigger a high pulse (one HFPERCLK) for one or more channels.
Setting a bit for a channel causes the bit in the register to remain high for one HFPERCLK cycle. Pulse is XORed with both the corresponding bit in PRS SWLEVEL register and the PRS input signal selected for the channel(s).
- Parameters
-
[in] channelsLogical ORed combination of channels to trigger a pulse for. Use PRS_SWPULSE_CHnPULSE defines.
â—† PRS_ChannelLevelSet()
|
inline |
Set the PRS channel level for one asynchronous PRS channel.
- Parameters
-
[in] chPRS channel number. [in] leveltrue to set the level high (1) and false to set the level low (0).
â—† PRS_ChannelPulse()
|
inline |
Trigger a pulse on one PRS channel.
- Parameters
-
[in] chPRS channel number.
Macro Definition Documentation
â—† PRS_SYNC_CHAN_COUNT
| #define PRS_SYNC_CHAN_COUNTÂ Â Â PRS_CHAN_COUNT |
PRS Synchronous channel count.
â—† PRS_ASYNC_CHAN_COUNT
| #define PRS_ASYNC_CHAN_COUNTÂ Â Â PRS_CHAN_COUNT |
PRS Asynchronous channel count.
â—† PRS_ASYNC_SUPPORTED
| #define PRS_ASYNC_SUPPORTEDÂ Â Â 1 |
PRS asynchronous support.
Enumeration Type Documentation
â—† PRS_ChType_t
| enum PRS_ChType_t |
â—† PRS_Edge_TypeDef
| enum PRS_Edge_TypeDef |
â—† PRS_Signal_t
| enum PRS_Signal_t |
PRS Signal.