Authenticated encryption with associated data (AEAD)
Description
Functions | |
psa_status_t | psa_aead_encrypt (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *nonce, size_t nonce_length, const uint8_t *additional_data, size_t additional_data_length, const uint8_t *plaintext, size_t plaintext_length, uint8_t *ciphertext, size_t ciphertext_size, size_t *ciphertext_length) |
Process an authenticated encryption operation. | |
psa_status_t | psa_aead_decrypt (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *nonce, size_t nonce_length, const uint8_t *additional_data, size_t additional_data_length, const uint8_t *ciphertext, size_t ciphertext_length, uint8_t *plaintext, size_t plaintext_size, size_t *plaintext_length) |
Process an authenticated decryption operation. | |
psa_status_t | psa_aead_encrypt_setup (psa_aead_operation_t *operation, mbedtls_svc_key_id_t key, psa_algorithm_t alg) |
Set the key for a multipart authenticated encryption operation. | |
psa_status_t | psa_aead_decrypt_setup (psa_aead_operation_t *operation, mbedtls_svc_key_id_t key, psa_algorithm_t alg) |
Set the key for a multipart authenticated decryption operation. | |
psa_status_t | psa_aead_generate_nonce (psa_aead_operation_t *operation, uint8_t *nonce, size_t nonce_size, size_t *nonce_length) |
Generate a random nonce for an authenticated encryption operation. | |
psa_status_t | psa_aead_set_nonce (psa_aead_operation_t *operation, const uint8_t *nonce, size_t nonce_length) |
Set the nonce for an authenticated encryption or decryption operation. | |
psa_status_t | psa_aead_set_lengths (psa_aead_operation_t *operation, size_t ad_length, size_t plaintext_length) |
Declare the lengths of the message and additional data for AEAD. | |
psa_status_t | psa_aead_update_ad (psa_aead_operation_t *operation, const uint8_t *input, size_t input_length) |
Pass additional data to an active AEAD operation. | |
psa_status_t | psa_aead_update (psa_aead_operation_t *operation, const uint8_t *input, size_t input_length, uint8_t *output, size_t output_size, size_t *output_length) |
Encrypt or decrypt a message fragment in an active AEAD operation. | |
psa_status_t | psa_aead_finish (psa_aead_operation_t *operation, uint8_t *ciphertext, size_t ciphertext_size, size_t *ciphertext_length, uint8_t *tag, size_t tag_size, size_t *tag_length) |
Finish encrypting a message in an AEAD operation. | |
psa_status_t | psa_aead_verify (psa_aead_operation_t *operation, uint8_t *plaintext, size_t plaintext_size, size_t *plaintext_length, const uint8_t *tag, size_t tag_length) |
Finish authenticating and decrypting a message in an AEAD operation. | |
psa_status_t | psa_aead_abort (psa_aead_operation_t *operation) |
Abort an AEAD operation. | |
Macros | |
#define | PSA_AEAD_OPERATION_INIT {0, 0, 0, 0, 0, 0, 0, 0, 0, 0, {0}} |
Function Documentation
◆ psa_aead_encrypt()
psa_status_t psa_aead_encrypt | ( | mbedtls_svc_key_id_t | key, |
psa_algorithm_t | alg, |
||
const uint8_t * | nonce, |
||
size_t | nonce_length, |
||
const uint8_t * | additional_data, |
||
size_t | additional_data_length, |
||
const uint8_t * | plaintext, |
||
size_t | plaintext_length, |
||
uint8_t * | ciphertext, |
||
size_t | ciphertext_size, |
||
size_t * | ciphertext_length |
||
) |
Process an authenticated encryption operation.
- Parameters
-
key
Identifier of the key to use for the operation. It must allow the usage PSA_KEY_USAGE_ENCRYPT. alg
The AEAD algorithm to compute ( PSA_ALG_XXX
value such that PSA_ALG_IS_AEAD(alg
) is true).[in] nonce
Nonce or IV to use. nonce_length
Size of the nonce
buffer in bytes.[in] additional_data
Additional data that will be authenticated but not encrypted. additional_data_length
Size of additional_data
in bytes.[in] plaintext
Data that will be authenticated and encrypted. plaintext_length
Size of plaintext
in bytes.[out] ciphertext
Output buffer for the authenticated and encrypted data. The additional data is not part of this output. For algorithms where the encrypted data and the authentication tag are defined as separate outputs, the authentication tag is appended to the encrypted data. ciphertext_size
Size of the ciphertext
buffer in bytes. This must be appropriate for the selected algorithm and key:- A sufficient output size is #PSA_AEAD_ENCRYPT_OUTPUT_SIZE(
key_type
,alg
,plaintext_length
) wherekey_type
is the type ofkey
. - #PSA_AEAD_ENCRYPT_OUTPUT_MAX_SIZE(
plaintext_length
) evaluates to the maximum ciphertext size of any supported AEAD encryption.
[out] ciphertext_length
On success, the size of the output in the ciphertext
buffer. - A sufficient output size is #PSA_AEAD_ENCRYPT_OUTPUT_SIZE(
- Return values
-
PSA_SUCCESS
Success. PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_INVALID_ARGUMENT
key
is not compatible withalg
.PSA_ERROR_NOT_SUPPORTED
alg
is not supported or is not an AEAD algorithm.PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_BUFFER_TOO_SMALL
ciphertext_size
is too small. #PSA_AEAD_ENCRYPT_OUTPUT_SIZE(key_type
,alg
,plaintext_length
) or #PSA_AEAD_ENCRYPT_OUTPUT_MAX_SIZE(plaintext_length
) can be used to determine the required buffer size.PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_aead_decrypt()
psa_status_t psa_aead_decrypt | ( | mbedtls_svc_key_id_t | key, |
psa_algorithm_t | alg, |
||
const uint8_t * | nonce, |
||
size_t | nonce_length, |
||
const uint8_t * | additional_data, |
||
size_t | additional_data_length, |
||
const uint8_t * | ciphertext, |
||
size_t | ciphertext_length, |
||
uint8_t * | plaintext, |
||
size_t | plaintext_size, |
||
size_t * | plaintext_length |
||
) |
Process an authenticated decryption operation.
- Parameters
-
key
Identifier of the key to use for the operation. It must allow the usage PSA_KEY_USAGE_DECRYPT. alg
The AEAD algorithm to compute ( PSA_ALG_XXX
value such that PSA_ALG_IS_AEAD(alg
) is true).[in] nonce
Nonce or IV to use. nonce_length
Size of the nonce
buffer in bytes.[in] additional_data
Additional data that has been authenticated but not encrypted. additional_data_length
Size of additional_data
in bytes.[in] ciphertext
Data that has been authenticated and encrypted. For algorithms where the encrypted data and the authentication tag are defined as separate inputs, the buffer must contain the encrypted data followed by the authentication tag. ciphertext_length
Size of ciphertext
in bytes.[out] plaintext
Output buffer for the decrypted data. plaintext_size
Size of the plaintext
buffer in bytes. This must be appropriate for the selected algorithm and key:- A sufficient output size is #PSA_AEAD_DECRYPT_OUTPUT_SIZE(
key_type
,alg
,ciphertext_length
) wherekey_type
is the type ofkey
. - #PSA_AEAD_DECRYPT_OUTPUT_MAX_SIZE(
ciphertext_length
) evaluates to the maximum plaintext size of any supported AEAD decryption.
[out] plaintext_length
On success, the size of the output in the plaintext
buffer. - A sufficient output size is #PSA_AEAD_DECRYPT_OUTPUT_SIZE(
- Return values
-
PSA_SUCCESS
Success. PSA_ERROR_INVALID_HANDLE
PSA_ERROR_INVALID_SIGNATURE
The ciphertext is not authentic. PSA_ERROR_NOT_PERMITTED
PSA_ERROR_INVALID_ARGUMENT
key
is not compatible withalg
.PSA_ERROR_NOT_SUPPORTED
alg
is not supported or is not an AEAD algorithm.PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_BUFFER_TOO_SMALL
plaintext_size
is too small. #PSA_AEAD_DECRYPT_OUTPUT_SIZE(key_type
,alg
,ciphertext_length
) or #PSA_AEAD_DECRYPT_OUTPUT_MAX_SIZE(ciphertext_length
) can be used to determine the required buffer size.PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_aead_encrypt_setup()
psa_status_t psa_aead_encrypt_setup | ( | psa_aead_operation_t * | operation, |
mbedtls_svc_key_id_t | key, |
||
psa_algorithm_t | alg |
||
) |
Set the key for a multipart authenticated encryption operation.
- Note
- Multipart AEAD is not implemented in this Silicon Labs release.
The sequence of operations to encrypt a message with authentication is as follows:
- Allocate an operation object which will be passed to all the functions listed here.
- Initialize the operation object with one of the methods described in the documentation for #psa_aead_operation_t, e.g. PSA_AEAD_OPERATION_INIT.
- Call psa_aead_encrypt_setup() to specify the algorithm and key.
- If needed, call psa_aead_set_lengths() to specify the length of the inputs to the subsequent calls to psa_aead_update_ad() and psa_aead_update(). See the documentation of psa_aead_set_lengths() for details.
- Call either psa_aead_generate_nonce() or psa_aead_set_nonce() to generate or set the nonce. You should use psa_aead_generate_nonce() unless the protocol you are implementing requires a specific nonce value.
- Call psa_aead_update_ad() zero, one or more times, passing a fragment of the non-encrypted additional authenticated data each time.
- Call psa_aead_update() zero, one or more times, passing a fragment of the message to encrypt each time.
- Call psa_aead_finish().
If an error occurs at any step after a call to psa_aead_encrypt_setup(), the operation will need to be reset by a call to psa_aead_abort(). The application may call psa_aead_abort() at any time after the operation has been initialized.
After a successful call to psa_aead_encrypt_setup(), the application must eventually terminate the operation. The following events terminate an operation:
- A successful call to psa_aead_finish().
- A call to psa_aead_abort().
- Parameters
-
[in,out] operation
The operation object to set up. It must have been initialized as per the documentation for #psa_aead_operation_t and not yet in use. key
Identifier of the key to use for the operation. It must remain valid until the operation terminates. It must allow the usage PSA_KEY_USAGE_ENCRYPT. alg
The AEAD algorithm to compute ( PSA_ALG_XXX
value such that PSA_ALG_IS_AEAD(alg
) is true).
- Return values
-
PSA_SUCCESS
Success. PSA_ERROR_BAD_STATE
The operation state is not valid (it must be inactive). PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_INVALID_ARGUMENT
key
is not compatible withalg
.PSA_ERROR_NOT_SUPPORTED
alg
is not supported or is not an AEAD algorithm.PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_aead_decrypt_setup()
psa_status_t psa_aead_decrypt_setup | ( | psa_aead_operation_t * | operation, |
mbedtls_svc_key_id_t | key, |
||
psa_algorithm_t | alg |
||
) |
Set the key for a multipart authenticated decryption operation.
- Note
- Multipart AEAD is not implemented in this Silicon Labs release.
The sequence of operations to decrypt a message with authentication is as follows:
- Allocate an operation object which will be passed to all the functions listed here.
- Initialize the operation object with one of the methods described in the documentation for #psa_aead_operation_t, e.g. PSA_AEAD_OPERATION_INIT.
- Call psa_aead_decrypt_setup() to specify the algorithm and key.
- If needed, call psa_aead_set_lengths() to specify the length of the inputs to the subsequent calls to psa_aead_update_ad() and psa_aead_update(). See the documentation of psa_aead_set_lengths() for details.
- Call psa_aead_set_nonce() with the nonce for the decryption.
- Call psa_aead_update_ad() zero, one or more times, passing a fragment of the non-encrypted additional authenticated data each time.
- Call psa_aead_update() zero, one or more times, passing a fragment of the ciphertext to decrypt each time.
- Call psa_aead_verify().
If an error occurs at any step after a call to psa_aead_decrypt_setup(), the operation will need to be reset by a call to psa_aead_abort(). The application may call psa_aead_abort() at any time after the operation has been initialized.
After a successful call to psa_aead_decrypt_setup(), the application must eventually terminate the operation. The following events terminate an operation:
- A successful call to psa_aead_verify().
- A call to psa_aead_abort().
- Parameters
-
[in,out] operation
The operation object to set up. It must have been initialized as per the documentation for #psa_aead_operation_t and not yet in use. key
Identifier of the key to use for the operation. It must remain valid until the operation terminates. It must allow the usage PSA_KEY_USAGE_DECRYPT. alg
The AEAD algorithm to compute ( PSA_ALG_XXX
value such that PSA_ALG_IS_AEAD(alg
) is true).
- Return values
-
PSA_SUCCESS
Success. PSA_ERROR_BAD_STATE
The operation state is not valid (it must be inactive). PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_INVALID_ARGUMENT
key
is not compatible withalg
.PSA_ERROR_NOT_SUPPORTED
alg
is not supported or is not an AEAD algorithm.PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_aead_generate_nonce()
psa_status_t psa_aead_generate_nonce | ( | psa_aead_operation_t * | operation, |
uint8_t * | nonce, |
||
size_t | nonce_size, |
||
size_t * | nonce_length |
||
) |
Generate a random nonce for an authenticated encryption operation.
- Note
- Multipart AEAD is not implemented in this Silicon Labs release.
This function generates a random nonce for the authenticated encryption operation with an appropriate size for the chosen algorithm, key type and key size.
The application must call psa_aead_encrypt_setup() before calling this function.
If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().
- Parameters
-
[in,out] operation
Active AEAD operation. [out] nonce
Buffer where the generated nonce is to be written. nonce_size
Size of the nonce
buffer in bytes.[out] nonce_length
On success, the number of bytes of the generated nonce.
- Return values
-
PSA_SUCCESS
Success. PSA_ERROR_BAD_STATE
The operation state is not valid (it must be an active aead encrypt operation, with no nonce set). PSA_ERROR_BUFFER_TOO_SMALL
The size of the nonce
buffer is too small.PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_aead_set_nonce()
psa_status_t psa_aead_set_nonce | ( | psa_aead_operation_t * | operation, |
const uint8_t * | nonce, |
||
size_t | nonce_length |
||
) |
Set the nonce for an authenticated encryption or decryption operation.
- Note
- Multipart AEAD is not implemented in this Silicon Labs release.
This function sets the nonce for the authenticated encryption or decryption operation.
The application must call psa_aead_encrypt_setup() or psa_aead_decrypt_setup() before calling this function.
If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().
- Note
- When encrypting, applications should use psa_aead_generate_nonce() instead of this function, unless implementing a protocol that requires a non-random IV.
- Parameters
-
[in,out] operation
Active AEAD operation. [in] nonce
Buffer containing the nonce to use. nonce_length
Size of the nonce in bytes.
- Return values
-
PSA_SUCCESS
Success. PSA_ERROR_BAD_STATE
The operation state is not valid (it must be active, with no nonce set). PSA_ERROR_INVALID_ARGUMENT
The size of nonce
is not acceptable for the chosen algorithm.PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_aead_set_lengths()
psa_status_t psa_aead_set_lengths | ( | psa_aead_operation_t * | operation, |
size_t | ad_length, |
||
size_t | plaintext_length |
||
) |
Declare the lengths of the message and additional data for AEAD.
- Note
- Multipart AEAD is not implemented in this Silicon Labs release.
The application must call this function before calling psa_aead_update_ad() or psa_aead_update() if the algorithm for the operation requires it. If the algorithm does not require it, calling this function is optional, but if this function is called then the implementation must enforce the lengths.
You may call this function before or after setting the nonce with psa_aead_set_nonce() or psa_aead_generate_nonce().
- For PSA_ALG_CCM, calling this function is required.
- For the other AEAD algorithms defined in this specification, calling this function is not required.
- For vendor-defined algorithm, refer to the vendor documentation.
If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().
- Parameters
-
[in,out] operation
Active AEAD operation. ad_length
Size of the non-encrypted additional authenticated data in bytes. plaintext_length
Size of the plaintext to encrypt in bytes.
- Return values
-
PSA_SUCCESS
Success. PSA_ERROR_BAD_STATE
The operation state is not valid (it must be active, and psa_aead_update_ad() and psa_aead_update() must not have been called yet). PSA_ERROR_INVALID_ARGUMENT
At least one of the lengths is not acceptable for the chosen algorithm. PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_aead_update_ad()
psa_status_t psa_aead_update_ad | ( | psa_aead_operation_t * | operation, |
const uint8_t * | input, |
||
size_t | input_length |
||
) |
Pass additional data to an active AEAD operation.
- Note
- Multipart AEAD is not implemented in this Silicon Labs release.
Additional data is authenticated, but not encrypted.
You may call this function multiple times to pass successive fragments of the additional data. You may not call this function after passing data to encrypt or decrypt with psa_aead_update().
Before calling this function, you must:
- Call either psa_aead_encrypt_setup() or psa_aead_decrypt_setup().
- Set the nonce with psa_aead_generate_nonce() or psa_aead_set_nonce().
If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().
- Warning
- When decrypting, until psa_aead_verify() has returned PSA_SUCCESS, there is no guarantee that the input is valid. Therefore, until you have called psa_aead_verify() and it has returned PSA_SUCCESS, treat the input as untrusted and prepare to undo any action that depends on the input if psa_aead_verify() returns an error status.
- Parameters
-
[in,out] operation
Active AEAD operation. [in] input
Buffer containing the fragment of additional data. input_length
Size of the input
buffer in bytes.
- Return values
-
PSA_SUCCESS
Success. PSA_ERROR_BAD_STATE
The operation state is not valid (it must be active, have a nonce set, have lengths set if required by the algorithm, and psa_aead_update() must not have been called yet). PSA_ERROR_INVALID_ARGUMENT
The total input length overflows the additional data length that was previously specified with psa_aead_set_lengths(). PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_aead_update()
psa_status_t psa_aead_update | ( | psa_aead_operation_t * | operation, |
const uint8_t * | input, |
||
size_t | input_length, |
||
uint8_t * | output, |
||
size_t | output_size, |
||
size_t * | output_length |
||
) |
Encrypt or decrypt a message fragment in an active AEAD operation.
- Note
- Multipart AEAD is not implemented in this Silicon Labs release.
Before calling this function, you must:
- Call either psa_aead_encrypt_setup() or psa_aead_decrypt_setup(). The choice of setup function determines whether this function encrypts or decrypts its input.
- Set the nonce with psa_aead_generate_nonce() or psa_aead_set_nonce().
- Call psa_aead_update_ad() to pass all the additional data.
If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().
- Warning
- When decrypting, until psa_aead_verify() has returned PSA_SUCCESS, there is no guarantee that the input is valid. Therefore, until you have called psa_aead_verify() and it has returned PSA_SUCCESS:
- Do not use the output in any way other than storing it in a confidential location. If you take any action that depends on the tentative decrypted data, this action will need to be undone if the input turns out not to be valid. Furthermore, if an adversary can observe that this action took place (for example through timing), they may be able to use this fact as an oracle to decrypt any message encrypted with the same key.
- In particular, do not copy the output anywhere but to a memory or storage space that you have exclusive access to.
This function does not require the input to be aligned to any particular block boundary. If the implementation can only process a whole block at a time, it must consume all the input provided, but it may delay the end of the corresponding output until a subsequent call to psa_aead_update(), psa_aead_finish() or psa_aead_verify() provides sufficient input. The amount of data that can be delayed in this way is bounded by #PSA_AEAD_UPDATE_OUTPUT_SIZE.
- Parameters
-
[in,out] operation
Active AEAD operation. [in] input
Buffer containing the message fragment to encrypt or decrypt. input_length
Size of the input
buffer in bytes.[out] output
Buffer where the output is to be written. output_size
Size of the output
buffer in bytes. This must be appropriate for the selected algorithm and key:- A sufficient output size is #PSA_AEAD_UPDATE_OUTPUT_SIZE(
key_type
,alg
,input_length
) wherekey_type
is the type of key andalg
is the algorithm that were used to set up the operation. - #PSA_AEAD_UPDATE_OUTPUT_MAX_SIZE(
input_length
) evaluates to the maximum output size of any supported AEAD algorithm.
[out] output_length
On success, the number of bytes that make up the returned output. - A sufficient output size is #PSA_AEAD_UPDATE_OUTPUT_SIZE(
- Return values
-
PSA_SUCCESS
Success. PSA_ERROR_BAD_STATE
The operation state is not valid (it must be active, have a nonce set, and have lengths set if required by the algorithm). PSA_ERROR_BUFFER_TOO_SMALL
The size of the output
buffer is too small. #PSA_AEAD_UPDATE_OUTPUT_SIZE(key_type
,alg
,input_length
) or #PSA_AEAD_UPDATE_OUTPUT_MAX_SIZE(input_length
) can be used to determine the required buffer size.PSA_ERROR_INVALID_ARGUMENT
The total length of input to psa_aead_update_ad() so far is less than the additional data length that was previously specified with psa_aead_set_lengths(). PSA_ERROR_INVALID_ARGUMENT
The total input length overflows the plaintext length that was previously specified with psa_aead_set_lengths(). PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_aead_finish()
psa_status_t psa_aead_finish | ( | psa_aead_operation_t * | operation, |
uint8_t * | ciphertext, |
||
size_t | ciphertext_size, |
||
size_t * | ciphertext_length, |
||
uint8_t * | tag, |
||
size_t | tag_size, |
||
size_t * | tag_length |
||
) |
Finish encrypting a message in an AEAD operation.
- Note
- Multipart AEAD is not implemented in this Silicon Labs release.
The operation must have been set up with psa_aead_encrypt_setup().
This function finishes the authentication of the additional data formed by concatenating the inputs passed to preceding calls to psa_aead_update_ad() with the plaintext formed by concatenating the inputs passed to preceding calls to psa_aead_update().
This function has two output buffers:
ciphertext
contains trailing ciphertext that was buffered from preceding calls to psa_aead_update().tag
contains the authentication tag.
When this function returns successfuly, the operation becomes inactive. If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().
- Parameters
-
[in,out] operation
Active AEAD operation. [out] ciphertext
Buffer where the last part of the ciphertext is to be written. ciphertext_size
Size of the ciphertext
buffer in bytes. This must be appropriate for the selected algorithm and key:- A sufficient output size is #PSA_AEAD_FINISH_OUTPUT_SIZE(
key_type
,alg
) wherekey_type
is the type of key andalg
is the algorithm that were used to set up the operation. - #PSA_AEAD_FINISH_OUTPUT_MAX_SIZE evaluates to the maximum output size of any supported AEAD algorithm.
[out] ciphertext_length
On success, the number of bytes of returned ciphertext. [out] tag
Buffer where the authentication tag is to be written. tag_size
Size of the tag
buffer in bytes. This must be appropriate for the selected algorithm and key:- The exact tag size is #PSA_AEAD_TAG_LENGTH(
key_type
,key_bits
,alg
) wherekey_type
andkey_bits
are the type and bit-size of the key, andalg
is the algorithm that were used in the call to psa_aead_encrypt_setup(). - #PSA_AEAD_TAG_MAX_SIZE evaluates to the maximum tag size of any supported AEAD algorithm.
[out] tag_length
On success, the number of bytes that make up the returned tag. - A sufficient output size is #PSA_AEAD_FINISH_OUTPUT_SIZE(
- Return values
-
PSA_SUCCESS
Success. PSA_ERROR_BAD_STATE
The operation state is not valid (it must be an active encryption operation with a nonce set). PSA_ERROR_BUFFER_TOO_SMALL
The size of the ciphertext
ortag
buffer is too small. #PSA_AEAD_FINISH_OUTPUT_SIZE(key_type
,alg
) or #PSA_AEAD_FINISH_OUTPUT_MAX_SIZE can be used to determine the requiredciphertext
buffer size. #PSA_AEAD_TAG_LENGTH(key_type
,key_bits
,alg
) or #PSA_AEAD_TAG_MAX_SIZE can be used to determine the requiredtag
buffer size.PSA_ERROR_INVALID_ARGUMENT
The total length of input to psa_aead_update_ad() so far is less than the additional data length that was previously specified with psa_aead_set_lengths(). PSA_ERROR_INVALID_ARGUMENT
The total length of input to psa_aead_update() so far is less than the plaintext length that was previously specified with psa_aead_set_lengths(). PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_aead_verify()
psa_status_t psa_aead_verify | ( | psa_aead_operation_t * | operation, |
uint8_t * | plaintext, |
||
size_t | plaintext_size, |
||
size_t * | plaintext_length, |
||
const uint8_t * | tag, |
||
size_t | tag_length |
||
) |
Finish authenticating and decrypting a message in an AEAD operation.
- Note
- Multipart AEAD is not implemented in this Silicon Labs release.
The operation must have been set up with psa_aead_decrypt_setup().
This function finishes the authenticated decryption of the message components:
- The additional data consisting of the concatenation of the inputs passed to preceding calls to psa_aead_update_ad().
- The ciphertext consisting of the concatenation of the inputs passed to preceding calls to psa_aead_update().
- The tag passed to this function call.
If the authentication tag is correct, this function outputs any remaining plaintext and reports success. If the authentication tag is not correct, this function returns PSA_ERROR_INVALID_SIGNATURE.
When this function returns successfuly, the operation becomes inactive. If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().
- Note
- Implementations shall make the best effort to ensure that the comparison between the actual tag and the expected tag is performed in constant time.
- Parameters
-
[in,out] operation
Active AEAD operation. [out] plaintext
Buffer where the last part of the plaintext is to be written. This is the remaining data from previous calls to psa_aead_update() that could not be processed until the end of the input. plaintext_size
Size of the plaintext
buffer in bytes. This must be appropriate for the selected algorithm and key:- A sufficient output size is #PSA_AEAD_VERIFY_OUTPUT_SIZE(
key_type
,alg
) wherekey_type
is the type of key andalg
is the algorithm that were used to set up the operation. - #PSA_AEAD_VERIFY_OUTPUT_MAX_SIZE evaluates to the maximum output size of any supported AEAD algorithm.
[out] plaintext_length
On success, the number of bytes of returned plaintext. [in] tag
Buffer containing the authentication tag. tag_length
Size of the tag
buffer in bytes. - A sufficient output size is #PSA_AEAD_VERIFY_OUTPUT_SIZE(
- Return values
-
PSA_SUCCESS
Success. PSA_ERROR_INVALID_SIGNATURE
The calculations were successful, but the authentication tag is not correct. PSA_ERROR_BAD_STATE
The operation state is not valid (it must be an active decryption operation with a nonce set). PSA_ERROR_BUFFER_TOO_SMALL
The size of the plaintext
buffer is too small. #PSA_AEAD_VERIFY_OUTPUT_SIZE(key_type
,alg
) or #PSA_AEAD_VERIFY_OUTPUT_MAX_SIZE can be used to determine the required buffer size.PSA_ERROR_INVALID_ARGUMENT
The total length of input to psa_aead_update_ad() so far is less than the additional data length that was previously specified with psa_aead_set_lengths(). PSA_ERROR_INVALID_ARGUMENT
The total length of input to psa_aead_update() so far is less than the plaintext length that was previously specified with psa_aead_set_lengths(). PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_aead_abort()
psa_status_t psa_aead_abort | ( | psa_aead_operation_t * | operation | ) |
Abort an AEAD operation.
- Note
- Multipart AEAD is not implemented in this Silicon Labs release.
Aborting an operation frees all associated resources except for the operation
structure itself. Once aborted, the operation object can be reused for another operation by calling psa_aead_encrypt_setup() or psa_aead_decrypt_setup() again.
You may call this function any time after the operation object has been initialized as described in #psa_aead_operation_t.
In particular, calling psa_aead_abort() after the operation has been terminated by a call to psa_aead_abort(), psa_aead_finish() or psa_aead_verify() is safe and has no effect.
- Parameters
-
[in,out] operation
Initialized AEAD operation.
- Return values
-
PSA_SUCCESS
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
Macro Definition Documentation
◆ PSA_AEAD_OPERATION_INIT
#define PSA_AEAD_OPERATION_INIT {0, 0, 0, 0, 0, 0, 0, 0, 0, 0, {0}} |
This macro returns a suitable initializer for an AEAD operation object of type #psa_aead_operation_t.