Microcontroller functions
Description
Microcontroller functions.
Many of the supplied example applications use these microcontroller functions. See hal/micro/micro.h for source code.
- Note
- The term SFD refers to the Start Frame Delimiter.
See also hal/micro/cortexm3/micro.h for source code.
Functions | |
void | halInit (void) |
Initializes microcontroller-specific peripherals. | |
void | halReboot (void) |
Restarts the microcontroller and therefore everything else. | |
void | halInternalEnableWatchDog (void) |
Enables the watchdog timer. | |
void | halInternalDisableWatchDog (uint8_t magicKey) |
Disables the watchdog timer. | |
bool | halInternalWatchDogEnabled (void) |
Determines whether the watchdog has been enabled or disabled. | |
void | halResetWatchdog (void) |
void | halInternalSetCtune (uint16_t tune) |
Change the CTUNE value. | |
uint16_t | halInternalGetCtune (void) |
Get the CTUNE value. | |
uint8_t | halGetResetInfo (void) |
Gets information about what caused the microcontroller to reset. | |
const char * | halGetResetString (void) |
Calls halGetResetInfo() and supplies a string describing it. | |
void | halInternalSysReset (uint16_t extendedCause) |
Records the specified reset cause then forces a reboot. | |
uint16_t | halGetExtendedResetInfo (void) |
Returns the Extended Reset Cause information. | |
uint8_t | halGetEm2xxResetInfo (void) |
Calls halGetExtendedResetInfo() and translates the EM35x reset code to the corresponding value used by the EM2XX HAL. | |
const char * | halGetExtendedResetString (void) |
Calls halGetExtendedResetInfo() and supplies a string describing the extended cause of the reset. | |
Macros | |
#define | MICRO_DISABLE_WATCH_DOG_KEY 0xA5U |
The value that must be passed as the single parameter to halInternalDisableWatchDog() in order to successfully disable the watchdog timer. | |
#define | EM2XX_RESET_UNKNOWN 0 |
EM2xx-compatible reset code returned by halGetEm2xxResetInfo() | |
#define | EM2XX_RESET_EXTERNAL 1 |
#define | EM2XX_RESET_POWERON 2 |
#define | EM2XX_RESET_WATCHDOG 3 |
#define | EM2XX_RESET_ASSERT 6 |
#define | EM2XX_RESET_BOOTLOADER 9 |
#define | EM2XX_RESET_SOFTWARE 11 |
Vector Table Index Definitions | |
These are numerical definitions for vector table. Only Cortex-M standard exception vectors (indices 0 through 15) are represented since device specific vectors can be (and often are) different across dies. | |
#define | STACK_VECTOR_INDEX 0U |
A numerical definition for a vector. | |
#define | RESET_VECTOR_INDEX 1U |
#define | NMI_VECTOR_INDEX 2U |
#define | HARD_FAULT_VECTOR_INDEX 3U |
#define | MEMORY_FAULT_VECTOR_INDEX 4U |
#define | BUS_FAULT_VECTOR_INDEX 5U |
#define | USAGE_FAULT_VECTOR_INDEX 6U |
#define | RESERVED07_VECTOR_INDEX 7U |
#define | RESERVED08_VECTOR_INDEX 8U |
#define | RESERVED09_VECTOR_INDEX 9U |
#define | RESERVED10_VECTOR_INDEX 10U |
#define | SVCALL_VECTOR_INDEX 11U |
#define | DEBUG_MONITOR_VECTOR_INDEX 12U |
#define | RESERVED13_VECTOR_INDEX 13U |
#define | PENDSV_VECTOR_INDEX 14U |
#define | SYSTICK_VECTOR_INDEX 15U |
#define | IRQ_TO_VECTOR_NUMBER(x) ((x) + 16U) |
Utility macro to convert from IRQ numbers to exception numbers/ vector indices. | |
#define | VECTOR_TABLE_LENGTH (IRQ_TO_VECTOR_NUMBER(EXT_IRQ_COUNT)) |
Number of vectors. | |
Function Documentation
◆ halInit()
void halInit | ( | void |
| ) |
Initializes microcontroller-specific peripherals.
◆ halReboot()
void halReboot | ( | void |
| ) |
Restarts the microcontroller and therefore everything else.
◆ halInternalEnableWatchDog()
void halInternalEnableWatchDog | ( | void |
| ) |
Enables the watchdog timer.
◆ halInternalDisableWatchDog()
void halInternalDisableWatchDog | ( | uint8_t | magicKey | ) |
Disables the watchdog timer.
- Note
- To prevent the watchdog from being disabled accidentally, a magic key must be provided.
- Parameters
-
magicKey
A value (MICRO_DISABLE_WATCH_DOG_KEY) that enables the function.
◆ halInternalWatchDogEnabled()
bool halInternalWatchDogEnabled | ( | void |
| ) |
Determines whether the watchdog has been enabled or disabled.
- Returns
- A bool value indicating if the watchdog is current enabled.
◆ halInternalSetCtune()
void halInternalSetCtune | ( | uint16_t | tune | ) |
Change the CTUNE value.
Involves switching to HFRCO and turning off the HFXO temporarily.
- Parameters
-
tune
Value to set CTUNE to.
◆ halInternalGetCtune()
uint16_t halInternalGetCtune | ( | void |
| ) |
Get the CTUNE value.
- Returns
- Current CTUNE value.
◆ halGetResetInfo()
uint8_t halGetResetInfo | ( | void |
| ) |
Gets information about what caused the microcontroller to reset.
- Returns
- A code identifying the cause of the reset.
◆ halGetResetString()
const char* halGetResetString | ( | void |
| ) |
Calls halGetResetInfo() and supplies a string describing it.
@appusage Useful for diagnostic printing of text just after program initialization.
- Returns
- A pointer to a program space string.
◆ halInternalSysReset()
void halInternalSysReset | ( | uint16_t | extendedCause | ) |
Records the specified reset cause then forces a reboot.
◆ halGetExtendedResetInfo()
uint16_t halGetExtendedResetInfo | ( | void |
| ) |
Returns the Extended Reset Cause information.
- Returns
- A 16-bit code identifying the base and extended cause of the reset
◆ halGetEm2xxResetInfo()
uint8_t halGetEm2xxResetInfo | ( | void |
| ) |
Calls halGetExtendedResetInfo() and translates the EM35x reset code to the corresponding value used by the EM2XX HAL.
Any reset codes not present in the EM2XX are returned after being OR'ed with 0x80.
@appusage Used by the EZSP host as a platform-independent NCP reset code.
- Returns
- The EM2XX-compatible reset code. If not supported by the EM2XX, return the platform-specific code with B7 set.
◆ halGetExtendedResetString()
const char* halGetExtendedResetString | ( | void |
| ) |
Calls halGetExtendedResetInfo() and supplies a string describing the extended cause of the reset.
halGetResetString() should also be called to get the string for the base reset cause
@appusage Useful for diagnostic printing of text just after program initialization.
- Returns
- A pointer to a program space string.
Macro Definition Documentation
◆ MICRO_DISABLE_WATCH_DOG_KEY
#define MICRO_DISABLE_WATCH_DOG_KEY 0xA5U |
The value that must be passed as the single parameter to halInternalDisableWatchDog() in order to successfully disable the watchdog timer.
◆ STACK_VECTOR_INDEX
#define STACK_VECTOR_INDEX 0U |
A numerical definition for a vector.
◆ IRQ_TO_VECTOR_NUMBER
#define IRQ_TO_VECTOR_NUMBER | ( | x | ) | ((x) + 16U) |
Utility macro to convert from IRQ numbers to exception numbers/ vector indices.
These are different because the latter include the Cortex-M standard exceptions while the former do not.
◆ VECTOR_TABLE_LENGTH
#define VECTOR_TABLE_LENGTH (IRQ_TO_VECTOR_NUMBER(EXT_IRQ_COUNT)) |
Number of vectors.
EXT_IRQ_COUNT is defined in the device header but does not include the Cortex-M standard exceptions.
◆ EM2XX_RESET_UNKNOWN
#define EM2XX_RESET_UNKNOWN 0 |
EM2xx-compatible reset code returned by halGetEm2xxResetInfo()