Legacy HAL
Description
The Legacy HAL is an implementation of the Hardware Abstraction Layer (HAL) that was used by the Zigbee EmberZNet and Flex Connect stacks before their transition to the new component-based architecture (Zigbee version 7.0 and Connect version 3.0). This component is not a complete duplicate of the old HAL. It only contains the most commonly used pieces to enable our networking stacks and sample applications and to support porting customer applications to the new component-based implementation. Currently, Zigbee and Connect sample applications are dependent on this component. Eventually, they will be ported to use new HAL components directly so that this component can become optional or be deprecated.
- Note
- This component is only designed to be used with Zigbee and Connect stack applications. Do not use with any other stacks as it will likely introduce problems.
Modules |
|
| Application Bootloader Interface | |
|
Definition of the application bootloader interface.
|
|
| Button | |
|
Sample API functions for using push-buttons.
|
|
| Common Bootloader | |
|
Common bootloader interface defines and functions.
|
|
| Cyclic Redundancy Check | |
|
Functions that provide access to cyclic redundancy code (CRC) calculation. See crc.h for source code.
|
|
| Diagnostics | |
|
Crash and watchdog diagnostic functions.
|
|
| LED | |
|
Sample API funtions for controlling LEDs.
|
|
| Microcontroller functions | |
|
Microcontroller functions.
|
|
| Random generation | |
|
Functions that provide access to random numbers.
|
|
| Reset Cause Definitions | |
|
Definitions for all the reset cause types.
|
|
| SimEE2 to NVM3 Upgrade | |
| Simulated EEPROM 1 and 2 | |
|
Simulated EEPROM 1 and 2 legacy storage.
|
|
| Standalone Bootloader | |
|
Definition of the standalone bootloader interface.
|
|
Data Structures |
|
| struct | HalEepromInformationType |
|
This structure defines a variety of information about the attached external EEPROM device.
|
|
| struct | EepromStateType |
Functions |
|
| const HalEepromInformationType * | halEepromInfo (void) |
|
Call this function to get information about the external EEPROM and its capabilities.
|
|
| uint16_t | halCommonGetInt16uMillisecondTick (void) |
| uint32_t | halCommonGetInt32uMillisecondTick (void) |
| uint64_t | halCommonGetInt64uMillisecondTick (void) |
| uint16_t | halCommonGetInt16uQuarterSecondTick (void) |
| uint16_t | halInternalStartSystemTimer (void) |
| void | halCommonDelayMicroseconds (uint16_t us) |
| void | halCommonDelayMilliseconds (uint16_t ms) |
| EmberStatus | halCommonIdleForMilliseconds (uint32_t *duration) |
| void | halStackSymbolDelayAIsr (void) |
| void | halStackRadioPowerMainControl (bool powerUp) |
| void | halStackRadioPowerUpBoard (void) |
| void | halStackRadioPowerDownBoard (void) |
| void | halStackProcessBootCount (void) |
| EmberStatus | emDebugInit (void) |
| void | emRadioSeedRandom (void) |
Macros |
|
| #define | EEPROM_PAGE_SIZE (128ul) |
|
Definition of an EEPROM page size, in bytes.
|
|
| #define | EEPROM_FIRST_PAGE (0) |
|
Define the location of the first page in EEPROM.
|
|
| #define | EEPROM_IMAGE_START ( EEPROM_FIRST_PAGE * EEPROM_PAGE_SIZE ) |
|
Define the location of the image start in EEPROM as a function of the
EEPROM_FIRST_PAGE
and
EEPROM_PAGE_SIZE
.
|
|
| #define | EEPROM_SUCCESS 0U |
|
Define EEPROM success status.
|
|
| #define | EEPROM_ERR 1U |
|
Define EEPROM error status.
|
|
| #define | EEPROM_ERR_MASK 0x80U |
|
Define EEPROM error mask.
|
|
| #define | EEPROM_ERR_PG_BOUNDARY 0x81U |
|
Define EEPROM page boundary error.
|
|
| #define | EEPROM_ERR_PG_SZ 0x82U |
|
Define EEPROM page size error.
|
|
| #define | EEPROM_ERR_WRT_DATA 0x83U |
|
Define EEPROM write data error.
|
|
| #define | EEPROM_ERR_IMG_SZ 0x84U |
|
Define EEPROM image too large error.
|
|
| #define | EEPROM_ERR_ADDR 0x85U |
|
Define EEPROM invalid address error.
|
|
| #define | EEPROM_ERR_INVALID_CHIP 0x86U |
|
Define EEPROM chip initialization error.
|
|
| #define | EEPROM_ERR_ERASE_REQUIRED 0x87U |
|
Define EEPROM erase required error.
|
|
| #define | EEPROM_ERR_NO_ERASE_SUPPORT 0x88U |
|
Define EEPROM error for no erase support.
|
|
| #define | EEPROM_INFO_VERSION (0x0202) |
|
The current version of the
HalEepromInformationType
data structure.
|
|
| #define | EEPROM_INFO_MAJOR_VERSION (0x0200) |
| #define | EEPROM_INFO_MAJOR_VERSION_MASK (0xFF00) |
| #define | EEPROM_INFO_MIN_VERSION_WITH_WORD_SIZE_SUPPORT 0x0102U |
| #define | EEPROM_CAPABILITIES_ERASE_SUPPORTED (0x0001U) |
|
Eeprom capabilites mask that indicates the erase API is supported.
|
|
| #define | EEPROM_CAPABILITIES_PAGE_ERASE_REQD (0x0002U) |
|
Eeprom capabilites mask that indicates page erasing is required before new data can be written to a device.
|
|
| #define | EEPROM_CAPABILITIES_BLOCKING_WRITE (0x0004U) |
|
Eeprom capabilites mask that indicates that the write routine is blocking on this device.
|
|
| #define | EEPROM_CAPABILITIES_BLOCKING_ERASE (0x0008U) |
|
Eeprom capabilites mask that indicates that the erase routine is blocking on this device.
|
|
| #define | EEPROM_CAPABILITIES_PART_ERASE_SECONDS (0x0010U) |
|
Eeprom capabilities mask that indicateds that the partEraseTime field of
HalEepromInformationType
is in seconds instead of the usual millisecondss.
|
|
| #define | simulatedTimePasses () |
Function Documentation
◆ halEepromInfo()
| const HalEepromInformationType * halEepromInfo | ( | void |
|
) |
Call this function to get information about the external EEPROM and its capabilities.
The format of this call must not be altered. However, the content can be changed to work with a different device.
- Returns
- A pointer to a HalEepromInformationType data structure, or NULL if the driver does not support this API
Macro Definition Documentation
◆ EEPROM_PAGE_SIZE
| #define EEPROM_PAGE_SIZE (128ul) |
Definition of an EEPROM page size, in bytes.
This definition is deprecated, and should no longer be used.
◆ EEPROM_FIRST_PAGE
| #define EEPROM_FIRST_PAGE (0) |
Define the location of the first page in EEPROM.
This definition is deprecated, and should no longer be used.
◆ EEPROM_IMAGE_START
| #define EEPROM_IMAGE_START ( EEPROM_FIRST_PAGE * EEPROM_PAGE_SIZE ) |
Define the location of the image start in EEPROM as a function of the EEPROM_FIRST_PAGE and EEPROM_PAGE_SIZE .
This definition is deprecated, and should no longer be used.
◆ EEPROM_SUCCESS
| #define EEPROM_SUCCESS 0U |
Define EEPROM success status.
◆ EEPROM_ERR
| #define EEPROM_ERR 1U |
Define EEPROM error status.
◆ EEPROM_ERR_MASK
| #define EEPROM_ERR_MASK 0x80U |
Define EEPROM error mask.
◆ EEPROM_ERR_PG_BOUNDARY
| #define EEPROM_ERR_PG_BOUNDARY 0x81U |
Define EEPROM page boundary error.
◆ EEPROM_ERR_PG_SZ
| #define EEPROM_ERR_PG_SZ 0x82U |
Define EEPROM page size error.
◆ EEPROM_ERR_WRT_DATA
| #define EEPROM_ERR_WRT_DATA 0x83U |
Define EEPROM write data error.
◆ EEPROM_ERR_IMG_SZ
| #define EEPROM_ERR_IMG_SZ 0x84U |
Define EEPROM image too large error.
◆ EEPROM_ERR_ADDR
| #define EEPROM_ERR_ADDR 0x85U |
Define EEPROM invalid address error.
◆ EEPROM_ERR_INVALID_CHIP
| #define EEPROM_ERR_INVALID_CHIP 0x86U |
Define EEPROM chip initialization error.
◆ EEPROM_ERR_ERASE_REQUIRED
| #define EEPROM_ERR_ERASE_REQUIRED 0x87U |
Define EEPROM erase required error.
◆ EEPROM_ERR_NO_ERASE_SUPPORT
| #define EEPROM_ERR_NO_ERASE_SUPPORT 0x88U |
Define EEPROM error for no erase support.
◆ EEPROM_INFO_VERSION
| #define EEPROM_INFO_VERSION (0x0202) |
The current version of the HalEepromInformationType data structure.
◆ EEPROM_CAPABILITIES_ERASE_SUPPORTED
| #define EEPROM_CAPABILITIES_ERASE_SUPPORTED (0x0001U) |
Eeprom capabilites mask that indicates the erase API is supported.
◆ EEPROM_CAPABILITIES_PAGE_ERASE_REQD
| #define EEPROM_CAPABILITIES_PAGE_ERASE_REQD (0x0002U) |
Eeprom capabilites mask that indicates page erasing is required before new data can be written to a device.
◆ EEPROM_CAPABILITIES_BLOCKING_WRITE
| #define EEPROM_CAPABILITIES_BLOCKING_WRITE (0x0004U) |
Eeprom capabilites mask that indicates that the write routine is blocking on this device.
◆ EEPROM_CAPABILITIES_BLOCKING_ERASE
| #define EEPROM_CAPABILITIES_BLOCKING_ERASE (0x0008U) |
Eeprom capabilites mask that indicates that the erase routine is blocking on this device.
◆ EEPROM_CAPABILITIES_PART_ERASE_SECONDS
| #define EEPROM_CAPABILITIES_PART_ERASE_SECONDS (0x0010U) |
Eeprom capabilities mask that indicateds that the partEraseTime field of HalEepromInformationType is in seconds instead of the usual millisecondss.