cli_storage_ram_t Struct Reference
Struct representing an instance of the CLI storage RAM.
#include <sl_cli_storage_ram.h>
Data Fields |
|
| sl_cli_handle_t | cli_handle |
|
The CLI instance associated with this instance.
|
|
| char * | prompt |
|
The command prompt.
|
|
| char * | end_string |
|
The string that define the end of definition.
|
|
| size_t | ram_size |
|
The number of command lines that can be stored in RAM.
|
|
| size_t | ram_next |
|
The next free line in RAM.
|
|
| char * | ram_buffer |
|
Pointer to the RAM buffer.
|
|
| bool | execute_while_define |
|
True if the command shell execute when defined.
|
|
| bool | define_in_progress |
|
True when definition is in progress.
|
|
| bool | execute_in_progress |
|
True when execute is in progress.
|
|
Struct representing an instance of the CLI storage RAM.
Field Documentation
◆ cli_handle
| sl_cli_handle_t cli_storage_ram_t::cli_handle |
The CLI instance associated with this instance.
◆ prompt
| char* cli_storage_ram_t::prompt |
The command prompt.
◆ end_string
| char* cli_storage_ram_t::end_string |
The string that define the end of definition.
◆ ram_size
| size_t cli_storage_ram_t::ram_size |
The number of command lines that can be stored in RAM.
◆ ram_next
| size_t cli_storage_ram_t::ram_next |
The next free line in RAM.
◆ ram_buffer
| char* cli_storage_ram_t::ram_buffer |
Pointer to the RAM buffer.
◆ execute_while_define
| bool cli_storage_ram_t::execute_while_define |
True if the command shell execute when defined.
◆ define_in_progress
| bool cli_storage_ram_t::define_in_progress |
True when definition is in progress.
◆ execute_in_progress
| bool cli_storage_ram_t::execute_in_progress |
True when execute is in progress.