RAM execution disable

Description

RAM execution disable utilities can be used to disable execution from RAM and other selected memory regions.

RAM execution disable utilities are useful to protect against code injection attacks. These utilities make use of MPU to disable execution from RAM and other selected memory regions.

Functions

void sl_mpu_disable_execute_from_ram (void)
Configures internal SRAM as non-executable and enable MPU.
sl_status_t sl_mpu_disable_execute (uint32_t address_begin, uint32_t address_end, uint32_t size)
Configures an address range as non-executable and enable MPU.

Function Documentation

sl_mpu_disable_execute_from_ram()

void sl_mpu_disable_execute_from_ram ( void )

Configures internal SRAM as non-executable and enable MPU.

Note
This function configures the MPU in order to make the entire RAM as non-executable (with the exception of the functions marked as ramfunc).

sl_mpu_disable_execute()

sl_status_t sl_mpu_disable_execute ( uint32_t address_begin,
uint32_t address_end,
uint32_t size
)

Configures an address range as non-executable and enable MPU.

Note
Configures a MPU region in order to make an address range as non-executable. The memory region must have a size of at least 32 bytes.
Parameters
address_begin Beginning of memory segment.
address_end End of memory segment.
size Size of memory segment.
Returns
0 if successful. Error code otherwise.