Built-in keys
Description
Macros |
|
| #define | MBEDTLS_PSA_KEY_ID_BUILTIN_MIN (( psa_key_id_t )0x7fff0000) |
|
The minimum value for a key identifier that is built into the implementation.
|
|
| #define | MBEDTLS_PSA_KEY_ID_BUILTIN_MAX (( psa_key_id_t )0x7fffefff) |
|
The maximum value for a key identifier that is built into the implementation.
|
|
Typedefs |
|
| typedef uint64_t | psa_drv_slot_number_t |
|
A slot number identifying a key in a driver.
|
|
Macro Definition Documentation
◆ MBEDTLS_PSA_KEY_ID_BUILTIN_MIN
| #define MBEDTLS_PSA_KEY_ID_BUILTIN_MIN (( psa_key_id_t )0x7fff0000) |
The minimum value for a key identifier that is built into the implementation.
The range of key identifiers from MBEDTLS_PSA_KEY_ID_BUILTIN_MIN to MBEDTLS_PSA_KEY_ID_BUILTIN_MAX within the range from PSA_KEY_ID_VENDOR_MIN and PSA_KEY_ID_VENDOR_MAX and must not intersect with any other set of implementation-chosen key identifiers.
This value is part of the library's ABI since changing it would invalidate the values of built-in key identifiers in applications.
◆ MBEDTLS_PSA_KEY_ID_BUILTIN_MAX
| #define MBEDTLS_PSA_KEY_ID_BUILTIN_MAX (( psa_key_id_t )0x7fffefff) |
The maximum value for a key identifier that is built into the implementation.
See MBEDTLS_PSA_KEY_ID_BUILTIN_MIN for more information.
Typedef Documentation
◆ psa_drv_slot_number_t
| typedef uint64_t psa_drv_slot_number_t |
A slot number identifying a key in a driver.
Values of this type are used to identify built-in keys.