LFRCO Initialization
Description
Initialize the LFRCO oscillator.
Initialize the low frequency RC oscillator. On Series 2 devices with precision mode support, the precision mode is configured in the configuration header
sl_device_init_lfrco_config.h
. On other devices, there is nothing to configure.
If using Simplicity Studio, this configuration header is also configurable through the Project Configurator, by selecting the "Device Init: LFRCO" configuration component.
Functions |
|
| sl_status_t | sl_device_init_lfrco (void) |
|
Initialize LFRCO.
|
|
Function Documentation
◆ sl_device_init_lfrco()
| sl_status_t sl_device_init_lfrco | ( | void |
|
) |
Initialize LFRCO.
Initialize the low frequency RC oscillator. On devices that support high precision mode, this function configures the precision mode based on the configuration option SL_DEVICE_INIT_LFRCO_PRECISION.
- Returns
- Status code
- Return values
-
SL_STATUS_OKLFRCO initialized successfully