CPC

Description

CPC.

Overview

TODO

Initialization

TODO

Data Structures

struct sl_cpc_endpoint_handle_t
Struct representing an CPC endpoint handle.
struct sl_cpc_endpoint_debug_counters_t
Struct representing CPC Core debug stats.
struct sl_cpc_core_debug_counters_t
Struct representing CPC Core debug counters.
struct sl_cpc_mem_pool_handle_t
Struct representing a memory pool handle.
struct sl_cpc_debug_memory_t
Struct representing a memory pool debug.

Functions

sl_status_t sl_cpc_init (void)
Initialize CPC module.
sl_status_t sl_cpc_open_user_endpoint ( sl_cpc_endpoint_handle_t *endpoint_handle, sl_cpc_user_endpoint_id_t id, uint8_t flags, uint8_t tx_window_size)
The baremetal process action function.
sl_status_t sl_cpc_set_endpoint_option ( sl_cpc_endpoint_handle_t *endpoint_handle, sl_cpc_endpoint_option_t option, void *value)
Set endpoint option.
sl_status_t sl_cpc_close_endpoint ( sl_cpc_endpoint_handle_t *endpoint_handle)
Close endpoint.
sl_status_t sl_cpc_abort_read ( sl_cpc_endpoint_handle_t *endpoint_handle)
Abort read.
sl_status_t sl_cpc_read ( sl_cpc_endpoint_handle_t *endpoint_handle, void **data, uint16_t *data_length, uint32_t timeout, uint8_t flags)
Read Data.
sl_status_t sl_cpc_write ( sl_cpc_endpoint_handle_t *endpoint_handle, void *data, uint16_t data_length, uint8_t flag, void *on_write_completed_arg)
Write Data.
sl_cpc_endpoint_state_t sl_cpc_get_endpoint_state ( sl_cpc_endpoint_handle_t *endpoint_handle)
Get endpoint state.
sl_status_t sl_cpc_free_rx_buffer (void *data)
Free buffer returned by sl_cpc_read() .

Macros

#define SL_CPC_OPEN_ENDPOINT_FLAG_NONE 0
#define SL_CPC_USER_ENDPOINT_ID_START ((uint8_t) SL_CPC_ENDPOINT_USER_ID_0 )
#define SL_CPC_USER_ENDPOINT_ID_END ((uint8_t)( SL_CPC_ENDPOINT_USER_ID_0 + SL_CPC_USER_ENDPOINT_MAX_COUNT - 1))
#define SL_CPC_FLAG_NO_BLOCK 0x01
#define SL_CPC_APP_DATA_MAX_LENGTH (4087)
#define SL_CPC_TRANSMIT_WINDOW_MIN_SIZE 1
#define SL_CPC_TRANSMIT_WINDOW_MAX_SIZE 1

Typedefs

typedef void(* sl_cpc_on_write_completed_t ) ( sl_cpc_user_endpoint_id_t endpoint_id, void *buffer, void *arg, sl_status_t status)
typedef void(* sl_cpc_on_data_reception_t ) (uint8_t endpoint_id, void *arg)
typedef void(* sl_cpc_on_error_callback_t ) (uint8_t endpoint_id, void *arg)
typedef void(* sl_cpc_on_poll_t ) (uint8_t endpoint_id, void *arg, void *poll_data, uint32_t poll_data_length, void **reply_data, uint32_t *reply_data_lenght, void **on_write_complete_arg)
typedef void(* sl_cpc_on_final_t ) (uint8_t endpoint_id, void *arg, void *answer, uint32_t answer_lenght)

Enumerations

enum sl_cpc_user_endpoint_id_t {
SL_CPC_ENDPOINT_USER_ID_0 = 90,
SL_CPC_ENDPOINT_USER_ID_1 = 91,
SL_CPC_ENDPOINT_USER_ID_2 = 92,
SL_CPC_ENDPOINT_USER_ID_3 = 93,
SL_CPC_ENDPOINT_USER_ID_4 = 94,
SL_CPC_ENDPOINT_USER_ID_5 = 95,
SL_CPC_ENDPOINT_USER_ID_6 = 96,
SL_CPC_ENDPOINT_USER_ID_7 = 97,
SL_CPC_ENDPOINT_USER_ID_8 = 98,
SL_CPC_ENDPOINT_USER_ID_9 = 99
}
Enumeration representing user endpoint.
enum sl_cpc_endpoint_state_t {
SL_CPC_STATE_OPEN = 0,
SL_CPC_STATE_CLOSED ,
SL_CPC_STATE_CLOSING ,
SL_CPC_STATE_ERROR_DESTINATION_UNREACHABLE ,
SL_CPC_STATE_ERROR_SECURITY_INCIDENT ,
SL_CPC_STATE_ERROR_FAULT ,
SL_CPC_STATE_FREED
}
Enumeration representing the possible endpoint state.
enum sl_cpc_endpoint_option_t {
SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE = 0,
SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE_ARG ,
SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE ,
SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE_ARG ,
SL_CPC_ENDPOINT_ON_IFRAME_WRITE_COMPLETED ,
SL_CPC_ENDPOINT_ON_UFRAME_WRITE_COMPLETED ,
SL_CPC_ENDPOINT_ON_POLL ,
SL_CPC_ENDPOINT_ON_POLL_ARG ,
SL_CPC_ENDPOINT_ON_FINAL ,
SL_CPC_ENDPOINT_ON_FINAL_ARG ,
SL_CPC_ENDPOINT_ON_ERROR ,
SL_CPC_ENDPOINT_ON_ERROR_ARG
}
Enumeration representing the possible configurable options for an endpoint.

Function Documentation

◆ sl_cpc_init()

sl_status_t sl_cpc_init ( void )

Initialize CPC module.

Returns
Status code

◆ sl_cpc_open_user_endpoint()

sl_status_t sl_cpc_open_user_endpoint ( sl_cpc_endpoint_handle_t * endpoint_handle,
sl_cpc_user_endpoint_id_t id,
uint8_t flags,
uint8_t tx_window_size
)

The baremetal process action function.

Open endpoint

Parameters
[in] endpoint_handle Endpoint handle
[in] id Endpoint ID
[in] flags Endpoint type flags
[in] tx_window_size Transmit window size
Returns
Status code

◆ sl_cpc_set_endpoint_option()

sl_status_t sl_cpc_set_endpoint_option ( sl_cpc_endpoint_handle_t * endpoint_handle,
sl_cpc_endpoint_option_t option,
void * value
)

Set endpoint option.

Parameters
[in] endpoint_handle Endpoint handle
[in] option Endpoint Option to set
[in] value Option value
Returns
Status code
Note
Options are as follow:

SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE: Set an on iframe receive callback. value is a sl_cpc_on_data_reception_t type.

SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE_ARG: Set an on iframe receive argument.

SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE: Set an on uframe receive callback. value is a sl_cpc_on_data_reception_t type.

SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE_ARG: Set an on uframe receive argument.

SL_CPC_ENDPOINT_ON_IFRAME_WRITE_COMPLETED: Set an on iframe write completed callback. value is a sl_cpc_on_write_completed_t type.

SL_CPC_ENDPOINT_ON_UFRAME_WRITE_COMPLETED: Set an on uframe write completed callback. value is a sl_cpc_on_write_completed_t type.

SL_CPC_ENDPOINT_ON_POLL: Set an on poll callback. value is a sl_cpc_on_poll_t type.

SL_CPC_ENDPOINT_ON_POLL_ARG: Set an on poll callback argument.

SL_CPC_ENDPOINT_ON_FINAL: Set an on final callback. value is a sl_cpc_on_final_t type.

SL_CPC_ENDPOINT_ON_FINAL_ARG: Set an on final callback argument.

SL_CPC_ENDPOINT_ON_ERROR: Set an on error callback. value is a sl_cpc_on_error_callback_t type.

SL_CPC_ENDPOINT_ON_ERROR_ARG: Set an on error callback argument.

◆ sl_cpc_close_endpoint()

sl_status_t sl_cpc_close_endpoint ( sl_cpc_endpoint_handle_t * endpoint_handle )

Close endpoint.

Parameters
[in] endpoint_handle Endpoint handle
Returns
Status code

◆ sl_cpc_abort_read()

sl_status_t sl_cpc_abort_read ( sl_cpc_endpoint_handle_t * endpoint_handle )

Abort read.

Parameters
[in] endpoint_handle Endpoint handle
Returns
Status code
Note
This function can be called from an ISR.

◆ sl_cpc_read()

sl_status_t sl_cpc_read ( sl_cpc_endpoint_handle_t * endpoint_handle,
void ** data,
uint16_t * data_length,
uint32_t timeout,
uint8_t flags
)

Read Data.

Parameters
[in] endpoint_handle Endpoint handle
[out] data Address of the variable that will receive the data pointer.
[out] data_length Length of the data contained in the buffer.
[in] timeout Timeout in ticks for the read operation. (Requires RTOS) Note: No effect if SL_CPC_FLAG_NO_BLOCK is provided as a flag
[in] flags Optional flags. i.g. SL_CPC_FLAG_NO_BLOCK Note: SL_CPC_FLAG_NO_BLOCK will cause the function to return SL_STATUS_EMPTY on baremetal applications
Returns
Status code

◆ sl_cpc_write()

sl_status_t sl_cpc_write ( sl_cpc_endpoint_handle_t * endpoint_handle,
void * data,
uint16_t data_length,
uint8_t flag,
void * on_write_completed_arg
)

Write Data.

Parameters
[in] endpoint_handle Endpoint handle
[in] data Pointer to data buffer.
[in] data_length Length of the data contained in the buffer.
[in] flags Optional flags.
[in] on_write_completed_arg Argument that will be passed to on_write_completed().
Returns
Status code
Note
This function cannot be called from an ISR.

◆ sl_cpc_get_endpoint_state()

sl_cpc_endpoint_state_t sl_cpc_get_endpoint_state ( sl_cpc_endpoint_handle_t * endpoint_handle )

Get endpoint state.

Parameters
[in] endpoint_handle Endpoint handle
Returns
Endpoint state

◆ sl_cpc_free_rx_buffer()

sl_status_t sl_cpc_free_rx_buffer ( void * data )

Free buffer returned by sl_cpc_read() .

Parameters
[in] data Pointer to data buffer to free.
Returns
Status code

Enumeration Type Documentation

◆ sl_cpc_user_endpoint_id_t

Enumeration representing user endpoint.

Enumerator
SL_CPC_ENDPOINT_USER_ID_0

User endpoint ID 0.

SL_CPC_ENDPOINT_USER_ID_1

User endpoint ID 1.

SL_CPC_ENDPOINT_USER_ID_2

User endpoint ID 2.

SL_CPC_ENDPOINT_USER_ID_3

User endpoint ID 3.

SL_CPC_ENDPOINT_USER_ID_4

User endpoint ID 4.

SL_CPC_ENDPOINT_USER_ID_5

User endpoint ID 5.

SL_CPC_ENDPOINT_USER_ID_6

User endpoint ID 6.

SL_CPC_ENDPOINT_USER_ID_7

User endpoint ID 7.

SL_CPC_ENDPOINT_USER_ID_8

User endpoint ID 8.

SL_CPC_ENDPOINT_USER_ID_9

User endpoint ID 9.

◆ sl_cpc_endpoint_state_t

Enumeration representing the possible endpoint state.

Enumerator
SL_CPC_STATE_OPEN

State open.

SL_CPC_STATE_CLOSED

State close.

SL_CPC_STATE_CLOSING

State closing.

SL_CPC_STATE_ERROR_DESTINATION_UNREACHABLE

Error state, destination unreachable.

SL_CPC_STATE_ERROR_SECURITY_INCIDENT

Error state, security incident.

SL_CPC_STATE_ERROR_FAULT

Error state, fault.

SL_CPC_STATE_FREED

State freed.

◆ sl_cpc_endpoint_option_t

Enumeration representing the possible configurable options for an endpoint.

Enumerator
SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE

Option: iframe receive.

SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE_ARG

Option: iframe receive argument.

SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE

Option: uframe receive.

SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE_ARG

Option: uframe receive argument.

SL_CPC_ENDPOINT_ON_IFRAME_WRITE_COMPLETED

Option: iframe write completed.

SL_CPC_ENDPOINT_ON_UFRAME_WRITE_COMPLETED

Option: uframe write completed.

SL_CPC_ENDPOINT_ON_POLL

Option: on poll.

SL_CPC_ENDPOINT_ON_POLL_ARG

Option: on poll argument.

SL_CPC_ENDPOINT_ON_FINAL

Option: on final.

SL_CPC_ENDPOINT_ON_FINAL_ARG

Option: on final argument.

SL_CPC_ENDPOINT_ON_ERROR

Option: on error.

SL_CPC_ENDPOINT_ON_ERROR_ARG

Option: on error argument.