NVIC Initialization
Description
Initialize the NVIC Interrupt Handlers priority.
Set all interrupt priorities, except the Fault exceptions, to
CORE_INTERRUPT_DEFAULT_PRIORITY
value.
When the Device Init NVIC module is present and no configuration overwrites the em_core
CORE_ATOMIC_METHOD
define, the atomic method is automatically set to BASEPRI (
CORE_ATOMIC_METHOD_BASEPRI
).
Functions |
|
| sl_status_t | sl_device_init_nvic (void) |
|
Sets default priority for all configurable interrupts in NVIC.
|
|
Function Documentation
◆ sl_device_init_nvic()
| sl_status_t sl_device_init_nvic | ( | void |
|
) |
Sets default priority for all configurable interrupts in NVIC.
- Returns
- Status code