HFRCO Initialization
Description
Initialize the HFRCO oscillator.
Configure the frequency band of the HFRCO. The configuration define SL_DEVICE_INIT_HFRCO_BAND is used to configure the frequency. If using Simplicity Studio, this configuration header is also configurable through the Project Configurator, by selecting the "Device Init: HFRCO" configuration component.
Functions |
|
| sl_status_t | sl_device_init_hfrco (void) |
|
Initialize HFRCO.
|
|
Function Documentation
◆ sl_device_init_hfrco()
| sl_status_t sl_device_init_hfrco | ( | void |
|
) |
Initialize HFRCO.
Configure the frequency band of the HFRCO. The configuration define SL_DEVICE_INIT_HFRCO_BAND is used to configure the frequency.
- Returns
- Status code
- Return values
-
SL_STATUS_OKHFRCO initialized successfully