Simple RGB PWM LED Driver
Description
Simple Red/Green/Blue PWM LED Driver.
Introduction
The Simple RGB PWM LED Driver is a module for the LED driver that provides functionality for controlling Red/Green/Blue LEDs that are driven by PWM.
RGB PWM LED Configuration
RGB PWM LEDs use the sl_led_t struct, and their own structs sl_simple_rgb_pwm_led_context_t and sl_led_rgb_pwm_t . These are automatically generated into the following files, as well as instance specific headers with macro definitions in them. The samples below are for a single instance called "inst0".
- Note
- The sl_simple_rgb_pwm_led_instances.c file is shown with only one instance, but if more were in use they would all appear in this .c file.
- Note
- The sl_simple_rgb_pwm_led_instances.h file is shown with only one instance, but if more were in use they would all appear in this .h file.
RGB PWM LED Usage
The RGB PWM Led driver provides functionality for controlling Red/Green/Blue/White LEDs that are driven by PWM. The LEDs can be turned on and off and toggled, and remember their color and brightness state when being turned back on. The color and brightness can be set using values of 0-65535 for red, green, blue, and white. Retrieving the state gives the on/off value, while retrieving the color gives the rgb values. The following code shows how to control these LEDs. An LED should always be initialized before calling any other functions with it.
Data Structures |
|
| struct | sl_simple_rgb_pwm_led_context_t |
|
A Simple RGB LED context.
|
|
| struct | sl_led_rgb_pwm_t |
|
A Simple RGB LED PWM instance.
|
|
Functions |
|
| sl_status_t | sl_simple_rgb_pwm_led_init (void *rgb) |
|
Initialize an RGB PWM LED driver.
|
|
| void | sl_simple_rgb_pwm_led_turn_on (void *rgb) |
|
Turn on an RBG LED.
|
|
| void | sl_simple_rgb_pwm_led_turn_off (void *rgb) |
|
Turn off an RGB LED.
|
|
| void | sl_simple_rgb_pwm_led_toggle (void *rgb) |
|
Toggle an RGB LED.
|
|
| sl_led_state_t | sl_simple_rgb_pwm_led_get_state (void *rgb) |
|
Get status of an RGB LED.
|
|
| void | sl_simple_rgb_pwm_led_set_color (void *rgb, uint16_t red, uint16_t green, uint16_t blue) |
|
Set color mixing and dimming level of an RGB LED.
|
|
| void | sl_simple_rgb_pwm_led_get_color (void *rgb, uint16_t *red, uint16_t *green, uint16_t *blue) |
|
Get current color mixing and dimming level of an RGB LED.
|
|
| void | sl_led_set_rgb_color (const sl_led_rgb_pwm_t *rgb, uint16_t red, uint16_t green, uint16_t blue) |
|
LED set RGB color.
|
|
| void | sl_led_get_rgb_color (const sl_led_rgb_pwm_t *rgb, uint16_t *red, uint16_t *green, uint16_t *blue) |
|
LED get RGB setting.
|
|
Macros |
|
| #define | SL_SIMPLE_RGB_PWM_LED_POLARITY_ACTIVE_HIGH 0U |
|
LED Active polarity High.
|
|
| #define | SL_SIMPLE_RGB_PWM_LED_POLARITY_ACTIVE_LOW 1U |
|
LED Active polarity Low.
|
|
| #define | SL_SIMPLE_RGB_PWM_LED_COLOR_R 0U |
|
LED Red.
|
|
| #define | SL_SIMPLE_RGB_PWM_LED_COLOR_G 1U |
|
LED Green.
|
|
| #define | SL_SIMPLE_RGB_PWM_LED_COLOR_B 2U |
|
LED Blue.
|
|
| #define | SL_SIMPLE_RGB_PWM_LED_NUM_CC_REQUIRED 3U |
|
Number of Timer Capture Channels required (1 for each RGB color)
|
|
Function Documentation
◆ sl_simple_rgb_pwm_led_init()
| sl_status_t sl_simple_rgb_pwm_led_init | ( | void * |
rgb
|
) |
Initialize an RGB PWM LED driver.
- Parameters
-
[in] led_handlePointer to rgb-pwm-led specific data.
- Returns
-
Status Code:
- SL_STATUS_OK Success
- SL_STATUS_FAIL Init error
◆ sl_simple_rgb_pwm_led_turn_on()
| void sl_simple_rgb_pwm_led_turn_on | ( | void * |
rgb
|
) |
Turn on an RBG LED.
Turns on at previously set color levels If no previous levels set, turns on at max level for all RGB LEDs
- Parameters
-
[in] led_handlePointer to rgb_pwm-led specific data.
◆ sl_simple_rgb_pwm_led_turn_off()
| void sl_simple_rgb_pwm_led_turn_off | ( | void * |
rgb
|
) |
Turn off an RGB LED.
- Parameters
-
[in] led_handlePointer to rgb-pwm-led specific data.
◆ sl_simple_rgb_pwm_led_toggle()
| void sl_simple_rgb_pwm_led_toggle | ( | void * |
rgb
|
) |
Toggle an RGB LED.
The toggle "ON" behavior is as defined for sl_simple_rgb_pwm_led_turn_on()
- Parameters
-
[in] led_handlePointer to rgb-pwm-led specific data.
◆ sl_simple_rgb_pwm_led_get_state()
| sl_led_state_t sl_simple_rgb_pwm_led_get_state | ( | void * |
rgb
|
) |
Get status of an RGB LED.
- Parameters
-
[in] led_handlePointer to rgb-pwm-led specific data.
- Returns
- sl_led_state_t Current state of RGB LED. 0 for Red, Green, Blue and White LEDs are all OFF 1 for Red, Green, Blue or White LED is ON
◆ sl_simple_rgb_pwm_led_set_color()
| void sl_simple_rgb_pwm_led_set_color | ( | void * |
rgb,
|
| uint16_t |
red,
|
||
| uint16_t |
green,
|
||
| uint16_t |
blue
|
||
| ) |
Set color mixing and dimming level of an RGB LED.
- Parameters
-
[in] led_handlePointer to rgb-pwm-led specific data: [in] redRed color level (PWM duty-cycle [0-65535]) [in] greenGreen color level (PWM duty-cycle [0-65535]) [in] blueBlue color level (PWM duty-cycle [0-65535])
◆ sl_simple_rgb_pwm_led_get_color()
| void sl_simple_rgb_pwm_led_get_color | ( | void * |
rgb,
|
| uint16_t * |
red,
|
||
| uint16_t * |
green,
|
||
| uint16_t * |
blue
|
||
| ) |
Get current color mixing and dimming level of an RGB LED.
- Note
- Will return the last stored levels regardless of the current ON/OFF state. Call sl_simple_rgb_pwm_led_get_state() to determine if the RGB LED is actually ON or OFF.
- Parameters
-
[in] led_handlePointer to rgb-pwm-led specific data: [out] redRed color level (PWM duty-cycle [0-65535]) [out] greenGreen color level (PWM duty-cycle [0-65535]) [out] blueBlue color level (PWM duty-cycle [0-65535])
◆ sl_led_set_rgb_color()
| void sl_led_set_rgb_color | ( | const sl_led_rgb_pwm_t * |
rgb,
|
| uint16_t |
red,
|
||
| uint16_t |
green,
|
||
| uint16_t |
blue
|
||
| ) |
LED set RGB color.
- Parameters
-
rgbLED Instance handle redLED red intensity greenLED green intensity blueLED blue intensity
◆ sl_led_get_rgb_color()
| void sl_led_get_rgb_color | ( | const sl_led_rgb_pwm_t * |
rgb,
|
| uint16_t * |
red,
|
||
| uint16_t * |
green,
|
||
| uint16_t * |
blue
|
||
| ) |
LED get RGB setting.
- Parameters
-
rgbLED Instance handle redLED red intensity greenLED green intensity blueLED blue intensity
Macro Definition Documentation
◆ SL_SIMPLE_RGB_PWM_LED_POLARITY_ACTIVE_HIGH
| #define SL_SIMPLE_RGB_PWM_LED_POLARITY_ACTIVE_HIGH 0U |
LED Active polarity High.
◆ SL_SIMPLE_RGB_PWM_LED_POLARITY_ACTIVE_LOW
| #define SL_SIMPLE_RGB_PWM_LED_POLARITY_ACTIVE_LOW 1U |
LED Active polarity Low.
◆ SL_SIMPLE_RGB_PWM_LED_COLOR_R
| #define SL_SIMPLE_RGB_PWM_LED_COLOR_R 0U |
LED Red.
◆ SL_SIMPLE_RGB_PWM_LED_COLOR_G
| #define SL_SIMPLE_RGB_PWM_LED_COLOR_G 1U |
LED Green.
◆ SL_SIMPLE_RGB_PWM_LED_COLOR_B
| #define SL_SIMPLE_RGB_PWM_LED_COLOR_B 2U |
LED Blue.
◆ SL_SIMPLE_RGB_PWM_LED_NUM_CC_REQUIRED
| #define SL_SIMPLE_RGB_PWM_LED_NUM_CC_REQUIRED 3U |
Number of Timer Capture Channels required (1 for each RGB color)