Configuration Over SWO

Configuration Over SWO.

Overview

When working with VCOM and/or PTI with a Silicon Labs kit (WSTK or WPK), it's important that the configuration of the kit's board controller matches that of the target application. The Configuration Over SWO component provides a way to automatically configure the board controller to use the same settings for VCOM and PTI configuration is sent to the board controller over SWO at startup, ensuring that the configuration is synchronized.