Cpc_system_common

Description

CPC System Endpoint Common.

Data Structures

struct sl_cpc_system_cmd_header_t
struct sl_cpc_system_cmd_t
struct sl_cpc_system_property_cmd_t

Macros

#define EP_ID_TO_PROPERTY_ID (ep_id)   (( sl_cpc_property_id_t )((0x00001000 | ((ep_id) & 0x000000FF))))
Helper macros to convert an enpoint id (uint8_t) to a PROP_ENDPOINT_STATE_x enum value.
#define PROPERTY_ID_TO_EP_ID (property_id)   ((uint8_t)(property_id) & 0x000000FF)
Helper macros to convert a PROP_ENDPOINT_STATE_x enum value to an endpoint id (uint8_t)
#define AGGREGATED_STATE_LOW (agg)   (( sl_cpc_endpoint_state_t )(agg & 0x0F))
Helper macros to extract the two aggregated endpoint states encoded in one single byte.
#define AGGREGATED_STATE_HIGH (agg)   (( sl_cpc_endpoint_state_t )(agg >> 4))
#define GET_ENDPOINT_STATE_FROM_STATES (payload, ep_id)
#define CPC_CAPABILITIES_SECURITY_ENDPOINT_MASK (1 << 0)
Capabilities mask.
#define CPC_CAPABILITIES_PACKED_ENDPOINT_MASK (1 << 1)
#define CPC_CAPABILITIES_GPIO_ENDPOINT_MASK (1 << 2)
#define PAYLOAD_LENGTH_MAX 16
System endpoint command type.

Enumerations

enum sl_cpc_property_id_t {
PROP_LAST_STATUS = 0x00,
PROP_PROTOCOL_VERSION = 0x01,
PROP_CAPABILITIES = 0x02,
PROP_SECONDARY_VERSION = 0x03,
PROP_RX_CAPABILITY = 0x20,
PROP_BOOTLOADER_INFO = 0x200,
PROP_BOOTLOADER_REBOOT_MODE = 0x202,
PROP_SECURITY_STATE = 0x301,
PROP_CORE_DEBUG_COUNTERS = 0x400,
PROP_ENDPOINT_STATE_0 = 0x1000,
PROP_ENDPOINT_STATE_1 = 0x1001,
PROP_ENDPOINT_STATE_2 = 0x1002,
PROP_ENDPOINT_STATE_3 = 0x1003,
PROP_ENDPOINT_STATE_4 = 0x1004,
PROP_ENDPOINT_STATE_5 = 0x1005,
PROP_ENDPOINT_STATE_6 = 0x1006,
PROP_ENDPOINT_STATE_7 = 0x1007,
PROP_ENDPOINT_STATE_8 = 0x1008,
PROP_ENDPOINT_STATE_9 = 0x1009,
PROP_ENDPOINT_STATE_10 = 0x100a,
PROP_ENDPOINT_STATE_11 = 0x100b,
PROP_ENDPOINT_STATE_12 = 0x100c,
PROP_ENDPOINT_STATE_13 = 0x100d,
PROP_ENDPOINT_STATE_14 = 0x100e,
PROP_ENDPOINT_STATE_15 = 0x100f,
PROP_ENDPOINT_STATE_16 = 0x1010,
PROP_ENDPOINT_STATE_17 = 0x1011,
PROP_ENDPOINT_STATE_18 = 0x1012,
PROP_ENDPOINT_STATE_19 = 0x1013,
PROP_ENDPOINT_STATE_20 = 0x1014,
PROP_ENDPOINT_STATE_21 = 0x1015,
PROP_ENDPOINT_STATE_22 = 0x1016,
PROP_ENDPOINT_STATE_23 = 0x1017,
PROP_ENDPOINT_STATE_24 = 0x1018,
PROP_ENDPOINT_STATE_25 = 0x1019,
PROP_ENDPOINT_STATE_26 = 0x101a,
PROP_ENDPOINT_STATE_27 = 0x101b,
PROP_ENDPOINT_STATE_28 = 0x101c,
PROP_ENDPOINT_STATE_29 = 0x101d,
PROP_ENDPOINT_STATE_30 = 0x101e,
PROP_ENDPOINT_STATE_31 = 0x101f,
PROP_ENDPOINT_STATE_32 = 0x1020,
PROP_ENDPOINT_STATE_33 = 0x1021,
PROP_ENDPOINT_STATE_34 = 0x1022,
PROP_ENDPOINT_STATE_35 = 0x1023,
PROP_ENDPOINT_STATE_36 = 0x1024,
PROP_ENDPOINT_STATE_37 = 0x1025,
PROP_ENDPOINT_STATE_38 = 0x1026,
PROP_ENDPOINT_STATE_39 = 0x1027,
PROP_ENDPOINT_STATE_40 = 0x1028,
PROP_ENDPOINT_STATE_41 = 0x1029,
PROP_ENDPOINT_STATE_42 = 0x102a,
PROP_ENDPOINT_STATE_43 = 0x102b,
PROP_ENDPOINT_STATE_44 = 0x102c,
PROP_ENDPOINT_STATE_45 = 0x102d,
PROP_ENDPOINT_STATE_46 = 0x102e,
PROP_ENDPOINT_STATE_47 = 0x102f,
PROP_ENDPOINT_STATE_48 = 0x1030,
PROP_ENDPOINT_STATE_49 = 0x1031,
PROP_ENDPOINT_STATE_50 = 0x1032,
PROP_ENDPOINT_STATE_51 = 0x1033,
PROP_ENDPOINT_STATE_52 = 0x1034,
PROP_ENDPOINT_STATE_53 = 0x1035,
PROP_ENDPOINT_STATE_54 = 0x1036,
PROP_ENDPOINT_STATE_55 = 0x1037,
PROP_ENDPOINT_STATE_56 = 0x1038,
PROP_ENDPOINT_STATE_57 = 0x1039,
PROP_ENDPOINT_STATE_58 = 0x103a,
PROP_ENDPOINT_STATE_59 = 0x103b,
PROP_ENDPOINT_STATE_60 = 0x103c,
PROP_ENDPOINT_STATE_61 = 0x103d,
PROP_ENDPOINT_STATE_62 = 0x103e,
PROP_ENDPOINT_STATE_63 = 0x103f,
PROP_ENDPOINT_STATE_64 = 0x1040,
PROP_ENDPOINT_STATE_65 = 0x1041,
PROP_ENDPOINT_STATE_66 = 0x1042,
PROP_ENDPOINT_STATE_67 = 0x1043,
PROP_ENDPOINT_STATE_68 = 0x1044,
PROP_ENDPOINT_STATE_69 = 0x1045,
PROP_ENDPOINT_STATE_70 = 0x1046,
PROP_ENDPOINT_STATE_71 = 0x1047,
PROP_ENDPOINT_STATE_72 = 0x1048,
PROP_ENDPOINT_STATE_73 = 0x1049,
PROP_ENDPOINT_STATE_74 = 0x104a,
PROP_ENDPOINT_STATE_75 = 0x104b,
PROP_ENDPOINT_STATE_76 = 0x104c,
PROP_ENDPOINT_STATE_77 = 0x104d,
PROP_ENDPOINT_STATE_78 = 0x104e,
PROP_ENDPOINT_STATE_79 = 0x104f,
PROP_ENDPOINT_STATE_80 = 0x1050,
PROP_ENDPOINT_STATE_81 = 0x1051,
PROP_ENDPOINT_STATE_82 = 0x1052,
PROP_ENDPOINT_STATE_83 = 0x1053,
PROP_ENDPOINT_STATE_84 = 0x1054,
PROP_ENDPOINT_STATE_85 = 0x1055,
PROP_ENDPOINT_STATE_86 = 0x1056,
PROP_ENDPOINT_STATE_87 = 0x1057,
PROP_ENDPOINT_STATE_88 = 0x1058,
PROP_ENDPOINT_STATE_89 = 0x1059,
PROP_ENDPOINT_STATE_90 = 0x105a,
PROP_ENDPOINT_STATE_91 = 0x105b,
PROP_ENDPOINT_STATE_92 = 0x105c,
PROP_ENDPOINT_STATE_93 = 0x105d,
PROP_ENDPOINT_STATE_94 = 0x105e,
PROP_ENDPOINT_STATE_95 = 0x105f,
PROP_ENDPOINT_STATE_96 = 0x1060,
PROP_ENDPOINT_STATE_97 = 0x1061,
PROP_ENDPOINT_STATE_98 = 0x1062,
PROP_ENDPOINT_STATE_99 = 0x1063,
PROP_ENDPOINT_STATE_100 = 0x1064,
PROP_ENDPOINT_STATE_101 = 0x1065,
PROP_ENDPOINT_STATE_102 = 0x1066,
PROP_ENDPOINT_STATE_103 = 0x1067,
PROP_ENDPOINT_STATE_104 = 0x1068,
PROP_ENDPOINT_STATE_105 = 0x1069,
PROP_ENDPOINT_STATE_106 = 0x106a,
PROP_ENDPOINT_STATE_107 = 0x106b,
PROP_ENDPOINT_STATE_108 = 0x106c,
PROP_ENDPOINT_STATE_109 = 0x106d,
PROP_ENDPOINT_STATE_110 = 0x106e,
PROP_ENDPOINT_STATE_111 = 0x106f,
PROP_ENDPOINT_STATE_112 = 0x1070,
PROP_ENDPOINT_STATE_113 = 0x1071,
PROP_ENDPOINT_STATE_114 = 0x1072,
PROP_ENDPOINT_STATE_115 = 0x1073,
PROP_ENDPOINT_STATE_116 = 0x1074,
PROP_ENDPOINT_STATE_117 = 0x1075,
PROP_ENDPOINT_STATE_118 = 0x1076,
PROP_ENDPOINT_STATE_119 = 0x1077,
PROP_ENDPOINT_STATE_120 = 0x1078,
PROP_ENDPOINT_STATE_121 = 0x1079,
PROP_ENDPOINT_STATE_122 = 0x107a,
PROP_ENDPOINT_STATE_123 = 0x107b,
PROP_ENDPOINT_STATE_124 = 0x107c,
PROP_ENDPOINT_STATE_125 = 0x107d,
PROP_ENDPOINT_STATE_126 = 0x107e,
PROP_ENDPOINT_STATE_127 = 0x107f,
PROP_ENDPOINT_STATE_128 = 0x1080,
PROP_ENDPOINT_STATE_129 = 0x1081,
PROP_ENDPOINT_STATE_130 = 0x1082,
PROP_ENDPOINT_STATE_131 = 0x1083,
PROP_ENDPOINT_STATE_132 = 0x1084,
PROP_ENDPOINT_STATE_133 = 0x1085,
PROP_ENDPOINT_STATE_134 = 0x1086,
PROP_ENDPOINT_STATE_135 = 0x1087,
PROP_ENDPOINT_STATE_136 = 0x1088,
PROP_ENDPOINT_STATE_137 = 0x1089,
PROP_ENDPOINT_STATE_138 = 0x108a,
PROP_ENDPOINT_STATE_139 = 0x108b,
PROP_ENDPOINT_STATE_140 = 0x108c,
PROP_ENDPOINT_STATE_141 = 0x108d,
PROP_ENDPOINT_STATE_142 = 0x108e,
PROP_ENDPOINT_STATE_143 = 0x108f,
PROP_ENDPOINT_STATE_144 = 0x1090,
PROP_ENDPOINT_STATE_145 = 0x1091,
PROP_ENDPOINT_STATE_146 = 0x1092,
PROP_ENDPOINT_STATE_147 = 0x1093,
PROP_ENDPOINT_STATE_148 = 0x1094,
PROP_ENDPOINT_STATE_149 = 0x1095,
PROP_ENDPOINT_STATE_150 = 0x1096,
PROP_ENDPOINT_STATE_151 = 0x1097,
PROP_ENDPOINT_STATE_152 = 0x1098,
PROP_ENDPOINT_STATE_153 = 0x1099,
PROP_ENDPOINT_STATE_154 = 0x109a,
PROP_ENDPOINT_STATE_155 = 0x109b,
PROP_ENDPOINT_STATE_156 = 0x109c,
PROP_ENDPOINT_STATE_157 = 0x109d,
PROP_ENDPOINT_STATE_158 = 0x109e,
PROP_ENDPOINT_STATE_159 = 0x109f,
PROP_ENDPOINT_STATE_160 = 0x10a0,
PROP_ENDPOINT_STATE_161 = 0x10a1,
PROP_ENDPOINT_STATE_162 = 0x10a2,
PROP_ENDPOINT_STATE_163 = 0x10a3,
PROP_ENDPOINT_STATE_164 = 0x10a4,
PROP_ENDPOINT_STATE_165 = 0x10a5,
PROP_ENDPOINT_STATE_166 = 0x10a6,
PROP_ENDPOINT_STATE_167 = 0x10a7,
PROP_ENDPOINT_STATE_168 = 0x10a8,
PROP_ENDPOINT_STATE_169 = 0x10a9,
PROP_ENDPOINT_STATE_170 = 0x10aa,
PROP_ENDPOINT_STATE_171 = 0x10ab,
PROP_ENDPOINT_STATE_172 = 0x10ac,
PROP_ENDPOINT_STATE_173 = 0x10ad,
PROP_ENDPOINT_STATE_174 = 0x10ae,
PROP_ENDPOINT_STATE_175 = 0x10af,
PROP_ENDPOINT_STATE_176 = 0x10b0,
PROP_ENDPOINT_STATE_177 = 0x10b1,
PROP_ENDPOINT_STATE_178 = 0x10b2,
PROP_ENDPOINT_STATE_179 = 0x10b3,
PROP_ENDPOINT_STATE_180 = 0x10b4,
PROP_ENDPOINT_STATE_181 = 0x10b5,
PROP_ENDPOINT_STATE_182 = 0x10b6,
PROP_ENDPOINT_STATE_183 = 0x10b7,
PROP_ENDPOINT_STATE_184 = 0x10b8,
PROP_ENDPOINT_STATE_185 = 0x10b9,
PROP_ENDPOINT_STATE_186 = 0x10ba,
PROP_ENDPOINT_STATE_187 = 0x10bb,
PROP_ENDPOINT_STATE_188 = 0x10bc,
PROP_ENDPOINT_STATE_189 = 0x10bd,
PROP_ENDPOINT_STATE_190 = 0x10be,
PROP_ENDPOINT_STATE_191 = 0x10bf,
PROP_ENDPOINT_STATE_192 = 0x10c0,
PROP_ENDPOINT_STATE_193 = 0x10c1,
PROP_ENDPOINT_STATE_194 = 0x10c2,
PROP_ENDPOINT_STATE_195 = 0x10c3,
PROP_ENDPOINT_STATE_196 = 0x10c4,
PROP_ENDPOINT_STATE_197 = 0x10c5,
PROP_ENDPOINT_STATE_198 = 0x10c6,
PROP_ENDPOINT_STATE_199 = 0x10c7,
PROP_ENDPOINT_STATE_200 = 0x10c8,
PROP_ENDPOINT_STATE_201 = 0x10c9,
PROP_ENDPOINT_STATE_202 = 0x10ca,
PROP_ENDPOINT_STATE_203 = 0x10cb,
PROP_ENDPOINT_STATE_204 = 0x10cc,
PROP_ENDPOINT_STATE_205 = 0x10cd,
PROP_ENDPOINT_STATE_206 = 0x10ce,
PROP_ENDPOINT_STATE_207 = 0x10cf,
PROP_ENDPOINT_STATE_208 = 0x10d0,
PROP_ENDPOINT_STATE_209 = 0x10d1,
PROP_ENDPOINT_STATE_210 = 0x10d2,
PROP_ENDPOINT_STATE_211 = 0x10d3,
PROP_ENDPOINT_STATE_212 = 0x10d4,
PROP_ENDPOINT_STATE_213 = 0x10d5,
PROP_ENDPOINT_STATE_214 = 0x10d6,
PROP_ENDPOINT_STATE_215 = 0x10d7,
PROP_ENDPOINT_STATE_216 = 0x10d8,
PROP_ENDPOINT_STATE_217 = 0x10d9,
PROP_ENDPOINT_STATE_218 = 0x10da,
PROP_ENDPOINT_STATE_219 = 0x10db,
PROP_ENDPOINT_STATE_220 = 0x10dc,
PROP_ENDPOINT_STATE_221 = 0x10dd,
PROP_ENDPOINT_STATE_222 = 0x10de,
PROP_ENDPOINT_STATE_223 = 0x10df,
PROP_ENDPOINT_STATE_224 = 0x10e0,
PROP_ENDPOINT_STATE_225 = 0x10e1,
PROP_ENDPOINT_STATE_226 = 0x10e2,
PROP_ENDPOINT_STATE_227 = 0x10e3,
PROP_ENDPOINT_STATE_228 = 0x10e4,
PROP_ENDPOINT_STATE_229 = 0x10e5,
PROP_ENDPOINT_STATE_230 = 0x10e6,
PROP_ENDPOINT_STATE_231 = 0x10e7,
PROP_ENDPOINT_STATE_232 = 0x10e8,
PROP_ENDPOINT_STATE_233 = 0x10e9,
PROP_ENDPOINT_STATE_234 = 0x10ea,
PROP_ENDPOINT_STATE_235 = 0x10eb,
PROP_ENDPOINT_STATE_236 = 0x10ec,
PROP_ENDPOINT_STATE_237 = 0x10ed,
PROP_ENDPOINT_STATE_238 = 0x10ee,
PROP_ENDPOINT_STATE_239 = 0x10ef,
PROP_ENDPOINT_STATE_240 = 0x10f0,
PROP_ENDPOINT_STATE_241 = 0x10f1,
PROP_ENDPOINT_STATE_242 = 0x10f2,
PROP_ENDPOINT_STATE_243 = 0x10f3,
PROP_ENDPOINT_STATE_244 = 0x10f4,
PROP_ENDPOINT_STATE_245 = 0x10f5,
PROP_ENDPOINT_STATE_246 = 0x10f6,
PROP_ENDPOINT_STATE_247 = 0x10f7,
PROP_ENDPOINT_STATE_248 = 0x10f8,
PROP_ENDPOINT_STATE_249 = 0x10f9,
PROP_ENDPOINT_STATE_250 = 0x10fa,
PROP_ENDPOINT_STATE_251 = 0x10fb,
PROP_ENDPOINT_STATE_252 = 0x10fc,
PROP_ENDPOINT_STATE_253 = 0x10fd,
PROP_ENDPOINT_STATE_254 = 0x10fe,
PROP_ENDPOINT_STATE_255 = 0x10ff,
PROP_ENDPOINT_STATES = 0x1100
}
System endpoint property id enum.
enum sl_cpc_system_status_t {
STATUS_OK = 0,
STATUS_FAILURE = 1,
STATUS_UNIMPLEMENTED = 2,
STATUS_INVALID_ARGUMENT = 3,
STATUS_INVALID_STATE = 4,
STATUS_INVALID_COMMAND = 5,
STATUS_INVALID_INTERFACE = 6,
STATUS_INTERNAL_ERROR = 7,
STATUS_SECURITY_ERROR = 8,
STATUS_PARSE_ERROR = 9,
STATUS_IN_PROGRESS = 10,
STATUS_NOMEM = 11,
STATUS_BUSY = 12,
STATUS_PROP_NOT_FOUND = 13,
STATUS_PACKET_DROPPED = 14,
STATUS_EMPTY = 15,
STATUS_CMD_TOO_BIG = 16,
STATUS_NO_ACK = 17,
STATUS_CCA_FAILURE = 18,
STATUS_ALREADY = 19,
STATUS_ITEM_NOT_FOUND = 20,
STATUS_INVALID_COMMAND_FOR_PROP = 21,
STATUS_RESET_POWER_ON = 112,
STATUS_RESET_EXTERNAL = 113,
STATUS_RESET_SOFTWARE = 114,
STATUS_RESET_FAULT = 115,
STATUS_RESET_CRASH = 116,
STATUS_RESET_ASSERT = 117,
STATUS_RESET_OTHER = 118,
STATUS_RESET_UNKNOWN = 119,
STATUS_RESET_WATCHDOG = 120
}
System status code id.
enum sl_cpc_system_reboot_mode_t {
REBOOT_APPLICATION = 0,
REBOOT_BOOTLOADER = 1
}
Bootloader reboot mode.
enum sl_cpc_system_cmd_id_t {
CMD_SYSTEM_NOOP = 0x00,
CMD_SYSTEM_RESET = 0x01,
CMD_SYSTEM_PROP_VALUE_GET = 0x02,
CMD_SYSTEM_PROP_VALUE_SET = 0x03,
CMD_SYSTEM_PROP_VALUE_IS = 0x06
}
System endpoint command id enum.

Macro Definition Documentation

◆ EP_ID_TO_PROPERTY_ID

#define EP_ID_TO_PROPERTY_ID ( ep_id ) (( sl_cpc_property_id_t )((0x00001000 | ((ep_id) & 0x000000FF))))

Helper macros to convert an enpoint id (uint8_t) to a PROP_ENDPOINT_STATE_x enum value.

◆ PROPERTY_ID_TO_EP_ID

#define PROPERTY_ID_TO_EP_ID ( property_id ) ((uint8_t)(property_id) & 0x000000FF)

Helper macros to convert a PROP_ENDPOINT_STATE_x enum value to an endpoint id (uint8_t)

◆ AGGREGATED_STATE_LOW

#define AGGREGATED_STATE_LOW ( agg ) (( sl_cpc_endpoint_state_t )(agg & 0x0F))

Helper macros to extract the two aggregated endpoint states encoded in one single byte.

◆ GET_ENDPOINT_STATE_FROM_STATES

#define GET_ENDPOINT_STATE_FROM_STATES ( payload,
ep_id
)
Value:
((ep_id % 2 == 0) ? AGGREGATED_STATE_LOW (((uint8_t*)payload)[ep_id / 2]) \
: AGGREGATED_STATE_HIGH(((uint8_t*)payload)[ep_id / 2]))

◆ CPC_CAPABILITIES_SECURITY_ENDPOINT_MASK

#define CPC_CAPABILITIES_SECURITY_ENDPOINT_MASK   (1 << 0)

Capabilities mask.

Note
Used with the value returned by a property-get on PROP_CAPABILITIES

◆ PAYLOAD_LENGTH_MAX

#define PAYLOAD_LENGTH_MAX   16

System endpoint command type.

Enumeration Type Documentation

◆ sl_cpc_property_id_t

System endpoint property id enum.

This enum contains each of the supported property used by the CMD_SYSTEM_PROP_* system commands.

Note
This enum is encoded with 4 bytes.
Enumerator
PROP_ENDPOINT_STATES

Aggregates all endpoint state information into a single field.

◆ sl_cpc_system_status_t

System status code id.

This enum contains each of the spinel protocol status code

Note
This enum is encoded with 4 bytes.
Enumerator
STATUS_OK

Operation has completed successfully.

STATUS_FAILURE

Operation has failed for some undefined reason.

STATUS_UNIMPLEMENTED

The given operation has not been implemented.

STATUS_INVALID_ARGUMENT

An argument to the given operation is invalid.

STATUS_INVALID_STATE

The given operation is invalid for the current state of the device.

STATUS_INVALID_COMMAND

The given command is not recognized.

STATUS_INVALID_INTERFACE

The given Spinel interface is not supported.

STATUS_INTERNAL_ERROR

An internal runtime error has occurred.

STATUS_SECURITY_ERROR

A security or authentication error has occurred.

STATUS_PARSE_ERROR

An error has occurred while parsing the command.

STATUS_IN_PROGRESS

The operation is in progress and will be completed asynchronously.

STATUS_NOMEM

The operation has been prevented due to memory pressure.

STATUS_BUSY

The device is currently performing a mutually exclusive operation.

STATUS_PROP_NOT_FOUND

The given property is not recognized.

STATUS_PACKET_DROPPED

The packet was dropped.

STATUS_EMPTY

The result of the operation is empty.

STATUS_CMD_TOO_BIG

The command was too large to fit in the internal buffer.

STATUS_NO_ACK

The packet was not acknowledged.

STATUS_CCA_FAILURE

The packet was not sent due to a CCA failure.

STATUS_ALREADY

The operation is already in progress or the property was already set to the given value.

STATUS_ITEM_NOT_FOUND

The given item could not be found in the property.

STATUS_INVALID_COMMAND_FOR_PROP

The given command cannot be performed on this property.

◆ sl_cpc_system_reboot_mode_t

Bootloader reboot mode.

Note
This enum is encoded with 4 bytes.
Enumerator
REBOOT_APPLICATION

At the next reboot application is executed.

REBOOT_BOOTLOADER

At the next reboot bootloader is executed.

◆ sl_cpc_system_cmd_id_t

System endpoint command id enum.