Library initialization
Description
Functions | |
psa_status_t | psa_crypto_init (void) |
Library initialization. | |
Function Documentation
◆ psa_crypto_init()
psa_status_t psa_crypto_init | ( | void |
| ) |
Library initialization.
Applications must call this function before calling any other function in this module.
Applications may call this function more than once. Once a call succeeds, subsequent calls are guaranteed to succeed.
If the application calls other functions before calling psa_crypto_init(), the behavior is undefined. Implementations are encouraged to either perform the operation as if the library had been initialized or to return PSA_ERROR_BAD_STATE or some other applicable error. In particular, implementations should not return a success status if the lack of initialization may have security implications, for example due to improper seeding of the random number generator.
- Return values
-
PSA_SUCCESS
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_INSUFFICIENT_STORAGE
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_INSUFFICIENT_ENTROPY
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_DATA_INVALID
PSA_ERROR_DATA_CORRUPT