sl_se_cert_size_type_t Struct Reference
Certificate size data structure.
#include <sl_se_manager_types.h>
Data Fields | |
uint32_t | batch_id_size |
size in bytes of the Batch certificate | |
uint32_t | se_id_size |
size in bytes of the SE ID certificate | |
uint32_t | host_id_size |
size in bytes of the Host ID certificate | |
Certificate size data structure.
Field Documentation
◆ batch_id_size
uint32_t sl_se_cert_size_type_t::batch_id_size |
size in bytes of the Batch certificate
◆ se_id_size
uint32_t sl_se_cert_size_type_t::se_id_size |
size in bytes of the SE ID certificate
◆ host_id_size
uint32_t sl_se_cert_size_type_t::host_id_size |
size in bytes of the Host ID certificate