ADC_InitSingle_TypeDef Struct Reference
Single conversion initialization structure.
      
       #include <em_adc.h>
      
     
| Data Fields | |
| ADC_PRSSEL_TypeDef | prsSel | 
| Peripheral reflex system trigger selection. | |
| ADC_AcqTime_TypeDef | acqTime | 
| Acquisition time (in ADC clock cycles). | |
| ADC_Ref_TypeDef | reference | 
| Sample reference selection. | |
| ADC_Res_TypeDef | resolution | 
| Sample resolution. | |
| ADC_SingleInput_TypeDef | input | 
| Sample input selection, use single-ended or differential input according to setting of 
          diff
         . | |
| bool | diff | 
| Select if single-ended or differential input. | |
| bool | prsEnable | 
| Peripheral reflex system trigger enable. | |
| bool | leftAdjust | 
| Select if left adjustment should be done. | |
| bool | rep | 
| Select if continuous conversion until explicit stop. | |
Single conversion initialization structure.
Field Documentation
◆ prsSel
| ADC_PRSSEL_TypeDef ADC_InitSingle_TypeDef::prsSel | 
Peripheral reflex system trigger selection.
        Only applicable if
        
         prsEnable
        
        is enabled.
       
◆ acqTime
| ADC_AcqTime_TypeDef ADC_InitSingle_TypeDef::acqTime | 
Acquisition time (in ADC clock cycles).
◆ reference
| ADC_Ref_TypeDef ADC_InitSingle_TypeDef::reference | 
Sample reference selection.
Note that, for external references, the ADC calibration register must be set explicitly.
◆ resolution
| ADC_Res_TypeDef ADC_InitSingle_TypeDef::resolution | 
Sample resolution.
◆ input
| ADC_SingleInput_TypeDef ADC_InitSingle_TypeDef::input | 
        Sample input selection, use single-ended or differential input according to setting of
        
         diff
        
        .
       
◆ diff
| bool ADC_InitSingle_TypeDef::diff | 
Select if single-ended or differential input.
◆ prsEnable
| bool ADC_InitSingle_TypeDef::prsEnable | 
Peripheral reflex system trigger enable.
◆ leftAdjust
| bool ADC_InitSingle_TypeDef::leftAdjust | 
Select if left adjustment should be done.
◆ rep
| bool ADC_InitSingle_TypeDef::rep | 
Select if continuous conversion until explicit stop.