WDOG_Init_TypeDef Struct Reference

Watchdog initialization structure.

#include <em_wdog.h>

Data Fields

bool enable
Enable Watchdog when initialization completed.
bool debugRun
Counter keeps running during debug halt.
bool em2Run
Counter keeps running when in EM2.
bool em3Run
Counter keeps running when in EM3.
bool em4Block
Block EMU from entering EM4.
bool swoscBlock
Block SW from disabling LFRCO/LFXO oscillators.
bool lock
Block SW from modifying the configuration (a reset is needed to reconfigure).
WDOG_ClkSel_TypeDef clkSel
Clock source to use for Watchdog.
WDOG_PeriodSel_TypeDef perSel
Watchdog timeout period.

Watchdog initialization structure.

Field Documentation

◆ enable

bool WDOG_Init_TypeDef::enable

Enable Watchdog when initialization completed.

◆ debugRun

bool WDOG_Init_TypeDef::debugRun

Counter keeps running during debug halt.

◆ em2Run

bool WDOG_Init_TypeDef::em2Run

Counter keeps running when in EM2.

◆ em3Run

bool WDOG_Init_TypeDef::em3Run

Counter keeps running when in EM3.

◆ em4Block

bool WDOG_Init_TypeDef::em4Block

Block EMU from entering EM4.

◆ swoscBlock

bool WDOG_Init_TypeDef::swoscBlock

Block SW from disabling LFRCO/LFXO oscillators.

◆ lock

bool WDOG_Init_TypeDef::lock

Block SW from modifying the configuration (a reset is needed to reconfigure).

◆ clkSel

WDOG_ClkSel_TypeDef WDOG_Init_TypeDef::clkSel

Clock source to use for Watchdog.

◆ perSel

WDOG_PeriodSel_TypeDef WDOG_Init_TypeDef::perSel

Watchdog timeout period.