TIMER_Init_TypeDef Struct Reference

TIMER initialization structure.

#include <em_timer.h>

Data Fields

bool enable
 Start counting when initialization completed.
 
bool debugRun
 Counter shall keep running during debug halt.
 
TIMER_Prescale_TypeDef prescale
 Prescaling factor, if HFPER / HFPERB clock used.
 
TIMER_ClkSel_TypeDef clkSel
 Clock selection.
 
bool count2x
 2x Count mode, counter increments/decrements by 2, meant for PWM mode.
 
bool ati
 ATI (Always Track Inputs) makes CCPOL always track the polarity of the inputs.
 
TIMER_InputAction_TypeDef fallAction
 Action on falling input edge.
 
TIMER_InputAction_TypeDef riseAction
 Action on rising input edge.
 
TIMER_Mode_TypeDef mode
 Counting mode.
 
bool dmaClrAct
 DMA request clear on active.
 
bool quadModeX4
 Select X2 or X4 quadrature decode mode (if used).
 
bool oneShot
 Determines if only counting up or down once.
 
bool sync
 Timer can be start/stop/reload by other timers.
 

TIMER initialization structure.

Field Documentation

◆ enable

bool TIMER_Init_TypeDef::enable

Start counting when initialization completed.

◆ debugRun

bool TIMER_Init_TypeDef::debugRun

Counter shall keep running during debug halt.

◆ prescale

TIMER_Prescale_TypeDef TIMER_Init_TypeDef::prescale

Prescaling factor, if HFPER / HFPERB clock used.

◆ clkSel

TIMER_ClkSel_TypeDef TIMER_Init_TypeDef::clkSel

Clock selection.

◆ count2x

bool TIMER_Init_TypeDef::count2x

2x Count mode, counter increments/decrements by 2, meant for PWM mode.

◆ ati

bool TIMER_Init_TypeDef::ati

ATI (Always Track Inputs) makes CCPOL always track the polarity of the inputs.

◆ fallAction

TIMER_InputAction_TypeDef TIMER_Init_TypeDef::fallAction

Action on falling input edge.

◆ riseAction

TIMER_InputAction_TypeDef TIMER_Init_TypeDef::riseAction

Action on rising input edge.

◆ mode

TIMER_Mode_TypeDef TIMER_Init_TypeDef::mode

Counting mode.

◆ dmaClrAct

bool TIMER_Init_TypeDef::dmaClrAct

DMA request clear on active.

◆ quadModeX4

bool TIMER_Init_TypeDef::quadModeX4

Select X2 or X4 quadrature decode mode (if used).

◆ oneShot

bool TIMER_Init_TypeDef::oneShot

Determines if only counting up or down once.

◆ sync

bool TIMER_Init_TypeDef::sync

Timer can be start/stop/reload by other timers.