DCDC Initialization
Description
Initialize the DC-DC converter.
Configures the DC-DC converter. If the DC-DC converter is not to be used, the configuration option SL_DEVICE_INIT_DCDC_ENABLE
can be disabled, and the converter will be powered off. On Series 1 devices, this option should only be used when DVDD is externally powered.
To enable the bypass switch and short the DC-DC converter input to the DC-DC output, set the configuration option SL_DEVICE_INIT_DCDC_BYPASS
.
See AN0948 Power Configurations and DC-DC for further details about DC-DC converter configuration and operation.
Functions | |
sl_status_t | sl_device_init_dcdc (void) |
Initialize DCDC. | |
Macros | |
#define | SL_DEVICE_INIT_DCDC_TYPE_BUCK 0 |
DC/DC Converter Type. | |
#define | SL_DEVICE_INIT_DCDC_TYPE_BOOST 1 |
Boost Type. | |
Function Documentation
◆ sl_device_init_dcdc()
sl_status_t sl_device_init_dcdc | ( | void |
| ) |
Initialize DCDC.
Configure and start the DCDC
- Returns
- Status code
- Return values
-
SL_STATUS_OK
DC-DC converter initialized successfully
Macro Definition Documentation
◆ SL_DEVICE_INIT_DCDC_TYPE_BUCK
#define SL_DEVICE_INIT_DCDC_TYPE_BUCK 0 |
DC/DC Converter Type.
Buck Type
◆ SL_DEVICE_INIT_DCDC_TYPE_BOOST
#define SL_DEVICE_INIT_DCDC_TYPE_BOOST 1 |
Boost Type.