You are viewing documentation for version: 4.2 | Version History
◆ len
uint64_t sl_se_gcm_multipart_context_t::len |
Total length of the encrypted data.
◆ add_len
uint64_t sl_se_gcm_multipart_context_t::add_len |
Total length of the additional data.
◆ tagbuf
uint8_t sl_se_gcm_multipart_context_t::tagbuf[16] |
◆ previous_se_ctx
uint8_t sl_se_gcm_multipart_context_t::previous_se_ctx[32] |
SE state from previous operation.
◆ se_ctx
uint8_t sl_se_gcm_multipart_context_t::se_ctx[32] |
◆ final_data
uint8_t sl_se_gcm_multipart_context_t::final_data[16] |
Input data saved for finish operation.
◆ final_data_length
uint8_t sl_se_gcm_multipart_context_t::final_data_length |
◆ mode
◆ first_operation
bool sl_se_gcm_multipart_context_t::first_operation |