ACMP_CapsenseInit_TypeDef Struct Reference
Capsense initialization structure.
      
       #include <em_acmp.h>
      
     
| Data Fields | |
| bool | fullBias | 
| Full-bias current. | |
| uint32_t | biasProg | 
| Bias current. | |
| ACMP_HysteresisLevel_TypeDef | hysteresisLevel_0 | 
| Hysteresis level when ACMP output is 0. | |
| ACMP_HysteresisLevel_TypeDef | hysteresisLevel_1 | 
| Hysteresis level when ACMP output is 1. | |
| ACMP_CapsenseResistor_TypeDef | resistor | 
| A resistor used in the capacitive sensing circuit. | |
| uint32_t | vddLevelHigh | 
| This value configures the upper voltage threshold of the capsense oscillation rail. | |
| uint32_t | vddLevelLow | 
| This value configures the lower voltage threshold of the capsense oscillation rail. | |
| bool | enable | 
| If true, ACMP is enabled after configuration. | |
Capsense initialization structure.
Field Documentation
◆ fullBias
| bool ACMP_CapsenseInit_TypeDef::fullBias | 
Full-bias current.
See the ACMP chapter about bias and response time in the reference manual for details.
◆ biasProg
| uint32_t ACMP_CapsenseInit_TypeDef::biasProg | 
Bias current.
See the ACMP chapter about bias and response time in the reference manual for details.
◆ hysteresisLevel_0
| ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel_0 | 
Hysteresis level when ACMP output is 0.
◆ hysteresisLevel_1
| ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel_1 | 
Hysteresis level when ACMP output is 1.
◆ resistor
| ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor | 
A resistor used in the capacitive sensing circuit.
For values see the device data sheet.
◆ vddLevelHigh
| uint32_t ACMP_CapsenseInit_TypeDef::vddLevelHigh | 
This value configures the upper voltage threshold of the capsense oscillation rail.
The voltage threshold is calculated as follows: VDD * (vddLevelHigh + 1) / 64
◆ vddLevelLow
| uint32_t ACMP_CapsenseInit_TypeDef::vddLevelLow | 
This value configures the lower voltage threshold of the capsense oscillation rail.
The voltage threshold is calculated as follows: VDD * (vddLevelLow + 1) / 64
◆ enable
| bool ACMP_CapsenseInit_TypeDef::enable | 
If true, ACMP is enabled after configuration.