LESENSE_DecCtrlDesc_TypeDef Struct Reference

LESENSE decoder control descriptor structure.

#include <em_lesense.h>

Data Fields

bool chkState
Set to enable decoder to check the present state in addition to the states defined in TCONF.
bool intMap
When set, a transition from state x in decoder will set the interrupt flag CHx.
bool hystPRS0
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 0.
bool hystPRS1
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 1.
bool hystPRS2
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 2.
bool hystIRQ
Set to enable hysteresis in decoder for suppressing the interrupt requests.
bool prsCount
Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.

LESENSE decoder control descriptor structure.

Field Documentation

chkState

bool LESENSE_DecCtrlDesc_TypeDef::chkState

Set to enable decoder to check the present state in addition to the states defined in TCONF.

intMap

bool LESENSE_DecCtrlDesc_TypeDef::intMap

When set, a transition from state x in decoder will set the interrupt flag CHx.

hystPRS0

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS0

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 0.

hystPRS1

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS1

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 1.

hystPRS2

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS2

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 2.

hystIRQ

bool LESENSE_DecCtrlDesc_TypeDef::hystIRQ

Set to enable hysteresis in decoder for suppressing the interrupt requests.

prsCount

bool LESENSE_DecCtrlDesc_TypeDef::prsCount

Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.