LDMA_DescriptorExtend_t Struct Reference
DMA extended descriptor.
#include <em_ldma.h>
Data Fields |
|
| uint32_t | structType : 2 |
|
Set to 0 to select XFER descriptor type.
|
|
| uint32_t | extend : 1 |
|
Extend data structure.
|
|
| uint32_t | structReq : 1 |
|
DMA transfer trigger during LINKLOAD.
|
|
| uint32_t | xferCnt : 11 |
|
Transfer count minus one.
|
|
| uint32_t | byteSwap : 1 |
|
Enable byte swapping transfers.
|
|
| uint32_t | blockSize : 4 |
|
Number of unit transfers per arbitration cycle.
|
|
| uint32_t | doneIfs : 1 |
|
Generate interrupt when done.
|
|
| uint32_t | reqMode : 1 |
|
Block or cycle transfer selector.
|
|
| uint32_t | decLoopCnt : 1 |
|
Enable looped transfers.
|
|
| uint32_t | ignoreSrec : 1 |
|
Ignore single requests.
|
|
| uint32_t | srcInc : 2 |
|
Source address increment unit size.
|
|
| uint32_t | size : 2 |
|
DMA transfer unit size.
|
|
| uint32_t | dstInc : 2 |
|
Destination address increment unit size.
|
|
| uint32_t | srcAddrMode : 1 |
|
Source addressing mode.
|
|
| uint32_t | dstAddrMode : 1 |
|
Destination addressing mode.
|
|
| uint32_t | srcAddr |
|
DMA source address.
|
|
| uint32_t | dstAddr |
|
DMA destination address.
|
|
| uint32_t | linkMode : 1 |
|
Select absolute or relative link address.
|
|
| uint32_t | link : 1 |
|
Enable LINKLOAD when transfer is done.
|
|
| int32_t | linkAddr : 30 |
|
Address of next (linked) descriptor.
|
|
| uint32_t | reserved1 : 4 |
|
Reserved
|
|
| uint32_t | dstIlEn : 1 |
|
Destination interleave.
|
|
| uint32_t | IlMode : 2 |
|
Interleave mode.
|
|
| uint32_t | bufferable : 1 |
|
Reserved
|
|
| uint32_t | reserved2 : 24 |
|
Allow AHB buffering.
|
|
| uint32_t | reserved3 |
|
Reserved
|
|
| uint32_t | IlSrc |
|
DMA rules table base address in memory.
|
|
DMA extended descriptor.
The extended descriptor adds additional fields for the extended features available on the MMLDMA peripheral: destination interleaving and bufferable. The same three different DMA descriptors supported by the LDMA DMA controller are available. Each consists of seven WORDs (instead of four in non-extended descriptors) which map directly onto HW control registers for a given DMA channel. The three descriptor types are XFER, SYNC and WRI. But the extended fields are true only for XFER. The extended fields are the following:
+- +- CTRL
| Original | SRC
| Structure | DST
Extended | +- LINK Structure | XCTRL | Reserved for future usage +- ILSRC
Refer to the reference manual for further information.
Field Documentation
◆ structType
| uint32_t LDMA_DescriptorExtend_t::structType |
Set to 0 to select XFER descriptor type.
◆ extend
| uint32_t LDMA_DescriptorExtend_t::extend |
Extend data structure.
◆ structReq
| uint32_t LDMA_DescriptorExtend_t::structReq |
DMA transfer trigger during LINKLOAD.
◆ xferCnt
| uint32_t LDMA_DescriptorExtend_t::xferCnt |
Transfer count minus one.
◆ byteSwap
| uint32_t LDMA_DescriptorExtend_t::byteSwap |
Enable byte swapping transfers.
◆ blockSize
| uint32_t LDMA_DescriptorExtend_t::blockSize |
Number of unit transfers per arbitration cycle.
◆ doneIfs
| uint32_t LDMA_DescriptorExtend_t::doneIfs |
Generate interrupt when done.
◆ reqMode
| uint32_t LDMA_DescriptorExtend_t::reqMode |
Block or cycle transfer selector.
◆ decLoopCnt
| uint32_t LDMA_DescriptorExtend_t::decLoopCnt |
Enable looped transfers.
◆ ignoreSrec
| uint32_t LDMA_DescriptorExtend_t::ignoreSrec |
Ignore single requests.
◆ srcInc
| uint32_t LDMA_DescriptorExtend_t::srcInc |
Source address increment unit size.
◆ size
| uint32_t LDMA_DescriptorExtend_t::size |
DMA transfer unit size.
◆ dstInc
| uint32_t LDMA_DescriptorExtend_t::dstInc |
Destination address increment unit size.
◆ srcAddrMode
| uint32_t LDMA_DescriptorExtend_t::srcAddrMode |
Source addressing mode.
◆ dstAddrMode
| uint32_t LDMA_DescriptorExtend_t::dstAddrMode |
Destination addressing mode.
◆ srcAddr
| uint32_t LDMA_DescriptorExtend_t::srcAddr |
DMA source address.
◆ dstAddr
| uint32_t LDMA_DescriptorExtend_t::dstAddr |
DMA destination address.
◆ linkMode
| uint32_t LDMA_DescriptorExtend_t::linkMode |
Select absolute or relative link address.
◆ link
| uint32_t LDMA_DescriptorExtend_t::link |
Enable LINKLOAD when transfer is done.
◆ linkAddr
| int32_t LDMA_DescriptorExtend_t::linkAddr |
Address of next (linked) descriptor.
◆ reserved1
| uint32_t LDMA_DescriptorExtend_t::reserved1 |
Reserved
◆ dstIlEn
| uint32_t LDMA_DescriptorExtend_t::dstIlEn |
Destination interleave.
◆ IlMode
| uint32_t LDMA_DescriptorExtend_t::IlMode |
Interleave mode.
◆ bufferable
| uint32_t LDMA_DescriptorExtend_t::bufferable |
Reserved
◆ reserved2
| uint32_t LDMA_DescriptorExtend_t::reserved2 |
Allow AHB buffering.
◆ reserved3
| uint32_t LDMA_DescriptorExtend_t::reserved3 |
Reserved
◆ IlSrc
| uint32_t LDMA_DescriptorExtend_t::IlSrc |
DMA rules table base address in memory.