Built-in keys#
Built-in key mechanism provides access to the keys stored in hardware.
It can be accessed using key ID that is in the range [MBEDTLS_PSA_KEY_ID_BUILTIN_MIN, MBEDLTS_PSA_KEY_ID_BUILTIN_MAX].
Note
Available builtin key IDs vary for different family of devices. For devices vith VSE see Builtin keys on devices with a VSE , and for devices with Secure Engine see Builtin keys on devices with Secure Engine .
Typedefs#
A slot number identifying a key in a driver.
Macros#
The minimum value for a key identifier that is built into the implementation.
The maximum value for a key identifier that is built into the implementation.
The minimum value for a key identifier that is built into the implementation.
The maximum value for a key identifier that is built into the implementation.
Typedef Documentation#
psa_drv_slot_number_t#
typedef uint64_t psa_drv_slot_number_t
A slot number identifying a key in a driver.
Values of this type are used to identify built-in keys.