Asymmetric cryptography#

Functions#

psa_sign_message(mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, uint8_t *signature, size_t signature_size, size_t *signature_length)

Sign a message with a private key.

psa_verify_message(mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *signature, size_t signature_length)

Verify the signature of a message with a public key, using a hash-and-sign verification algorithm.

psa_sign_hash(mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *hash, size_t hash_length, uint8_t *signature, size_t signature_size, size_t *signature_length)

Sign a hash or short message with a private key.

psa_verify_hash(mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *hash, size_t hash_length, const uint8_t *signature, size_t signature_length)

Verify the signature of a hash or short message using a public key.

psa_asymmetric_encrypt(mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *salt, size_t salt_length, uint8_t *output, size_t output_size, size_t *output_length)

Encrypt a short message with a public key.

psa_asymmetric_decrypt(mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *salt, size_t salt_length, uint8_t *output, size_t output_size, size_t *output_length)

Decrypt a short message with a private key.

Function Documentation#

psa_sign_message#

psa_status_t psa_sign_message (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t * input, size_t input_length, uint8_t * signature, size_t signature_size, size_t * signature_length)

Sign a message with a private key.

Parameters
TypeDirectionArgument NameDescription
mbedtls_svc_key_id_t[in]key

Identifier of the key to use for the operation. It must be an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_SIGN_MESSAGE.

psa_algorithm_t[in]alg

An asymmetric signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN_MESSAGE(alg) is true), that is compatible with the type of key.

const uint8_t *[in]input

The input message to sign.

size_t[in]input_length

Size of the input buffer in bytes.

uint8_t *[out]signature

Buffer where the signature is to be written.

size_t[in]signature_size

Size of the signature buffer in bytes. This must be appropriate for the selected algorithm and key:

  • The required signature size is #PSA_SIGN_OUTPUT_SIZE(key_type, key_bits, alg) where key_type and key_bits are the type and bit-size respectively of key.

  • #PSA_SIGNATURE_MAX_SIZE evaluates to the maximum signature size of any supported signature algorithm.

size_t *[out]signature_length

On success, the number of bytes that make up the returned signature value.

For hash-and-sign algorithms, this includes the hashing step.

Note

  • To perform a multi-part hash-and-sign signature algorithm, first use a multi-part hash operation and then pass the resulting hash to psa_sign_hash(). PSA_ALG_GET_HASH(alg) can be used to determine the hash algorithm to use.


psa_verify_message#

psa_status_t psa_verify_message (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t * input, size_t input_length, const uint8_t * signature, size_t signature_length)

Verify the signature of a message with a public key, using a hash-and-sign verification algorithm.

Parameters
TypeDirectionArgument NameDescription
mbedtls_svc_key_id_t[in]key

Identifier of the key to use for the operation. It must be a public key or an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_VERIFY_MESSAGE.

psa_algorithm_t[in]alg

An asymmetric signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN_MESSAGE(alg) is true), that is compatible with the type of key.

const uint8_t *[in]input

The message whose signature is to be verified.

size_t[in]input_length

Size of the input buffer in bytes.

const uint8_t *[out]signature

Buffer containing the signature to verify.

size_t[in]signature_length

Size of the signature buffer in bytes.

Note

  • To perform a multi-part hash-and-sign signature verification algorithm, first use a multi-part hash operation to hash the message and then pass the resulting hash to psa_verify_hash(). PSA_ALG_GET_HASH(alg) can be used to determine the hash algorithm to use.


psa_sign_hash#

psa_status_t psa_sign_hash (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t * hash, size_t hash_length, uint8_t * signature, size_t signature_size, size_t * signature_length)

Sign a hash or short message with a private key.

Parameters
TypeDirectionArgument NameDescription
mbedtls_svc_key_id_tN/Akey

Identifier of the key to use for the operation. It must be an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_SIGN_HASH.

psa_algorithm_tN/Aalg

A signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN_HASH(alg) is true), that is compatible with the type of key.

const uint8_t *[in]hash

The hash or message to sign.

size_tN/Ahash_length

Size of the hash buffer in bytes.

uint8_t *[out]signature

Buffer where the signature is to be written.

size_tN/Asignature_size

Size of the signature buffer in bytes.

size_t *[out]signature_length

On success, the number of bytes that make up the returned signature value.

Note that to perform a hash-and-sign signature algorithm, you must first calculate the hash by calling psa_hash_setup(), psa_hash_update() and psa_hash_finish(), or alternatively by calling psa_hash_compute(). Then pass the resulting hash as the hash parameter to this function. You can use PSA_ALG_SIGN_GET_HASH(alg) to determine the hash algorithm to use.


psa_verify_hash#

psa_status_t psa_verify_hash (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t * hash, size_t hash_length, const uint8_t * signature, size_t signature_length)

Verify the signature of a hash or short message using a public key.

Parameters
TypeDirectionArgument NameDescription
mbedtls_svc_key_id_tN/Akey

Identifier of the key to use for the operation. It must be a public key or an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_VERIFY_HASH.

psa_algorithm_tN/Aalg

A signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN_HASH(alg) is true), that is compatible with the type of key.

const uint8_t *[in]hash

The hash or message whose signature is to be verified.

size_tN/Ahash_length

Size of the hash buffer in bytes.

const uint8_t *[in]signature

Buffer containing the signature to verify.

size_tN/Asignature_length

Size of the signature buffer in bytes.

Note that to perform a hash-and-sign signature algorithm, you must first calculate the hash by calling psa_hash_setup(), psa_hash_update() and psa_hash_finish(), or alternatively by calling psa_hash_compute(). Then pass the resulting hash as the hash parameter to this function. You can use PSA_ALG_SIGN_GET_HASH(alg) to determine the hash algorithm to use.


psa_asymmetric_encrypt#

psa_status_t psa_asymmetric_encrypt (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t * input, size_t input_length, const uint8_t * salt, size_t salt_length, uint8_t * output, size_t output_size, size_t * output_length)

Encrypt a short message with a public key.

Parameters
TypeDirectionArgument NameDescription
mbedtls_svc_key_id_tN/Akey

Size of the salt buffer in bytes. If salt is NULL, pass 0.

psa_algorithm_t[out]alg

Buffer where the encrypted message is to be written.

const uint8_t *N/Ainput

Size of the output buffer in bytes.

size_t[out]input_length

On success, the number of bytes that make up the returned output.

const uint8_t *[in]salt

A salt or label, if supported by the encryption algorithm. If the algorithm does not support a salt, pass NULL. If the algorithm supports an optional salt and you do not want to pass a salt, pass NULL.

size_tN/Asalt_length
uint8_t *N/Aoutput
size_tN/Aoutput_size
size_t *N/Aoutput_length

psa_asymmetric_decrypt#

psa_status_t psa_asymmetric_decrypt (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t * input, size_t input_length, const uint8_t * salt, size_t salt_length, uint8_t * output, size_t output_size, size_t * output_length)

Decrypt a short message with a private key.

Parameters
TypeDirectionArgument NameDescription
mbedtls_svc_key_id_tN/Akey

Size of the salt buffer in bytes. If salt is NULL, pass 0.

psa_algorithm_t[out]alg

Buffer where the decrypted message is to be written.

const uint8_t *N/Ainput

Size of the output buffer in bytes.

size_t[out]input_length

On success, the number of bytes that make up the returned output.

const uint8_t *[in]salt

A salt or label, if supported by the encryption algorithm. If the algorithm does not support a salt, pass NULL. If the algorithm supports an optional salt and you do not want to pass a salt, pass NULL.

size_tN/Asalt_length
uint8_t *N/Aoutput
size_tN/Aoutput_size
size_t *N/Aoutput_length