SSL/TLS communication module#
The SSL/TLS communication module provides the means to create an SSL/TLS communication channel.
The basic provisions are:
initialise an SSL/TLS context (see
mbedtls_ssl_init()).perform an SSL/TLS handshake (see
mbedtls_ssl_handshake()).read/write (see
mbedtls_ssl_read()andmbedtls_ssl_write()).notify a peer that connection is being closed (see
mbedtls_ssl_close_notify()).
Many aspects of such a channel are set through parameters and callback functions:
the endpoint role: client or server.
the authentication mode. Should verification take place.
the Host-to-host communication channel. A TCP/IP module is provided.
the random number generator (RNG).
the ciphers to use for encryption/decryption.
session control functions.
X.509 parameters for certificate-handling and key exchange.
This module can be used to create an SSL/TLS server and client and to provide a basic framework to setup and communicate through an SSL/TLS communication channel. Note that you need to provide for several aspects yourself as mentioned above.