Message digests#

Functions#

psa_hash_compute(psa_algorithm_t alg, const uint8_t *input, size_t input_length, uint8_t *hash, size_t hash_size, size_t *hash_length)

Calculate the hash (digest) of a message.

psa_hash_compare(psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *hash, size_t hash_length)

Calculate the hash (digest) of a message and compare it with a reference value.

psa_hash_operation_t

Return an initial value for a hash operation object.

psa_hash_setup(psa_hash_operation_t *operation, psa_algorithm_t alg)

Set up a multipart hash operation.

psa_hash_update(psa_hash_operation_t *operation, const uint8_t *input, size_t input_length)

Add a message fragment to a multipart hash operation.

psa_hash_finish(psa_hash_operation_t *operation, uint8_t *hash, size_t hash_size, size_t *hash_length)

Finish the calculation of the hash of a message.

psa_hash_verify(psa_hash_operation_t *operation, const uint8_t *hash, size_t hash_length)

Finish the calculation of the hash of a message and compare it with an expected value.

psa_hash_abort(psa_hash_operation_t *operation)

Abort a hash operation.

psa_hash_clone(const psa_hash_operation_t *source_operation, psa_hash_operation_t *target_operation)

Clone a hash operation.

Function Documentation#

psa_hash_compute#

psa_status_t psa_hash_compute (psa_algorithm_t alg, const uint8_t * input, size_t input_length, uint8_t * hash, size_t hash_size, size_t * hash_length)

Calculate the hash (digest) of a message.

Parameters
TypeDirectionArgument NameDescription
psa_algorithm_tN/Aalg

The hash algorithm to compute (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(alg) is true).

const uint8_t *[in]input

Buffer containing the message to hash.

size_tN/Ainput_length

Size of the input buffer in bytes.

uint8_t *[out]hash

Buffer where the hash is to be written.

size_tN/Ahash_size

Size of the hash buffer in bytes.

size_t *[out]hash_length

On success, the number of bytes that make up the hash value. This is always #PSA_HASH_LENGTH(alg).

Note

  • To verify the hash of a message against an expected value, use psa_hash_compare() instead.


psa_hash_compare#

psa_status_t psa_hash_compare (psa_algorithm_t alg, const uint8_t * input, size_t input_length, const uint8_t * hash, size_t hash_length)

Calculate the hash (digest) of a message and compare it with a reference value.

Parameters
TypeDirectionArgument NameDescription
psa_algorithm_tN/Aalg

The hash algorithm to compute (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(alg) is true).

const uint8_t *[in]input

Buffer containing the message to hash.

size_tN/Ainput_length

Size of the input buffer in bytes.

const uint8_t *[out]hash

Buffer containing the expected hash value.

size_tN/Ahash_length

Size of the hash buffer in bytes.


psa_hash_operation_init#

static psa_hash_operation_t psa_hash_operation_init (void )

Return an initial value for a hash operation object.

Parameters
TypeDirectionArgument NameDescription
voidN/A

psa_hash_setup#

psa_status_t psa_hash_setup (psa_hash_operation_t * operation, psa_algorithm_t alg)

Set up a multipart hash operation.

Parameters
TypeDirectionArgument NameDescription
psa_hash_operation_t *[inout]operation

The operation object to set up. It must have been initialized as per the documentation for #psa_hash_operation_t and not yet in use.

psa_algorithm_tN/Aalg

The hash algorithm to compute (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(alg) is true).

The sequence of operations to calculate a hash (message digest) is as follows:

  1. Allocate an operation object which will be passed to all the functions listed here.

  2. Initialize the operation object with one of the methods described in the documentation for #psa_hash_operation_t, e.g. #PSA_HASH_OPERATION_INIT.

  3. Call psa_hash_setup() to specify the algorithm.

  4. Call psa_hash_update() zero, one or more times, passing a fragment of the message each time. The hash that is calculated is the hash of the concatenation of these messages in order.

  5. To calculate the hash, call psa_hash_finish(). To compare the hash with an expected value, call psa_hash_verify().

If an error occurs at any step after a call to psa_hash_setup(), the operation will need to be reset by a call to psa_hash_abort(). The application may call psa_hash_abort() at any time after the operation has been initialized.

After a successful call to psa_hash_setup(), the application must eventually terminate the operation. The following events terminate an operation:


psa_hash_update#

psa_status_t psa_hash_update (psa_hash_operation_t * operation, const uint8_t * input, size_t input_length)

Add a message fragment to a multipart hash operation.

Parameters
TypeDirectionArgument NameDescription
psa_hash_operation_t *[inout]operation

Active hash operation.

const uint8_t *[in]input

Buffer containing the message fragment to hash.

size_tN/Ainput_length

Size of the input buffer in bytes.

The application must call psa_hash_setup() before calling this function.

If this function returns an error status, the operation enters an error state and must be aborted by calling psa_hash_abort().


psa_hash_finish#

psa_status_t psa_hash_finish (psa_hash_operation_t * operation, uint8_t * hash, size_t hash_size, size_t * hash_length)

Finish the calculation of the hash of a message.

Parameters
TypeDirectionArgument NameDescription
psa_hash_operation_t *[inout]operation

Active hash operation.

uint8_t *[out]hash

Buffer where the hash is to be written.

size_tN/Ahash_size

Size of the hash buffer in bytes.

size_t *[out]hash_length

On success, the number of bytes that make up the hash value. This is always #PSA_HASH_LENGTH(alg) where alg is the hash algorithm that is calculated.

The application must call psa_hash_setup() before calling this function. This function calculates the hash of the message formed by concatenating the inputs passed to preceding calls to psa_hash_update().

When this function returns successfully, the operation becomes inactive. If this function returns an error status, the operation enters an error state and must be aborted by calling psa_hash_abort().

Warnings

  • Applications should not call this function if they expect a specific value for the hash. Call psa_hash_verify() instead. Beware that comparing integrity or authenticity data such as hash values with a function such as memcmp is risky because the time taken by the comparison may leak information about the hashed data which could allow an attacker to guess a valid hash and thereby bypass security controls.


psa_hash_verify#

psa_status_t psa_hash_verify (psa_hash_operation_t * operation, const uint8_t * hash, size_t hash_length)

Finish the calculation of the hash of a message and compare it with an expected value.

Parameters
TypeDirectionArgument NameDescription
psa_hash_operation_t *[inout]operation

Active hash operation.

const uint8_t *[in]hash

Buffer containing the expected hash value.

size_tN/Ahash_length

Size of the hash buffer in bytes.

The application must call psa_hash_setup() before calling this function. This function calculates the hash of the message formed by concatenating the inputs passed to preceding calls to psa_hash_update(). It then compares the calculated hash with the expected hash passed as a parameter to this function.

When this function returns successfully, the operation becomes inactive. If this function returns an error status, the operation enters an error state and must be aborted by calling psa_hash_abort().

Note

  • Implementations shall make the best effort to ensure that the comparison between the actual hash and the expected hash is performed in constant time.


psa_hash_abort#

psa_status_t psa_hash_abort (psa_hash_operation_t * operation)

Abort a hash operation.

Parameters
TypeDirectionArgument NameDescription
psa_hash_operation_t *[inout]operation

Initialized hash operation.

Aborting an operation frees all associated resources except for the operation structure itself. Once aborted, the operation object can be reused for another operation by calling psa_hash_setup() again.

You may call this function any time after the operation object has been initialized by one of the methods described in #psa_hash_operation_t.

In particular, calling psa_hash_abort() after the operation has been terminated by a call to psa_hash_abort(), psa_hash_finish() or psa_hash_verify() is safe and has no effect.


psa_hash_clone#

psa_status_t psa_hash_clone (const psa_hash_operation_t * source_operation, psa_hash_operation_t * target_operation)

Clone a hash operation.

Parameters
TypeDirectionArgument NameDescription
const psa_hash_operation_t *[in]source_operation

The active hash operation to clone.

psa_hash_operation_t *[inout]target_operation

The operation object to set up. It must be initialized but not active.

This function copies the state of an ongoing hash operation to a new operation object. In other words, this function is equivalent to calling psa_hash_setup() on target_operation with the same algorithm that source_operation was set up for, then psa_hash_update() on target_operation with the same input that that was passed to source_operation. After this function returns, the two objects are independent, i.e. subsequent calls involving one of the objects do not affect the other object.