CRYOTIMER initialization structure.

Public Attributes#

bool

Enable/disable counting when initialization is complete.

bool

Enable/disable timer counting during debug halt.

bool

Enable/disable EM4 Wakeup.

Select the oscillator for the CRYOTIMER.

A period between a wakeup event/interrupt.

Public Attribute Documentation#

enable#

bool CRYOTIMER_Init_TypeDef::enable

Enable/disable counting when initialization is complete.


debugRun#

bool CRYOTIMER_Init_TypeDef::debugRun

Enable/disable timer counting during debug halt.


em4Wakeup#

bool CRYOTIMER_Init_TypeDef::em4Wakeup

Enable/disable EM4 Wakeup.


osc#

CRYOTIMER_Osc_TypeDef CRYOTIMER_Init_TypeDef::osc

Select the oscillator for the CRYOTIMER.


presc#

CRYOTIMER_Presc_TypeDef CRYOTIMER_Init_TypeDef::presc

Prescaler.


period#

CRYOTIMER_Period_TypeDef CRYOTIMER_Init_TypeDef::period

A period between a wakeup event/interrupt.