RTCC capture/compare channel configuration structure.

Public Attributes#

Select mode of Capture/Compare channel.

Compare mode channel match output action.

Capture mode channel PRS input channel selection.

Capture mode channel input edge selection.

Comparison base of channel in compare mode.

uint8_t

The COMPMASK (5 bit) most significant bits of compare value will not be subject to comparison.

Public Attribute Documentation#

chMode#

RTCC_CapComChMode_TypeDef RTCC_CCChConf_TypeDef::chMode

Select mode of Capture/Compare channel.


Definition at line 257 of file platform/emlib/inc/em_rtcc.h

compMatchOutAction#

RTCC_CompMatchOutAction_TypeDef RTCC_CCChConf_TypeDef::compMatchOutAction

Compare mode channel match output action.


Definition at line 260 of file platform/emlib/inc/em_rtcc.h

prsSel#

RTCC_PRSSel_TypeDef RTCC_CCChConf_TypeDef::prsSel

Capture mode channel PRS input channel selection.


Definition at line 263 of file platform/emlib/inc/em_rtcc.h

inputEdgeSel#

RTCC_InEdgeSel_TypeDef RTCC_CCChConf_TypeDef::inputEdgeSel

Capture mode channel input edge selection.


Definition at line 266 of file platform/emlib/inc/em_rtcc.h

compBase#

RTCC_CompBase_TypeDef RTCC_CCChConf_TypeDef::compBase

Comparison base of channel in compare mode.


Definition at line 269 of file platform/emlib/inc/em_rtcc.h

compMask#

uint8_t RTCC_CCChConf_TypeDef::compMask

The COMPMASK (5 bit) most significant bits of compare value will not be subject to comparison.



Definition at line 274 of file platform/emlib/inc/em_rtcc.h

dayCompMode#

RTCC_DayCompareMode_TypeDef RTCC_CCChConf_TypeDef::dayCompMode

Day compare mode.


Definition at line 279 of file platform/emlib/inc/em_rtcc.h