TIMER initialization structure.

Public Attributes#

bool

Start counting when initialization completed.

bool

Counter shall keep running during debug halt.

Prescaling factor, if HFPER / HFPERB clock used.

Action on falling input edge.

Action on rising input edge.

Counting mode.

bool

DMA request clear on active.

bool

Select X2 or X4 quadrature decode mode (if used).

bool

Determines if only counting up or down once.

bool

Timer can be start/stop/reload by other timers.

Public Attribute Documentation#

enable#

bool TIMER_Init_TypeDef::enable

Start counting when initialization completed.


Definition at line 280 of file platform/emlib/inc/em_timer.h

debugRun#

bool TIMER_Init_TypeDef::debugRun

Counter shall keep running during debug halt.


Definition at line 283 of file platform/emlib/inc/em_timer.h

prescale#

TIMER_Prescale_TypeDef TIMER_Init_TypeDef::prescale

Prescaling factor, if HFPER / HFPERB clock used.


Definition at line 286 of file platform/emlib/inc/em_timer.h

clkSel#

TIMER_ClkSel_TypeDef TIMER_Init_TypeDef::clkSel

Clock selection.


Definition at line 289 of file platform/emlib/inc/em_timer.h

fallAction#

TIMER_InputAction_TypeDef TIMER_Init_TypeDef::fallAction

Action on falling input edge.


Definition at line 306 of file platform/emlib/inc/em_timer.h

riseAction#

TIMER_InputAction_TypeDef TIMER_Init_TypeDef::riseAction

Action on rising input edge.


Definition at line 309 of file platform/emlib/inc/em_timer.h

mode#

TIMER_Mode_TypeDef TIMER_Init_TypeDef::mode

Counting mode.


Definition at line 312 of file platform/emlib/inc/em_timer.h

dmaClrAct#

bool TIMER_Init_TypeDef::dmaClrAct

DMA request clear on active.


Definition at line 315 of file platform/emlib/inc/em_timer.h

quadModeX4#

bool TIMER_Init_TypeDef::quadModeX4

Select X2 or X4 quadrature decode mode (if used).


Definition at line 318 of file platform/emlib/inc/em_timer.h

oneShot#

bool TIMER_Init_TypeDef::oneShot

Determines if only counting up or down once.


Definition at line 321 of file platform/emlib/inc/em_timer.h

sync#

bool TIMER_Init_TypeDef::sync

Timer can be start/stop/reload by other timers.


Definition at line 324 of file platform/emlib/inc/em_timer.h